This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Scan for available Bluetooth devices[edit source]
AF:BD:3B:26:61 lmecxl0923 B0:55:08:40:33:84 HUAWEI P8 lite 2017hcitool scan Scanning ... A0:
2. Setting the device to Visible[edit source]
To control the visiblity of our Bluetooth device to other Bluetooth hardware.
- to enable visibility:
hciconfig hciX piscan
(hciX corresponds to the available Bluetooth hardware: hci0)
- To disable visibility:
hciconfig hciX noscan
(hciX corresponds to the available Bluetooth hardware: hci0)
3. How to scan via bluetoothd/systemd[edit source]
Systemd provides a tool for Bluetooth management: bluetoothctl.
Example session with bluetoothclt for scanning, pairing, connecting:
STM ... [bluetooth]# scan off [CHG] Controller 43:43:A1:12:1F:AC Discovering: no Discovery stopped [bluetooth]#pair D8:DB:36:D1:39:88 Pairing successful [bluetooth]# connect D8:DB:36:D1:39:88 Connection successful [STM]# quit Agent unregistered [DEL] Controller 43:43:A1:12:1F:AC stm32mp1 [default]bluetoothctl [NEW] Controller 43:43:A1:12:1F:AC stm32mp1 [default] Agent registered [bluetooth]# power on Changing power on succeeded [CHG] Controller 43:43:A1:12:1F:AC Powered: yes [bluetooth]# agent on Agent is already registered [bluetooth]# default-agent Default agent request successful [bluetooth]# scan on Discovery started [CHG] Controller 43:43:A1:12:1F:AC Discovering: yes [NEW] Device D8:DB:36:D1:39:88