Last edited 4 years ago

How to set up proxy and P2P Ethernet connection with STM32CubeIDE

1. Introduction[edit source]

This article explains how to set up a point-to-point connection to the STM32 MPU board, especially if a proxy is also setup on the PC for accessing the Internet.

2. Setting up the network[edit source]

To set up the connection

  • go to Windows -> Preferences -> General -> Network Connections
  • select "Manual" in the Active Provider field, and:
    • adjust your proxy setup with Edit... in Proxy entries
    • configure a new Proxy bypass with Add Host... giving the IP address of the STM32 MPU target


Network Setting in STM32CubeIDE