Last edited 3 years ago

Arm Cortex-A7

1 Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the Arm® Cortex®-A7 core and its main features
  • indicate the level of security supported by this processor

2 Peripheral overview[edit source]

The Arm Cortex-A7 can be instantiated several times into a single cluster.

The STM32MP15 main processor is a Cortex-A7 cluster embedding one or two core(s), depending on the selected line.

2.1 Features[edit source]

The Cortex-A7 is a 32-bit processor that belongs to ARMv7-VE architecture family. ARMv7-VE corresponds to the ARMv7-A architecture, with virtual extensions. Among a wide range of features, it includes a memory management unit (MMU), a separate L1 cache and a unified L2 cache in order to efficiently support rich operating systems such as Linux, with a high level of performance.

Refer to the STM32MP15 reference manuals for the complete list of features.

2.2 Security support[edit source]

The Cortex-A7 supports a non-secure and secure modes that define two hardware execution contexts, named Cortex-A7 non-secure and Cortex-A7 secure.

3 Peripheral usage and associated software[edit source]

All the software components executed by the Cortex-A7, at boot time and at runtime, constitute the OpenSTLinux distribution.

3.1 Boot time[edit source]

As soon as the STM32MP1 is powered up, the Cortex-A7 starts to execute the ROM code, which is the first stage of the boot chain. It then executes the FSBL TF-A in secure mode before jumping to the SSBL U-Boot in non-secure mode.

3.2 Runtime[edit source]

3.2.1 Overview[edit source]

The Cortex-A7 runs Linux in non-secure mode and OP-TEE in secure mode. Linux is executed in SMP mode on the dual-core versions, as explained in the above.

3.2.2 Software frameworks[edit source]

Domain Peripheral Software components Comment
OP-TEE Linux STM32Cube
Ecosystem Cortex-A7 OP-TEE Linux

3.2.3 Peripheral configuration[edit source]

The Cortex-A7 configuration is done by the various components running on it, according to build-time parameters, and also information from the device tree.

3.2.4 Peripheral assignment[edit source]

The Cortex-A7 is the main processor supporting Cortex-A7 secure and Cortex-A7 non-secure contexts. It therefore cannot be assigned but, it manages all the peripherals assigned to those contexts.

4 How to go further[edit source]

Refer to Arm website[1] for more detailed information on this core.

5 References[edit source]