This article provides basic information about the DMA engine and how STM32 DMA, DMAMUX and MDMA drivers are plugged into it.
1. Framework purpose[edit source]
This article provides basic information about the DMA framework. However it is worth browsing the Kernel documentation related to DMA concept[1].
The direct memory access (DMA) is a feature that allows some hardware subsystems to access memory independently from the central processing unit (CPU).
The DMA can transfer data between peripherals and memory or between memory and memory.
2. System overview[edit source]
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/3/36/DMA_schemas.png)
2.1. Component description[edit source]
- Peripheral DMA client drivers:
DMA clients are drivers that are mapped on the DMA API[2].
- DMA engine:
The DMA engine is the engine core on which all clients rely.
Refer to DMA provider[1] for useful information on DMA internal behaviour.
- Virtual DMA channel support:
The virtual DMA channel support manages virtual DMA channels and DMA requests queues. This layer is no used by DMA clients.
- STM32 xDMA driver:
The STM32 xDMA driver is used to develop the DMA engine API.
- STM32 DMAMUX driver:
The STM32 DMAMUX driver request multiplexer allows routing DMA request lines between the device peripherals and the DMA controllers.
- DMAMUX, DMA and MDMA IP controller:
This is the STM32 DMA controller that handles data transfers between peripherals and memories or memory and memory connected to the same bus.
DMAMUX (DMA request router): DMAMUX internal peripheral
DMA: DMA internal peripheral
MDMA : MDMA internal peripheral
- Peripheral clients:
Peripheral clients are peripherals where at least one DMA request line is mapped on DMAMUX.
- Memories:
Memories can be either internal (e.g. SRAM, RETRAM or BCKRAM) or external (DDR).
2.2. APIs description[edit source]
Please refer to DMA Engine API Guide[3] for a clear description of the DMA framework API.
In addition, going through Dynamic API[4] provides insight on the DMA memory allocation API. The client has to rely on this API to properly allocate DMA buffers so that they are processed by the DMA engine without any trouble.
The document Dynamic DMA mapping Guide[5] can be read in conjunction with the previous one.
It presents some examples and usecases.
3. Configuration[edit source]
3.1. Kernel Configuration[edit source]
The DMA engine and driver are enabled throughout menu config (see Menuconfig or how to configure kernel):
For DMA:
Device Drivers -> [*] DMA Engine support -> [*] STMicroelectronics STM32 DMA support
For DMAMUX:
Device Drivers ->
[*] DMA Engine support ->
[*] STMicroelectronics STM32 dma multiplexer support
For MDMA
Device Drivers ->
[*] DMA Engine support ->
[*] STMicroelectronics STM32 master dma support
3.2. Device Tree configuration[edit source]
The DT configuration can be done using the STM32CubeMX.
Refer to the following articles for a description of the DT configuration:
- For DMA: DMA device tree configuration
- For DMAMUX: DMAMUX device tree configuration
- For MDMA: MDMA device tree configuration
4. How to use the framework[edit source]
Refer to the DMA Engine API Guide[6].
4.1. Request a DMA channel[edit source]
SoC device tree contains the "dmas" and "dma-names" properties in peripheral nodes having request line mapped. Peripheral drivers just have to request one or more DMA channels, generally during probe.
#include <linux/dmaengine.h>
struct dma_chan *dma_request_chan(struct device *dev, const char *name);
Thanks to the name, dmaengine find a channel matching the configuration specified in the dmas property.
struct dma_chan *chan_rx, *chan_tx;
chan_rx = dma_request_chan(&pdev->dev, "rx");
chan_tx = dma_request_chan(&pdev->dev, "tx");
The returned channel can be null, if there are no more available channels or no one fits the requested configuration. So, the peripheral must check the returned channel, and switch to interrupt mode in case it is null.
4.2. Configure the DMA channel[edit source]
A part of channel configuration comes from the dmas property in peripheral device tree node. Refer to the description in DMA controller Device Tree bindings. dma_slave_config structure is also used to set up the channel. See the dma_slave_config structure definition in include/linux/dmaengine.h for an exhaustive description.
struct dma_slave_config {
enum dma_transfer_direction direction;
phys_addr_t src_addr;
phys_addr_t dst_addr;
enum dma_slave_buswidth src_addr_width;
enum dma_slave_buswidth dst_addr_width;
u32 src_maxburst;
u32 dst_maxburst;
u32 src_port_window_size;
u32 dst_port_window_size;
bool device_fc;
unsigned int slave_id;
};
Source/Destination addresses, Source/Destination address width, Source/Destination maximum burst are used by the DMA controller driver to configure the channel. The user should use dmaengine_slave_config() to set this dma_slave_config structure in the DMA controller driver.
struct dma_slave_config config;
/* In case of Memory to Device (TX) */
memset(&config, 0, sizeof(config));
config.dst_addr = phy_addr + txdr_offset;
config.dst_addr_width = DMA_SLAVE_BUSWIDTH_1_BYTE;
config.dst_maxburst = 1;
config.direction = DMA_MEM_TO_DEV;
/* In case of Device to Memory (RX/Capture)
memset(&config, 0, sizeof(config));
config.src_addr = phy_addr + rxdr_offset;
config.src_addr_width = DMA_SLAVE_BUSWIDTH_1_BYTE;
config.src_maxburst = 1;
config.direction = DMA_DEV_TO_MEM;
int dmaengine_slave_config(struct dma_chan *chan, struct dma_slave_config *config);
4.3. Configure the DMA transfer[edit source]
The dmaengine transfer API must be used to prepare the DMA transfer. Three modes are supported by STM32 DMA controllers drivers:
- slave_sg: prepare a transfer of a list of scatter gather buffer from/to a peripheral
- dma_cyclic: prepare a cyclic operation from/to a peripheral until the operation is stopped by the user
- dma_memcpy: prepare a memcpy operation (rarely used except by dmatest)
struct dma_async_tx_descriptor *dmaengine_prep_slave_sg(
struct dma_chan *chan, struct scatterlist *sgl,
unsigned int sg_len, enum dma_data_direction direction,
unsigned long flags);
struct dma_async_tx_descriptor *dmaengine_prep_dma_cyclic(
struct dma_chan *chan, dma_addr_t buf_addr, size_t buf_len,
size_t period_len, enum dma_data_direction direction);
struct dma_async_tx_descriptor *dmaengine_prep_dma_memcpy(
struct dma_chan *chan, dma_addr_t dst, dma_addr_t src,
size_t len, unsigned long flags);
A peripheral driver completion callback can be set up using the callback* fields of the dma_async_tx_descriptor returned by the dmaengine_prep* function.
struct dma_async_tx_descriptor *txdesc;
txdesc = dmaengine_prep_...
txdesc->callback = peripheral_driver_dma_callback;
txdesc->callback_param = peripheral_dev;
4.4. Submit the DMA transfer[edit source]
4.5. Terminate the DMA transfer[edit source]
4.6. Release the DMA channel[edit source]
5. How to trace and debug the framework[edit source]
5.1. How to trace[edit source]
Through menuconfig, enable DMA engine debugging and DMA engine verbose debugging (including STM32 drivers):
Device Drivers -> [*] DMA Engine support -> [*] DMA Engine debugging [*] DMA Engine verbose debugging (NEW)
5.2. How to debug[edit source]
5.2.1. devfs[edit source]
sysfs entry can be used to browse for available DMA channels.
More information can be found in sysfs.
The following command lists all the registered DMA channels:
Board $> ls /sys/class/dma/ dma0chan0 dma0chan13 dma0chan18 dma0chan22 dma0chan27 dma0chan31 dma0chan8 dma1chan3 dma2chan0 dma2chan5 dma0chan1 dma0chan14 dma0chan19 dma0chan23 dma0chan28 dma0chan4 dma0chan9 dma1chan4 dma2chan1 dma2chan6 dma0chan10 dma0chan15 dma0chan2 dma0chan24 dma0chan29 dma0chan5 dma1chan0 dma1chan5 dma2chan2 dma2chan7 dma0chan11 dma0chan16 dma0chan20 dma0chan25 dma0chan3 dma0chan6 dma1chan1 dma1chan6 dma2chan3 dma0chan12 dma0chan17 dma0chan21 dma0chan26 dma0chan30 dma0chan7 dma1chan2 dma1chan7 dma2chan4
Each channel is expanded as follows:
Board $> ls -la /sys/class/dma/dma0chan0/ total 0 drwxr-xr-x 3 root root 0 Jun 7 21:22 . drwxr-xr-x 34 root root 0 Jun 7 21:22 .. -r--r--r-- 1 root root 4096 Jun 9 13:11 bytes_transferred lrwxrwxrwx 1 root root 0 Jun 9 13:11 device -> ../../../58000000.dma -r--r--r-- 1 root root 4096 Jun 9 13:11 in_use -r--r--r-- 1 root root 4096 Jun 9 13:11 memcpy_count drwxr-xr-x 2 root root 0 Jun 9 13:11 power lrwxrwxrwx 1 root root 0 Jun 9 13:11 subsystem -> ../../../../../../class/dma -rw-r--r-- 1 root root 4096 Jun 7 21:22 uevent
device indicates which DMA driver manages the channel.
echoing in_use indicates whether the channel has been allocated or not.
Board $> cat /sys/class/dma/dma0chan0/in_use 1
5.2.2. Debugfs[edit source]
debugfs entries are available. Via the /sys/kernel/debug/dmaengine users can get information about the DMA devices and the used channels.
root@stm32mp1:~# cat /sys/kernel/debug/dmaengine/summary dma0 (58000000.dma-controller): number of channels: 32 dma0chan0 | 48000000.dma-controller:ch0 dma0chan1 | 48000000.dma-controller:ch1 dma0chan2 | 48000000.dma-controller:ch2 dma0chan3 | 48000000.dma-controller:ch3 dma0chan4 | 48000000.dma-controller:ch4 dma0chan5 | 48000000.dma-controller:ch5 dma0chan6 | 48000000.dma-controller:ch6 dma0chan7 | 48000000.dma-controller:ch7 dma0chan8 | 48001000.dma-controller:ch0 dma0chan9 | 48001000.dma-controller:ch1 dma0chan10 | 48001000.dma-controller:ch2 dma0chan11 | 48001000.dma-controller:ch3 dma0chan12 | 48001000.dma-controller:ch4 dma0chan13 | 48001000.dma-controller:ch5 dma0chan14 | 48001000.dma-controller:ch6 dma0chan15 | 48001000.dma-controller:ch7 dma0chan16 | 54002000.hash:in dma1 (48000000.dma-controller): number of channels: 8 dma1chan0 | 4000e000.serial:rx (via router: 48002000.dma-router) dma1chan1 | 4000e000.serial:tx (via router: 48002000.dma-router) dma1chan2 | 4000b000.audio-controller:tx (via router: 48002000.dma-router) dma1chan3 | 4000b000.audio-controller:rx (via router: 48002000.dma-router) dma1chan4 | 4400b004.audio-controller:tx (via router: 48002000.dma-router) dma1chan5 | 4400b024.audio-controller:rx (via router: 48002000.dma-router) dma2 (48001000.dma-controller): number of channels: 8
Other DMA debugfs entries are available when the Linux kernel is compiled with "Enable debugging of DMA-API usage" configuration. They are documented in Part III - Debug drivers use of the DMA-API[4].
5.2.3. dmatest[edit source]
dmatest can be used to validate or debug DMA engine and driver without using client devices. This module is more a test than a debug module. It performs a memory-to-memory copy using standard DMA engine API.
For details on how to use this kernel module, refer to [7].
6. Source code location[edit source]
DMA: drivers/dma/stm32-dma.c
MDMA: drivers/dma/stm32-mdma.c
DMAMUX: drivers/dma/stm32-dmamux.c
DMA engine:
- Engine: drivers/dma/dmaengine.c
- Virtual channel support: drivers/dma/virt-dma.c
7. To go further[edit source]
Very useful documentation can be found at DMAEngine documentation
8. References[edit source]