This page is a candidate for renaming (move). The requested new name is: Arm CoreSight peripheral . The supplied reason is: NSA : remove the 'S' at the end of peripheral, to be confirmed by MT . -- Registered User (-) 09:13, 6 January 2021 (CET). Wiki maintainers: remember to update the pages that link this page before renaming (moving) it. |
1. Article purpose[edit source]
The purpose of this article is to give information about the Arm® CoreSight™ subsystem.
It explains what are the principle peripherals of this subsystem.
2. Peripheral overview[edit source]
Arm® CoreSight™ products include a wide range of trace macrocells for Arm® processors, system and software instrumentation and a comprehensive set of IP blocks to enable the debug & trace of the most complex, multi-core SoCs.
Arm® has defined an open CoreSight architecture to allow SoC designers to add debug & trace capabilities for other IP cores in to the CoreSight infrastructure.
2.1. Components description[edit source]
The debug features are based on Arm® CoreSight™ components:
• SWJ-DP: JTAG/Serial-wire debug port
• AXI-AP: AXI access port
• AHB-AP: AHB access port
• APB-AP: APB access port
• ITM: Instrumentation Trace Macrocell
• DWT: Data Watchpoint and Trace
• ETM: Embedded Trace Macrocell
• ETF: Embedded Trace FIFO
• TPIU: Trace Port Interface Unit
• SWO: Serial Wire Output
• CTI: Cross Trigger Interface
• CTM: Cross Trigger Matrix
• TSGEN: Timestamp Generator
• STM: System Trace Macrocell
More information about these components can be found in the Arm® website [1]
2.2. Features[edit source]
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are really implemented.
2.3. Security support[edit source]
The Arm® CoreSight™ is a non secure peripheral.
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
The Arm® CoreSight™ is not used at boot time.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
Internal peripheral generates a trace stream, namely instruction traces, depending on instructions and events happening when CPUs are executing a program. This encoded stream can be then stored in a dedicated SRAM via a buffer and/or extracted through an external port.
3.2.2. Software frameworks[edit source]
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Trace & Debug | Arm CoreSight |
3.2.3. Peripheral configuration[edit source]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.
4. References[edit source]