1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the Arm® Cortex®-A7 core and its main features
- indicate the level of security supported by this processor
2. Peripheral overview[edit source]
The Arm Cortex-A7 is the main processor embedded in the STM32MP15 microprocessor, where it can be present in single or dual instance(s) across the STM32MP15x lines.
2.1. Features[edit source]
Among a wide range of features, the Cortex-A7 includes a memory management unit (MMU) in order to efficiently support rich OS such as Linux.
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.
2.2. Security support[edit source]
The Cortex-A7 supports a non-secure and a secure modes that are defining two hardware execution contexts, so called Cortex-A7 non-secure and Cortex-A7 secure.
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
As soon as the STM32MP1 is powered up, the Cortex-A7 starts to execute the ROM code, that is the first stage of the boot chain.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
The Cortex-A7 is running Linux, in SMP mode (on the dual core versions, as explained in the above).
3.2.2. Software frameworks[edit source]
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Domain | Peripheral (XXX internal peripheral) | Linux |
3.2.3. Peripheral configuration[edit source]
The Cortex-A7 configuration is done by the various components running on it, according to build times parameters but also information coming from the device tree.
3.2.4. Peripheral assignment[edit source]
The Cortex-A7 non-secure (resp. secure) mode is implicitely assigned to the Cortex-A7 non-secure (resp. secure) execution context.
4. How to go further[edit source]
Refer to the [1].
5. References[edit source]
- ↑ Cortex-A7 processor on Arm developer website for more detailled information on this core