How to install the Yocto Project SDK in STM32CubeIDE

Revision as of 14:47, 25 August 2020 by Registered User

This article explains the way STM32CubeIDE is managing Yocto SDK provided by OpenSTLinux.

1. Overview[edit source]

Two flavors are proposed for installing Yocto SDK:

  • Yocto SDK is already installed on host workstation, typically after a download of the STM32MP1 OpenSTLinux Developer Package. In that case, only a setup is needed for STM32CubeIDE to use it.
  • Yocto SDK is not present on host workstation, it can be installed via STM32CubeIDE.

The choice is proposed after the Setup OpenSTLinux menu, selecting Use existing.

OpenSTLinux SDK Installation Menu

Note that Setup OpenSTLinux phase also includes download and installation of OpenSTLinux Sources plugin.

2. Using already installed Yocto SDK[edit source]

You have then to give the Yocto SDK Install Root Path in the STM32Cube Preferences.

OpenSTLinux SDK Manager

3. Installing Yocto SDK via STM32CubeIDE[edit source]

This corresponds to the Download choice where OpenSTLinux SDK plugin is installed. Note that missing of OpenSTLinux required packages will lead to unpredictable Yocto SDK usage...

Warning white.png Warning
OpenSTLinux development requires specific packages on host workstation. See PC_prerequisites.

A second choice allows to install Yocto SDK as:

    • external, on host workstation disk, outside STM32CubeIDE scope; Yocto SDK removal is under final user responsibility
    • embedded inside the STM32CubeIDE; Yocto SDK removal is managed by STM32CubeIDE
OpenSTLinux SDK Install Location

.