How to integrate AWS IoT Greengrass on top of openSTLinux distribution

Revision as of 12:00, 24 June 2020 by Registered User (→‎AWS greengrass target initialization)


1. Article purpose[edit source]

The purpose of this article is to explain how to integrate Amazon Web Service (AWS) IoT Greengrass [1] on top of OpenSTLinux, included the security part with the connection to a Hardware Security Module (a TPMv2.0).

This article explains step by step how to add the yocto "meta-demo-aws" on top of OpenSTLinux distribution, to configure build and install the image, to execute the AWS greengrass certification testing and to configure the target for a secure connection with the AWS cloud.


2. Prerequisites[edit source]

You need some knowledge of the AWS IoT Greengrass, and to configure your AWS cloud account, follow the process described in [AWS amazon site][2]

2.1. Hardware prerequisites[edit source]

The process has been verified withe the board STM32MP157C-DK2 Discovery kit More info green.png and STM32MP157F-DK2 Discovery kit More info green.png.


  • STM32MP157C-DK2
STM32MP157C-DK2

For more information about the STM32 discovery board and how to start it up, jump to this section Getting_started/STM32MP1_boards/STM32MP157x-DK2

  • STPM4RasPI expansion board[3]
STPM4RasPI

The STPM4RasPI is an official extension board to connect the ST33 TPM products to the Raspberry Pi® device. It is designed for development, proof of concept or demonstration activities. The board is shipped with one trusted platform module soldered. The ST33 TPM device soldered is the ST33TPHF20SPI, it is a TPM V2.0 specification implementation.

2.2. Software prerequisites[edit source]

The STM32MP1 Distribution Package must be installed on your host. The process has been verified with the delivery ecosystem release v1.1.0 , ecosystem release v1.2.0 and ecosystem release v2.0.0 of the OpenSTlinux distribution.

3. Software update with meta-st-demo-aws[edit source]


Info white.png Information
The meta-st-stm32mpu-app-aws, is based on the AWS Greengrass Core v1.10.1
Info white.png Information
Some AMAZON Greengrass functionalities require to add a "Docker" and "Java-jdk" software components in the OpenSTLinux distribution

1.Clone following git repository into [your STM32MP1 Distribution path]/layers/meta-st/

  
  PC $>git clone ssh://${USER}@gerrit.st.com:29418/stm32mpuapp/meta/meta-st-stm32mpu-app-aws.git t
  PC $>cd meta-st-stm32mpu-app-aws 
  PC $>git checkout MMDV_V200

2.Enable TPM build

Apply the following patch in the file [your STM32MP1 Distribution path]/layers/meta-st/meta-st-openstlinux/conf/distro/include/openstlinux.inc

DISTRO_FEATURES_append = " tpm2 "

3.Add Virtualization (docker) in the OpenSTLinux distribution

Executes the command, on the host :

cd [your STM32MP1 Distribution path]/layers
git clone git://git.yoctoproject.org/meta-virtualization
git checkout remotes/origin/dunfell
bitbake add-layer [your STM32MP1 Distribution path]/layers/meta-virtualization

Update the file [your STM32MP1 Distribution path]/layers/meta-st/meta-st-openstlinux/conf/distro/openstlinux-weston.conf.

DISTRO_FEATURES_append = "virtualization"

4.Add Java-jdk

Follow the install process define in the article How to install JAVA JDK article.

5.Increase the Rootfs partition size

Update the file [your STM32MP1 Distribution path]/ layers/meta-st/meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc

#IMAGE_ROOTFS_MAXSIZE ?= "763904"
IMAGE_ROOTFS_MAXSIZE = "2097152"

6.Setup the build environment

Executes the command, on the host :

cd [your STM32MP1 Distribution path]
DISTRO=openstlinux-weston MACHINE=stm32mp1-demo-aws source layers/meta-st/scripts/envsetup.sh

7.Build the image

Info white.png Information
The image is configured by default to include elements for the execution of the AWS greengrass certification testing.

If you don't want this feature you can delete it from the image. In the file recipes-st/images/st-image-demo-aws.bb delete ${IMAGE_AWSGREENGRASSTEST_PART} in CORE_IMAGE_EXTRA_INSTALL definition.

In the folder [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws Executes the command :

bitbake st-image-demo-aws

8.Flash the sdcard

Use the programmer tool STM32CubeProgrammer

For example ,the tsv file FlashLayout_sdcard_ stm32mp157c-demo-aws-mx-trusted.tsv is located in [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws/tmp-glibc/deploy/images/stm32mp1-demo-aws/flashlayout_st-image-demo-aws

4. AWS greengrass target initialization[edit source]

1.Configuration of the target

Run the scripts for some extra configuration on the target (to execute only one time after the first boot).

source /greengrass/tpm_update.sh

If the image has been configured for the execution of the AWS greengrass certification testing.

source /greengrass/awsgreengrass_certif.sh

2.TPM token initialization

Info white.png Information
For the demo keep the values of the PINs (123456) and the PKCS11 STORE folder (usr/local/pkcs11_tpm), the scripts and greengrass config files examples use these values.
Info white.png Information
If you faced the ERROR ModuleNotFoundError: No module named 'pyasn1_modules', at the execution of the tpm2_tool command, use the python pip application to install the missing module:

cd /usr/bin

pip3 install pyasn1_modules

Note : if something goes wrong, you can reset the TPM and PKCS11 store with the following commands :

cd /usr/bin
./tpm2_clear -Q
rm -rf /usr/local/pkcs11_tpm/*

Executes the commands, on the target :

cd /tools
./tpm2_ptool init --primary-auth=123456 --path=$TPM2_PKCS11_STORE
./tpm2_ptool addtoken --pid=1 --sopin=123456 --userpin=123456 --label=greengrass --path $TPM2_PKCS11_STORE
./tpm2_ptool addkey --algorithm=rsa2048 --label="greengrass" --userpin=123456 --key-label=greenkey --path=$TPM2_PKCS11_STORE

OPTIONAL : Verifications with pkcs11-tool

Executes this command on the target to verify the token created.

pkcs11-tool --module /usr/lib/libtpm2_pkcs11.so.0 -L

Example of output expected :

Available slots:
   Slot 0 (0x1): greengrass STMicro
     token label        : greengrass
     token manufacturer : STMicro
     token model        :
    token flags        : login required, rng, token initialized, PIN initialized
     hardware version   : 1.38
     firmware version   : 74.8
     serial num         : 0000000000000000
     pin min/max        : 5/128

AT THIS STEP, THE CONFIGURATION OF THE BOARD IS COMPLETED TO BE USED  :

5. Process to execute the AWS Greengrass certification testing[edit source]

1.Install the AWS IoT Device Tester.

  Go to the AWS Amazon site to [AWS IoT Device Tester for AWS IoT Greengrass Versions] [4]

2.Configure your ssh connection (ssh keys)

  Go to the AWS Amazon site to [Configure Your Host Computer to Access Your Device Under Test][5]

3.Configure the IDT

  Example of the install config folder for Windows.
  C:\devicetester_greengrass_win\devicetester_greengrass_win\configs\
  Go to the AWS Amazon site [Setting Configuration to Run the AWS IoT Greengrass Qualification Suite][6]
  There is a  IDT configuration file example installed on your Host :
  /[your STM32MP1 Distribution path]/layers/meta-st/meta-st-demo-aws/recipes-aws/greengrasstests/greengrasstests/device-hsm.json
  Note : With this example the certification tests are performed in Root.

4.Execute the tests

  Go to the AWS Amazon site to [Running Tests][7]

6. Process to create a Certificat Signature Request using the hardware-protected private key[edit source]

1.Install the tool openssl on the target.

The packages are stored on your Host :

/[your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws/tmp-glibc/deploy/deb/cortexa7t2hf-neon-vfpv4

package openssl-bin_1.1.1a-r0_armhf.deb (usr/bin/openssl)
package openssl_1.1.1a-r0_armhf.deb (usr/lib/ssl-1.1/openssl.cnf ....; etc/ssl/certs and private folder)
package openssl-conf_1.1.1a-r0_armhf.deb (/etc/ssl/openssl.cnf)

Execute the commands, on the Host (the board is connected to your internet network) :

 scp openssl-bin_1.1.1a-r0_armhf.deb root@IP address of the board://root
 scp openssl_1.1.1a-r0_armhf.deb root@IP address of the board://root
 scp openssl-conf_1.1.1a-r0_armhf.deb root@IP address of the board://root

Execute the commands, on the target:

 cd /root
 dpkg -i openssl-bin_1.1.1a-r0_armhf.deb
 dpkg -i openssl-conf_1.1.1a-r0_armhf.deb
 dpkg -i openssl_1.1.1a-r0_armhf.deb
 sync

2.Update openssl configuration to use module tpm2_pkcs11

add the following lines in /etc/ssl/openssl.cnf :

openssl_conf = openssl_init
[openssl_init]
engines=engine_section
[engine_section]
pkcs11 = pkcs11_section
[pkcs11_section]
engine_id = pkcs11
dynamic_path = /usr/lib/engines-1.1/pkcs11.so
MODULE_PATH = /usr/lib/libtpm2_pkcs11.so.0
init = 0

3. How to create a CSR "Certificat Signature Request" with openssl (Prerequisite : openssl installed) Executes the command, on target :

openssl req -engine pkcs11 -new -key "pkcs11:token=greengrass;object=greenkey;type=private;pin-value=123456" -keyform engine -out /usr/local/req.csr

This CSR "/usr/local/req.csr" is used to create clients certificats on the AWS amazon Cloud to store on the board.

There is a greengrass configuration file example to update with your AWS account parameter and certificats created, on the target : /greengrass/config/config_secu_example.json

You need also to download the root CA on Amazon site and stored it on the target greengrass/certs/root.ca.pem.

For more information about HSM (Hardware Secure Module) integration for AWS greengrass, go to AWS Amazon site [Hardware Security Integration][8]

4.Connection to Amazon cloud

Before starting the greengrass core on the target you need to set the TPM2_PKCS11_STORE environment variable.

Executes the commands on the target :

export TPM2_PKCS11_STORE=/usr/local/pkcs11_tpm
cd /greengrass/ggc/core/
./greengrassd start

7. References[edit source]