1. Article purpose[edit source]
This article explains how to configure the SAI internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the ALSA framework.
The configuration is performed using the device tree mechanism that provides a hardware description of the SAI peripheral, used by the SAI linux driver.
2. DT bindings documentation[edit source]
STM32 SAI device tree bindings [1] document describes all the required and optional configuration properties.
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
The SAI is used as a component of a sound card through Linux® kernel ALSA framework. The device tree nodes related to the sound card are described in board device tree.
The STM32 SAI peripheral includes two independent audio subblocks that share common resources. The SAI device tree nodes reflects this architecture, as shown in the SAI DT sample below.
&saix { /* SAIx parent node. Configure common ressources */ clock-names = "pclk", "x8k", "x11k"; /* Peripheral and parent clock configuration. */ ... saixa { /* child node. Configure ressources dedicated to SAIxA subblock */ clock-names = "sai_ck"; /* SAIxA kernel clock confguration. */ pinctrl-names = "default"; /* GPIOsA configuration. */ ... }; saixb { /* child node. Configure ressources dedicated to SAIxB subblock */ clock-names = "sai_ck"; /* SAIxB kernel clock confguration. */ pinctrl-names = "default"; /* GPIOsB configuration. */ ... }; };
The STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit source]
The SAI nodes are declared in STM32 microprocessor device tree. They describe hardware parameters such as registers address, interrupt and DMA. This set of properties may not vary for a given STM32MPU. For STM32MP1, the corresponding DT file is stm32mp157c.dtsi[2].
3.2. DT configuration (board level)[edit source]
The SAI configuration is board dependent, whether is it connected or not to an external component such as an audio codec. The links between the SAI and the other components define a soundcard. This soundcard has to be configured in the board device tree. Refer to soundcard configuration for examples of SAI configuration on various STM32MPU boards.
3.3. DT configuration examples[edit source]
This chapter describes in detail advanced SAI configurations. These examples are based on STM32MP1 boards SAI use cases. The corresponding device trees can be found in soundcard article.
3.3.1. Setting SAI as a master clock provider[edit source]
The SAI peripheral can provide a clock to an external component (such as a codec) through the mclk output pin. In this case, it acts as master clock (mclk) provider. The below DT sample gives an example of SAI configuration as mclk provider.
In this example the codec driver supports mclk input based on ASoC DAPM mechanism. If this is not the case, the codec driver has to be adapted. This can be achieved by adding a DAPM clock supply widget to the codec driver. An example of the required clock supply DAPM widget can be found in Cirrus CS42L51 codec source code[3]. In the below device tree example, the codec DAPM clock widget is named "MCLKX".
To allow mclk activation/deactivation, a DAPM route must be defined in the DT. This route is defined in the sound node, as shown below.
soundcard { routing = "Playback" , "MCLKX", /* Set a route between "MCLKX" and "playback" widgets */ "Capture" , "MCLKX"; ... }; codec: { clocks = <&sai2a>; /* The codec is a consumer of SAI2A master clock */ clock-names = "MCLKX"; /* Feed MCLKX codec clock with SAI2A master clock provider */ ... }; &sai2 { ... sai2a: audio-controller@4400b004 { #clock-cells = <0>; /* Set SAI2A as master clock provider */ ... sai2a_endpoint: endpoint { mclk-fs = <256>; /* Set mclk/fs ratio. (256 or 512) */ }; }; };
3.3.2. Sharing master clock between two SAIs[edit source]
When a SAI is set as a master clock provider, another SAI can share this master clock. This can be achieved by setting a SAI as a mclk consumer through DT configuration. This means that the mclk consumer SAI can request to change the mclk rate, according to its own audio stream sampling rate. This implies that audio sampling rates must be identical when both SAI subblocks are used.
&sai2 { ... sai2a: audio-controller@4400b004 { #clock-cells = <0>; /* Set SAI2A as master clock provider */ ... }; sai2b: audio-controller@4400b024 { clocks = <&rcc SAI2_K>, <&sai2a>; /* SAI2B is a consumer of SAI2A master clock */ clock-names = "sai_ck", "MCLK"; /* Feed SAI2B MCLK clock with SAI2A master clock provider */ ... sai2b_endpoint: endpoint { mclk-fs = <256>; /* Set mclk/fs ratio. (256 or 512) */ }; }; };
3.3.3. Sharing the codec interface between two SAIs[edit source]
Two SAIs can share the same codec interface, by sharing the I2S bus (i.e. FS and SCK clocks). To achieve this, the codec has to be defined as the I2S bus master. Only one SAI is connected to the bus clocks. The other SAI has to be configured as a slave of the SAI connected to the bus. In this case, the GPIOs of both subblocks must be managed at parent level, so that the corresponding pins are activated whatever the running SAI.
From ASoC point of view, two CPU DAIs have to be connected to the same codec DAI. This topology is not supported natively by ASoC audio graph card, for time being. Indeed, when the audio graph card parses the codec nodes, it expects to find DAI interface indexes, matching the endpoints indexes. Implementing of_xlate_dai_id callback in the codec driver, allows to use the same DAI interface for both endpoints. An example of code can be found in the Cirrus CS42L51 codec source code[3].
- Code example
static int codec_of_xlate_dai_id(struct snd_soc_component *component,
struct device_node *endpoint)
{
/* return dai id 0, whatever the endpoint index */
return 0;
}
- DT example
codec { ... codec_port { codec_tx_endpoint { remote-endpoint = <&sai2a_endpoint>; frame-master; /* Set codec as master of SAI2A for FS clock. */ bitclock-master; /* Set codec as master of SAI2A for SCK clock. */ }; codec_rx_endpoint { /* Second endpoint mapped on codec DAI 0 via of_xlate */ remote-endpoint = <&sai2b_endpoint>; frame-master; /* Set codec as master of SAI2B for FS clock. */ bitclock-master; /* Set codec as master of SAI2B for SCK clock. */ }; }; }; &sai2 { pinctrl-names = "default", "sleep"; /* Defines SAI2A/B GPIOs at parent level. */ pinctrl-0 = <&sai2a_pins_a>, <&sai2b_pins_b>; pinctrl-1 = <&sai2a_sleep_pins_a>, <&sai2b_sleep_pins_b>; ... sai2a: audio-controller@4400b004 { remote-endpoint = <&codec_tx_endpoint>; ... }; sai2b: audio-controller@4400b024 { remote-endpoint = <&codec_rx_endpoint>; st,sync = <&sai2a 2>; /* Set SAI2B as slave of SAI2A. */ }; };
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References[edit source]
{{PublicationRequestId | 9809 | 2018-11-26 | AnneJ}