Last edited 5 years ago

How to use TTY with User Terminal

Template:ArticleMainWriter Template:ArticleApprovedVersion Template:UpdateNeededForNewRelease


1. Purpose[edit source]

This article describes how to use TTY with a user terminal. The TTY overview is described in Serial TTY overview article.

The use case of the following examples is a data transfer between a STM32 MPU board and PC, over a USB to a RS232 adapter cable.
The setup of this use case is described in details in the How to get Terminal article.


For the following examples:

  • uart4 is activated by default (for the Linux console)
  • usart3 is enabled by device tree
  • The usart3 pins are connected to a RS232 card
  • The RS232 card is connected to the PC over the USB to RS232 adapter cable.

Note: Some TTY tools are used in this article. A list of TTY tools is defined a dedicated article [TTY Tools ].

2. Print the file name of the terminal connected to standard input (with tty tool)[edit source]

Template:Board$ tty
Template:Green                                                                                 Template:Highlight

Template:InternalInfo

3. Change serial port configuration (with stty tool)[edit source]

Many serial port properties can be displayed and changed with the stty tool. The full feature list is available in stty user manual pages [1] .

Template:Board$ stty --help
  • Display the current configuration:
Template:Board$ stty -a -F /dev/ttySTM1                                                             Template:Highlight
speed 115200 baud; rows 45; columns 169; line = 0;

Template:InternalInfo

  • Display only the current baud rate:
Template:Board$ stty -F /dev/ttySTM1 speed
115200                                                                                     Template:Highlight

Template:InternalInfo

  • Change the baud rate:

stty -F /dev/ttySTMx EXPECTED_BAUDRATE

Example: change the baud rate to 19200

Template:Board$ stty -F /dev/ttySTM1 19200                                                          Template:Highlight

Template:InternalInfo

The stty tool proposes many arguments allowing many operations on a tty terminal, such as:

  • special settings (various arguments such as speed, line discipline, minimum number of characters for a completed read, size, timeout, etc...)
  • control settings
  • input settings
  • output settings
  • local settings
  • combination settings


Note: If you want to go further, an interesting tutorial describes termios and stty [2].

4. Send / Receive data (with stty, minicom, echo and cat tools)[edit source]

Sending data can be simply done by opening the device as a file and writing data to it:


  • Configure a port on ttySTM1 (usart3)
Template:Board$ stty -F /dev/ttySTM1 115200 -echo

Template:InternalInfo

  • Open a port on ttySTM1 (usart3) to receive data
Template:Board$ cat /dev/ttySTM1 &

Template:InternalInfo

  • On the remote PC, identify the tty terminal associated to RS232 card connected on STM32MPU USART3 pins
Template:PC$ ls /dev/ttyUSB*
/dev/ttyUSB0
  • Open a minicom terminal on the remote device connected on USART3 pins
Template:PC$ minicom -D /dev/ttyUSB0
  • Send data from remote PC to STM32MPU over USART3
Template:PC$ echo "HELLO" > /dev/ttyUSB0
  • send data from STM32MPU to remote PC over USART3
Template:Board$ echo "HELLO" > /dev/ttySTM1

Template:InternalInfo

5. Identify processes using a tty serial device (with fuser tool)[edit source]

Template:Board$ fuser /dev/ttySTM0
395 691 3872                                                                               Template:Highlight

Template:InternalInfo

6. Link a tty serial device with a line discipline (with ldattach tool)[edit source]

Attach ttySTM1 with line discipline number n :

Template:Board$ ldattach n /dev/ttySTM1

Template:InternalInfo

7. File transfer over serial console[edit source]

Please see the dedicated article How to transfer a file over serial console.

8. References[edit source]