This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleApprovedVersion
1. Introduction[edit source]
The purpose of this article is to describe how to build and execute the Khronos OpenGL ES 2.0 Conformance Tests.
These tests are provided by the Khronos Group [1]. They are available as open source from the Khronos CTS GitHub source repo [2].
For a detailed description of the Khronos OpenGL ES2.0 CTS, please refer to the openglcts README.md [3] file.
2. How to install khronos-cts[edit source]
2.1. Building khronos-cts[edit source]
Execute the following command in the OpenSTLinux build environment:
bitbake khronos-cts
2.2. Installing kronos-cts on the target board[edit source]
Execute the following command in the OpenSTLinux build environment:
scp -r tmp*/work/*neon*/khronos-cts/*/image/* root@<ip address of board>:/
3. How to execute khronos-cts[edit source]
Execute the following commands on the target board:
cd /home/root
./cts-runner --type=es2 1>results.txt
[ 1] EGL: enable default configs for conformance test
...
![Khronos gles cts1.png](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/thumb/3/3a/Khronos_gles_cts1.png/480px-Khronos_gles_cts1.png)
4. Testing verdict example[edit source]
... Test run totals: Passed: 13786/13957 (98.8%) Failed: 11/13957 (0.1%) Not supported: 131/13957 (0.9%) Warnings: 29/13957 (0.2%) 219/220 sessions passed, conformance test FAILED