1. Article Purpose[edit source]
This section details the TF-A BL2 component uses as FSBL.
It will explain the usage in STM32 MPU context and the build process from sources and how to deploy it on your target.
The build examples are based on the OpenSTLinux environment:
- Developer Package
- Distribution Package
2. Overview[edit source]
TF-A BL2 is the FSBL for the ST boot chain. It is loaded by ROM Code in internal SYSRAM.
The main goal of this stage is to start the DDR to load (and authenticate) other firmware from a FIP binary.
2.1. STM32 binary file[edit source]
The TF-A BL2 firmware needs to be STM32 encapsulated to be properly loaded into SYSRAM by the ROM Code.
STM32 header information are mandatory for the ROM Code to load, authenticate and start the firmware.
As the ROM code is only able to load a single binary, the STM32 file must embed in the same image the header, the device tree and the BL2 firmware.
TF-A BL2 is part of the trusted boot and can be signed to be ROM Code authenticated. See Secure boot process.
2.2. Device tree[edit source]
TF-A BL2 is based on device tree configuration. It uses the same device tree than the kernel but keeping only the mandatory nodes for the boot stage (to reduce binary size).
The device tree is part of the final STM32 file to be authenticated by the ROM Code and loaded at the same time in the SYSRAM.
It must be configured or updated depending on your platform.
2.3. Storage management[edit source]
TF-A BL2 needs to access storage to load the FIP binary. It will default use the boot device selected by boot pins or OTP.
This selected device needs to be properly setup:
- Device tree configuration (all devices)
- BL2 boot device configuration for Flash memories .
Each device support needs a specific framework in the BL2 firmware.
By default, STMicroelectronics chooses to select only one device support per binary. A BL2 full storage support could not fit with the SYSRAM size.
Storage build flags allow to configure the BL2 firmware to support the requested boot storage.
2.4. DDR[edit source]
TF-A BL2 needs to setup the DDR to load the next binaries. DDR settings come from device tree and need to be adapted by customer depending the DDR type, DDR configuration and boards. This can be done using STM32CubeMX DDR settings.
2.5. Clock management[edit source]
An initial clock tree as to be setup to allow access to DDR and external storage.
For performance benefits, it also allows to increase the default CPU speed and increase the storage transfer speeds.
2.6. Binary mapping[edit source]
Here is the TF-A BL2 with STM32 header layout.
The different size can be customized depending build options, device tree customization. All sizes can be changed in the platform definition file:
STM32MP1 platform uses plat/st/stm32mp1/stm32mp1_def.h .
- STM32MP_BL2_DTB_BASE : Device tree base address in SYSRAM with its associated SIZE
- STM32MP_BL2_RO_BASE: Define the start address where the code execution will be load and executed
- STM32MP_BL2_RW_BASE: Start address of read and write data used by code. It depends on the STM32MP_BL2_RO_SIZE. The STM32MP_BL2_RW_SIZE cannot exceed SYSRAM size.
2.7. BL2 load processing[edit source]
Based on FIP and firmware configuration files, the same BL2 is able to manage dynamically different binary configurations:
The BL2 process is executed as described:
- The ROM Code loads (and authenticates if required) the STM32 TF-A BL2 file with its device tree
- BL2 loads (and authenticates) FW_CONFIG file from FIP. BL2 parse the FW_CONFIG file to configure the binary to load.
- BL2 loads (and authenticates) all binaries listed in FW_CONFIG from FIP.
2.7.1. FW_CONFIG[edit source]
FW_CONFIG file is device tree based and allows to describe properties for binaries to be loaded. This file is mandatory in the FIP binary to configure dynamically BL2 that will properly load all images. It depends to the DDR size, defined mapping, choosen binaries. More details on FW_CONFIG and its configuration are details here.
2.7.2. BL2 load in programmer mode[edit source]
The programmer mode (USB or UART boot device) requires the complete FIP binary to start the load image process as previously explained.
This is achieved by loading the complete FIP binary into DDR before starting the normal boot sequence.
The FIP load address is fixed and must not override the next loaded address :
DWL_BUFFER_BASE used in plat/st/common/stm32_io_storage.c
2.7.3. Low power mode[edit source]
In case of low power exit, the BL2 will have to wake up DDR from self refresh and reload only binaries that have been lost.
.
2.8. Trusted boot support[edit source]
This feature is enabled by defining the TRUSTED_BOARD_BOOT build flag which is not default enabled.
As soon as the flag is enabled, authentication is enabled and certificates are mandatory into the FIP binary.
2.8.1. MBEDTLS[edit source]
Using FIP, X509.v3 certificates are embedded in the package to authenticate all loaded binaries. The certificate parser is done using MBEDTLS. The MBEDTLS[1] project is partially used during the trusted boot build process to retrieve part of the library to parse the certificate. The project needs to be downloaded closed to TF-A sources and defined the path using the MBEDTLS_DIR variable.
2.8.2. Dynamic authentication disable[edit source]
A DYN_DISABLE_AUTH flag can be used to build the full BL2 content (including the MDEBTLS files required) and allows to enable or disable authentication using a device tree property:
disable_auth = <0x0>; // To enable authentication disable_auth = <0x1>; // To bypass authentication
This device tree property is located in the BL2 device tree (trusted boot device tree).
2.8.3. Crypto Library[edit source]
STM32 MPU use its own cryptographic library (thanks to hardware accelerators or ROM Code services (STM32MP15 Only)) to verify certificate signatures: plat/st/common/stm32mp_crypto_lib.c
2.8.4. Keys[edit source]
Authentication is based on different keys and certificates. The Arm TBBR CoT is used by default and topology is defined in the BL2 device tree fdts/cot_descriptors.dtsi and can be customized by used <link here to authentication article>.
STM32 MPU use the default public root key hash in OTP as main root key for the CoT.
It can be redefined by customer in device tree redefining pkh_otp.
During development, the ROTPK hash is not mandatory. If not fused in OTP, it will be seen as NOT DEPLOYED and the final ROTPK hash control will be bypass. But the entire CoT will be verified.
3. Source code access and build process[edit source]
Cross compilation of TF-A BL2 is only required if it is to be modified.
By default, in the Starter Package, the TF-A BL2 images are named: tf-a-<board>-<storage>.stm32.
If changes are made, you must rebuild TF-A and update all the FSBL partitions of your boot device with this new image. A second FSBL image is used by ROM code as a backup image in case of corruption.
The build process creates a STM32 image. This binary is built in a single step during the build process.
4. Developer Package[edit source]
4.1. Install sources[edit source]
The Developer Package contains OpenSTLinux and TF-A sources: TF-A Installation
4.2. Official source tree[edit source]
Download source code from the official Trusted Firmware-A github.
git clone https://github.com/ARM-software/arm-trusted-firmware.git
For a full feature software, a STMicroelectronics github is available:
git clone https://github.com/STMicroelectronics/arm-trusted-firmware.git
4.3. Build Process[edit source]
4.3.1. Initialize the cross compile environment[edit source]
Setup Cross compile environment
4.3.2. TF-A Build flags[edit source]
Here is the list of the mandatory flags that needs to be specify to complete the TF-A BL2 build:
- ARM_ARCH_MAJOR=7: the major version of ARM Architecture to target (STM32MP1 is ARMv7 architecture based)
- ARCH=aarch32: specify aarch32 architecture to be built
- PLAT=stm32mp1: builds an stm32mp1 platform
- DTB_FILE_NAME=<fdt file name>.dtb: this must be defined to build the proper target and include the correct DTB file into the final file
- The boot device(s) you use, one (or more) of:
- STM32MP_EMMC=1
- STM32MP_SDMMC=1
- STM32MP_RAW_NAND=1
- STM32MP_SPI_NAND=1
- STM32MP_SPI_NOR=1
- Or a programming interface:
- STM32MP_UART_PROGRAMMER=1
- STM32MP_USB_PROGRAMMER=1
Optional flags:
- DEBUG=1: add debug information in all binaries
- V=1: print verbose compilation traces
- TRUSTED_BOARD_BOOT=1: add MBEDTLS build sources and authentication framework enabled
- DYN_DISABLE_AUTH=1: Allow to enable/disable authentication using device tree
- STM32MP_FORCE_MTD_START_OFFSET= <value>: Override the default start offset to read FIP on MTD devices (need to be aligned with FlashLayout).
- STM32MP_USE_EXTERNAL_HEAP=1: Can be enabled to define MBEDTLS heap out of BL2 sources (defined in device tree).
4.4. Build command[edit source]
As previously explained, the BL2 generation depends on selected storage, default is to only support one storage.
You must add your own environment flags:
unset LDFLAGS; unset CFLAGS;
Then you will have to compile the TF-A BL2.
To avoid binary override, it is recommended to specify BUILD_PLAT per selected storage.
The default build command for STM32MP15 is
make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \
<Selected storage> DTB_FILE_NAME=<board_name>.dtb BUILD_PLAT=build/<storage>
Here are build commands for the stm32mp157c-ev1 board (which support different storage):
- Flash programming support
make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_USB_PROGRAMMER=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb BUILD_PLAT=build/usb make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_UART_PROGRAMMER=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb BUILD_PLAT=build/uart
- Dedicated boot storage
make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 {{STM32MP_SDMMC=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb BUILD_PLAT=build/sdmmc
make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_EMMC=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb BUILD_PLAT=build/emmc
make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_RAW_NAND=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb BUILD_PLAT=build/raw_nand
make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_SPI_NOR=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb BUILD_PLAT=build/spi_nor
Not available on board
make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_SPI_NAND=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb BUILD_PLAT=build/spi_nand
From the Developer Package tarball, a Makefile.sdk is present and must be used to build the target.
It automatically sets the proper configuration for the TF-A build.
make -f Makefile.sdk TF_A_CONFIG=<to be completed>
The latest version of the helper file is also available in GitHub: README_HOWTO.txt .
4.5. Final image[edit source]
Final image is available for Flash or SD card update in the corresponding folder:
<BUILD_PLAT>/<target>/tf-a-<target>.stm32 Ex: build/sdmmc/stm32mp157c-ev1/tf-a-stm32mp157c-ev1.stm32
5. Distribution Package[edit source]
For an OpenSTLinux distribution, the TF-A image is built in release mode by default. The yocto recipe can be found in:
meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_<version>.bb
If you want to modify the TF-A BL2 code source, use the following steps starting from an already downloaded and built OpenSTLinux distribution.
5.1. Access sources[edit source]
You can use devtool to access the source.
cd <baseline root directory> devtool modify tf-a-stm32mp sources/boot/tf-a
By going to the sources/boot/tf-a folder, you can manage and modify the TF-A sources. To rebuild it, go back to the build-<distribution> folder and launch the TF-A recipe:
bitbake tf-a-stm32mp
The final image is deployed in the image default output folder.
6. Update software on board[edit source]
6.1. Partitioning of binaries[edit source]
The TF-A build provides a binary named tf-a-stm32mp157c-<board>.stm32 (or tf-a-stm32mp157c-<board>-storage.stm32 from Makefile.sdk) that MUST be copied to a dedicated partition named "fsblX" (X depends on the number of needed backups in the Flash).
6.2. Update via SDCARD[edit source]
If you use an SD card, you can simply update TF-A using the dd command on your host.
Plug your SD card into the computer and copy the binary to the dedicated partition; on an SDCard/USB disk the "fsbl1" partition is partition 1:
- SDCARD: /dev/mmcblkXp1 (where X is the instance number) - SDCARD via USB reader: /dev/sdX1 (where X is the instance number)
- Linux
dd if=<tf-a file>.stm32 of=/dev/<device partition> bs=1M conv=fdatasync
- Windows
CoreUtils [2] that includes the dd command is available for Windows.
6.3. Update via USB mass storage on U-boot[edit source]
See How to use USB mass storage in U-Boot
Follow the previous section to put tf-a-<board>-<storage>.stm32 onto SDCard/USB disk
6.4. Update your boot device via STM32CubeProgrammer[edit source]
Refer to the STM32CubeProgrammer documentation to update your target.
7. Secure secret provisioning[edit source]
STM32 MPU support SSP feature. One part of this feature is based on TF-A BL2.
- Exchange with STM32_CubeProgrammer
- Program OTPs
A specific TF-A BL2 build is required to manage SSP.
Dedicated files are delivered in the platform folder that contains the specific Makefile and bl2_plat_setup for the TF-A SSP.
The TF-A SSP is a subset part of the standard TF-A BL2 that only includes:
- BL2 device tree
- BL2 image with limited support to the serial link device.
7.1. Developer Package[edit source]
7.1.1. Install sources[edit source]
The Developer Package contains OpenSTLinux and TF-A-SSP sources: TF-A-SSP Installation
7.1.2. Additional Flags[edit source]
Mandatory flags to build the TF-A SSP are:
- STM32MP_SSP=1
For the serial link (exclusive)
- STM32MP_UART_PROGRAMMER=1
- STM32MP_USB_PROGRAMMER=1
7.1.3. Build command[edit source]
make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_SSP=1 STM32MP_USB_PROGRAMMER=1 \ DTB_FILE_NAME=<board>.dtb BUILD_PLAT=build/ssp_usb
or
make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_SSP=1 STM32MP_UART_PROGRAMMER=1 \ DTB_FILE_NAME=<board>.dtb BUILD_PLAT=build/ssp_uart
7.1.4. Final image[edit source]
Final image is available in the corresponding folder:
<BUILD_PLAT>/<target>/tf-a-ssp-<target>.stm32 Ex: build/ssp_usb/stm32mp157c-ev1/tf-a-ssp-stm32mp157c-ev1-usb.stm32
7.2. Distribution Package[edit source]
For an OpenSTLinux distribution, the TF-A SSP image is not built in release mode by default. The yocto recipe can be found in:
meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp-ssp_<version>.bb
If you want to modify the TF-A SSP code source, use the following steps starting from an already downloaded and built OpenSTLinux distribution.
7.2.1. Access sources[edit source]
You can use devtool to access the source.
cd <baseline root directory> devtool modify tf-a-stm32mp-ssp sources/boot/tf-a_ssp
By going to the sources/boot/tf-a_ssp folder, you can manage and modify the TF-A sources. To rebuild it, go back to the build-<distribution> folder and launch the TF-A recipe:
bitbake tf-a-stm32mp-ssp
The final image is deployed in the image default output folder.