![]() |
This page is a candidate for renaming (move). The requested new name is: How to manually update bootloaders . The supplied reason is: not only update U-Boot but also T-FA / FIP (OP-TEE) . -- Patrick Delaunay. Wiki maintainers: remember to update the pages that link this page before renaming (moving) it. |
This page explains how to manually update the bootloaders binary (including U-Boot and TF-A) on an SD card or on the e•MMC.
1. To update an SD card with the Linux dd command[edit source]
When a Linux console has access to the SD card device partitions:
- on a Linux PC
- with a card reader of this PC
- through a USB connection to the target and the
ums
command executed on a U-Boot console
- on target, with Linux console.
The 3 first GPT partitions on the SD card are:
- FSBL1
- FSBL2
- FIP
See Boot_chain_overview for the bootloader definitions.
You can use the Linux dd
command to copy the FSBL and SSBL directly to the correct partition:
dd if=<file> of=/dev/<dev> conv=fdatasync
<dev> is:
- mmcblk<X>p<n>: PC-embedded card reader case or target Linux console
- sd<X><n>: USB-connected SD card reader case
where <X> is the ID of the device, and <n> the ID of the partition.
Note: the dd option conv=fdatasync is used to force synchronous copying.
1.1. U-Boot environment[edit source]
The U-Boot environment is saved at the end of the U-Boot partition, named "fip": ID = 3.
To clear this environment, erase the U-Boot partition before any update; for example, by writing 0 to this partition:
dd if=/dev/zero of=/dev/mmcblk<X>p3 conv=fdatasync
dd if=/dev/zero of=sd<X>3 conv=fdatasync
1.2. SD card update example[edit source]
The internal card reader is /dev/mmcblk0 or for a target Linux console, GPT partition <n> is /dev/mmcblk0p<n>:
dd if=tf-a-sdcard.stm32 of=/dev/mmcblk0p1 conv=fdatasync dd if=tf-a-sdcard.stm32 of=/dev/mmcblk0p2 conv=fdatasync dd if=/dev/zero of=/dev/mmcblk0p3 conv=fdatasync dd if=fip.bin of=/dev/mmcblk0p3 conv=fdatasync
Alternatively, with U-Boot console, dev = 0 (SD card device on ST Microelectronics board), GPT partition <n> is /dev/sda<n>:
mmc dev 0 ums 0 mmc 0 dd if=tf-a-sdcard.stm32 of=/dev/sda1 conv=fdatasync dd if=tf-a-sdcard.stm32 of=/dev/sda2 conv=fdatasync dd if=/dev/zero of=/dev/sda3 conv=fdatasync dd if=fip.bin of=/dev/sda3 conv=fdatasync
1.3. SD card update example with SPL as FSBL[edit source]
The USB card reader is /dev/sdb, GPT partition <n> is /dev/sdb<n>:
dd if=u-boot-spl.stm32 of=/dev/sdb1 conv=fdatasync dd if=u-boot-spl.stm32 of=/dev/sdb2 conv=fdatasync dd if=/dev/zero of=/dev/sdb3 conv=fdatasync dd if=u-boot.img of=/dev/sdb3 conv=fdatasync
2. Update of e•MMC with the Linux dd command[edit source]
The same command, dd
, can be used to update e•MMC memory mapping:
- SSBL U-Boot is the first GPT partition in the e•MMC user area
- FSBL = TF-A (or SPL) is saved at the beginning of the e•MMC boot partition
The user needs to select the e•MMC hardware partition to update: user data, boot1, or boot2.
2.1. On a Linux console[edit source]
If dev = mmcblk1 for e•MMC device (default on ST Microelectronics board)
The boot partitions are available in /dev/mmcblk1boot0 and /dev/mmcblk1boot1 [1].
The user perhaps needs to allow access, for example with:
echo 0 > /sys/class/block/mmcblk1boot0/force_ro
The mmc tools allow the boot partition to be selected [2].
The STM32MP15x ROM code requires:
- <send_ack> =1
- the eMMC boot configuration is: 1 wire configuration and 25 MHz, it is done with the command:
mmc bootbus set single_backward x1 x1 dev/mmcblk1
To update TF-A in boot1 and select this boot partition:
dd if=tf-a-emmc.stm32 of=/dev/mmcblk1boot0 conv=fdatasync mmc bootpart enable 1 1 /dev/mmcblk1
To update TF-A in boot2 and select this boot partition:
dd if=tf-a-emmc.stm32 of=/dev/mmcblk1boot1 conv=fdatasync mmc bootpart enable 2 1 /dev/mmcblk1
To update U-Boot in the first GPT partition:
dd if=/dev/zero of=/dev/mmcblk1p1 conv=fdatasync dd if=fip.bin of=/dev/mmcblk1p1 conv=fdatasync
See also [3].
2.2. On a U-Boot console[edit source]
The e•MMC update is done with the ums
command and
the targeted e•MMC HW partition is selected in U-Boot by the third parameter partition_access of command mmc partconf
:
- 0: user data partition
- 1: boot partition 1
- 2: boot partition 2
help mmc
...
mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
- Set the BOOT_BUS_WIDTH field of the specified device
mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
- Change sizes of boot and RPMB partitions of specified device
mmc partconf dev [boot_ack boot_partition partition_access]
- Show or change the bits of the PARTITION_CONFIG field of the specified device
For example:
* dev = 1 (e•MMC device on ST Microelectronics board) * boot_ack=1 (Boot Acknowledge is needed by ROM code) * boot_partition = 1 (Boot partition 1 enabled for boot) * partition_access = 0 (No access to boot partition - default) * or partition_access = 1 (R/W boot partition 1)
And on a PC, the mass storage is mounted as /dev/sda
To update FSBL=TF-A, select the boot1 HW partition and come back to the user area at the end.
mmc dev 1 mmc partconf 1 1 1 1 ums 0 mmc 1 dd if=tf-a-emmc.stm32 of=/dev/sda conv=fdatasync mmc partconf 1 1 1 0
To update SSBL = U-Boot in the first GPT partition in the user partition
mmc dev 1 ums 0 mmc 1 dd if=fip.bin of=/dev/sda1 conv=fdatasync
Before the first boot, select the e•MMC correct boot configuration (1 wire, 25 MHz) with the command:
mmc bootbus 1 0 0 0
3. References[edit source]
Please refer to the following links for additional information: