This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion
Summary
Linux® kernel provides some user space tools that can be used for testing the IIO subsystem.
1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the IIO user space tools that comes with the Linux® kernel
- provide a few examples using these tools
2. Introduction[edit source]
These tools use IIO sysfs and character device directly without libiio (See IIO user space interface for further details).
3. Tools[edit source]
The Linux® kernel provides the following IIO user space tools:
- lsiio: example application that provides a list of IIO devices and triggers.
root@stm32mp1:~# lsiio Device 001: 48003000.adc:adc@100 Device 000: 48003000.adc:adc@0 Trigger 018: tim3_ch4 Trigger 007: tim1_ch3 ...
- iio_event_monitor: example application that reads events from an IIO device and prints them.
See How to get ADC analog watchdog events.
root@stm32mp1:~# iio_event_monitor /dev/iio:device0 & Event: time: 1529352199639112110, type: voltage, channel: 0, evtype: thresh, direction: either Event: time: ...
- iio_generic_buffer: example application that reads data from buffer.
- iio_utils: set of routines built-in above IIO tools, typically used to access sysfs files.
4. Source code[edit source]
The Linux® kernel IIO tools source code can be found under tools/iio[1] directory:
- tools/iio/lsiio.c
- tools/iio/iio_event_monitor.c
- tools/iio/iio_generic_buffer.c
- tools/iio/iio_utils.c
5. Installation on your target[edit source]
The Linux® kernel IIO tools are embedded by default in OpenSTLinux distribution.