IO expander hardware components

Revision as of 10:47, 10 November 2021 by Registered User (Nathalie Sangouard moved page IO expanders hardware components to IO expander hardware components without leaving a redirect: Souade/ADE/NSA : Correction for expander in singular .)
Renaming.png This page is a candidate for renaming (move).
The requested new name is: IO expander hardware components .
The supplied reason is: Correction for expander in singular .
-- Registered User (-) 15:39, 8 November 2021 (CET).
Wiki maintainers: remember to update the pages that link this page before renaming (moving) it.

1. Article purpose[edit source]

The purpose of this article is to:

  • list the I/O expander hardware components that might be integrated in the different STM32MPU boards
  • link these components to the corresponding software framework(s)
  • point to the datasheet(s) of these components
  • explain, when necessary, how to configure these components

2. Software frameworks[edit source]

Domain Peripheral Software components Comment
OP-TEE Linux STM32Cube
Core/I/Os ST MFX (Multi-Function eXpander) Linux IOs pins overview I/O expander

3. ST MFX (Multi-Function eXpander)[edit source]

The ST MFX is an STM32L152 slave controller whose firmware embeds an I/O expander feature with 16 GPIOs + 8 GPIOs extra if other features (resistive touchscreen controller and IDD measurement) are not enabled.

For details, refer to UM2535, chapter MFX IO expander.

3.1. Linux driver[edit source]

Bindings: Documentation/devicetree/bindings/mfd/st,stmfx.yaml

Sources: