1. Article purpose[edit source]
The purpose of this article is to explain how to configure a USB remote server with an STM32MP157x-DKx board used as an example, managed by Linux® on the Arm® Cortex®-A7 processor.
The goal is to transform an STM32MP157x-DKx board into a USB remote server, and then manage a USB device from a PC while the USB device is connected to a remote server on the network.
USBIP kernel modules are used to configure an STM32MP157x-DKx board as a USB remote server.
This article provides step-by-step instructions to:
- explain how to transform a Linux® board into a USB remote server with USBIP kernel modules and server
- configure Linux® software to enable the USBIP server (aka USB remote server)
- configure a PC client to connect to the USBIP server.
- further manage power for the USB device on the server using the uhubctl tool
2. Configure an STM32 MPU board with USBIP[edit source]
2.1. Overview[edit source]
As explained on the USB/IP Project webpage, the USB/IP Project aims to develop a general USB device sharing system over IP network. To share USB devices between computers with their full functionality, USB/IP encapsulates "USB I/O messages" into TCP/IP payloads and transmits them between computers. [1]
2.2. Step by step on server[edit source]
The installation of a USBIP server is made on boards with embedded Linux®.
The following chapter shows how to configure manually the USBIP service on board and how to enable it on an STM32 MPU board on which all the configurations, files, and services are present.
2.2.1. Manual setup[edit source]
Before using the usbip command, it is necessary to load the kernel modules associated to USBIP:
modprobe usbip-core modprobe usbip-host
Start the USBIP server:
usbipd -D
To make available a USB device connected to a board with embedded Linux®, it is necessary to bind the device.
List the available USB devices:
usbip list -l - busid 2-1.1 (03f0:e207) HP, Inc : unknown product (03f0:e207)
Bind this specific device to be visible by the PC client (here device 2-1.1):
usbip bind -b 2-1.1
(To automate the binding of new USB devices, see the next section Automated setup.)
2.2.2. Automated setup (available by default on STM32 MPU boards)[edit source]
All the configurations, files, services are present on STM32 MPU boards by default.
- Automate server startup via systemd:
Create on board a service dedicated to start the USBIP server.
Content of /lib/systemd/system/usbip.service:
[Unit]
Description=USB-IP Bindind
After=network.target
Wants=network.target
[Service]
Type=forking
ExecStartPre=-/sbin/modprobe usbip-core
ExecStartPre=-/sbin/modprobe usbip-host
ExecStart=/usr/sbin/usbipd -D
ExecStop=/usr/sbin/stm32mp-usbip-bind-unbind.sh unload
[Install]
WantedBy=multi-user.target
Start systemd USBIP service:
systemctl daemon-reload systemctl start usbip
- Automate the binding of new USB devices:
The binding of new USB devices can be made by a script, which binds or unbinds the usb devices depending if they are plugged or unplugged.
This script must be called by an udev rules for the case of device plug/unplug.
Content of script: /usr/sbin/stm32mp-usbip-bind-unbind.sh:
#!/bin/sh -
#echo "Parameter number $#" >> /tmp/usbip.log
action=$1
devpath=$2
#echo "Parameter: $1" >> /tmp/usbip.log
#echo "Parameter: $2" >> /tmp/usbip.log
case $1 in
unload)
modprobe -r usbip-core
modprobe -r usbip-host
kill -9 `pgrep usbipd`
exit 0
;;
esac
subpath=$(echo $2 | sed "s|.*/\([^/]*\)|\1|")
#echo "subpath >$subpath<" >> /tmp/usbip.log
if $(echo $subpath | grep -q ":");
then
#echo "No valid path" >> /tmp/usbip.log
exit 0
fi
# if usbip-core are not loaded, do nothing
if [ -z "$(cat /proc/modules | grep usbip_core)" ]; then
#echo "no module usbip_core loaded" >> /tmp/usbip.log
exit 0
fi
case $1 in
add)
#echo ">>> bind $subpath" >> /tmp/usbip.log
usbip bind -b $subpath
;;
remove)
#echo "<<< unbind $subpath" >> /tmp/usbip.log
usbip unbind -b $subpath
;;
esac
Content of udev rules: /etc/udev/rules.d/99-usb-usbip.rules:
ACTION=="remove", SUBSYSTEM=="usb", RUN+="/usr/sbin/stm32mp-usbip-bind-unbind.sh remove %p"
ACTION=="add", SUBSYSTEM=="usb", DRIVER=="usb", RUN+="/usr/sbin/stm32mp-usbip-bind-unbind.sh add %p"
2.3. Step by step on PC client[edit source]
2.3.1. On Windows®[edit source]
A USBIP client exists for Windows®. It is available via GitHub usbip-win.
2.3.1.1. Installation[edit source]
Follow the instructions specified on README.md.
2.3.1.2. Usage[edit source]
User action:
- List the USB devices available on the specific server:
usbip.exe list -l -r <usbip server ip>
- Attach a USB device available on the specific server (here 2-1):
usbip.exe list -r <usbip server ip> -b 2-1
- List USB devices attached on the host PC:
usbip.exe port
- Detach a specific attached USB device from the host PC:
List attached device on the host PC and detach it (here 00): usbip detach -p 00
2.3.2. On Linux®[edit source]
2.3.2.1. Installation[edit source]
On Ubuntu®, it is necessary to install some pre-requisite package:
sudo apt-get install sysfsutils libwrap0-dev libglib2.0-dev libtool automake autoconf pkg-config linux-tools-generic
For having a translation of USB device name and ID, insatll a specific hardware data base:
wget http://www.linux-usb.org/usb.ids sudo mkdir -p /usr/share/hwdata/ sudo cp usb.ids /usr/share/hwdata/
2.3.2.2. Usage[edit source]
Before using the usbip command, load the kernel modules associated to USBIP:
sudo modprobe usbip-core modprobe vhci-hcd
- List USB remote devices available on the specific server:
sudo usbip list -r <server IP>
- Attach a USB remote device available on the specific server:
sudo usbip attach -r <server IP> -b <USB ID>
- Detach a specific attached USB device from the host PC:
List the attached USB devices:
sudo usbip port
Detach the specific USB device attached as 00:
sudo usbip detach -p 00
3. Configure the STM32 MPU board to add USB power management with uhubctl[edit source]
3.1. Overview[edit source]
uhubctl is the utility to control per-port USB power on smart USB hubs. A smart hub is defined as a hub that implements per-port power switching[2].
3.2. Usage[edit source]
uhubctl Current status for hub 2-1 [0424:2514] Port 1: 0507 power highspeed suspend enable connect [03f0:e207 Hewlett Packard HP Webcam HD 2300] Port 2: 0100 power Port 3: 0100 power Port 4: 0100 power Current status for hub 2 [1d6b:0002 Linux 5.9.0-rc4 ehci_hcd EHCI Host Controller 5800d000.usbh-ehci] Port 1: 0503 power highspeed enable connect [0424:2514] Port 2: 0100 power Current status for hub 1 [1d6b:0002 Linux 5.9.0-rc4 dwc2_hsotg DWC OTG Controller 49000000.usb-otg] Port 1: 0000 off
On hub 2-1 Port 1, a USB webcam is plugged:
cat /sys/class/video4linux/video1/name HP Webcam HD 2300: HP Webcam HD
To power off the USB webcam connected on this port:
uhubctl -a off -p 1 -l 2-1 Current status for hub 2-1 [0424:2514] Port 1: 0507 power highspeed suspend enable connect [03f0:e207 Hewlett Packard HP Webcam HD 2300] Sent power off request New status for hub 2-1 [0424:2514] Port 1: 0000 off uhubctl Current status for hub 2-1 [0424:2514] Port 1: 0503 power highspeed enable connect [03f0:e207] Port 2: 0100 power Port 3: 0100 power Port 4: 0100 power Current status for hub 2 [1d6b:0002 Linux 5.9.0-rc4 ehci_hcd EHCI Host Controller 5800d000.usbh-ehci] Port 1: 0503 power highspeed enable connect [0424:2514] Port 2: 0100 power Current status for hub 1 [1d6b:0002 Linux 5.9.0-rc4 dwc2_hsotg DWC OTG Controller 49000000.usb-otg] Port 1: 0000 off
To power on the USB webcam connected on this port:
uhubctl -a on -p 1 -l 2-1 Current status for hub 2-1 [0424:2514] Port 1: 0507 power highspeed suspend enable connect [03f0:e207 Hewlett Packard HP Webcam HD 2300] Sent power on request New status for hub 2-1 [0424:2514] Port 1: 0503 power highspeed enable connect [03f0:e207 Hewlett Packard HP Webcam HD 2300] uhubctl Current status for hub 2-1 [0424:2514] Port 1: 0507 power highspeed suspend enable connect [03f0:e207 Hewlett Packard HP Webcam HD 2300] Port 2: 0100 power Port 3: 0100 power Port 4: 0100 power Current status for hub 2 [1d6b:0002 Linux 5.9.0-rc4 ehci_hcd EHCI Host Controller 5800d000.usbh-ehci] Port 1: 0503 power highspeed enable connect [0424:2514] Port 2: 0100 power Current status for hub 1 [1d6b:0002 Linux 5.9.0-rc4 dwc2_hsotg DWC OTG Controller 49000000.usb-otg] Port 1: 0000 off
4. References[edit source]