How to integrate AWS IoT Greengrass on top of openSTLinux distribution

Revision as of 14:59, 26 November 2020 by Registered User (→‎AWS Greengrass target initialization)

1. Article purpose[edit source]

The purpose of this article is to explain how to integrate Amazon Web Service (AWS) IoT Greengrass [1] on top of OpenSTLinux, including the security part that enables the connection to a hardware security module (TPMv2.0).

This article explains step by step how to add the yocto "meta-st-stm32mpu-app-aws" layer on top of OpenSTLinux distribution, how to configure, build and install the image, how to execute the AWS Greengrass certification testing and configure the target for a secure connection with the AWS cloud.


2. Prerequisites[edit source]

Knowledge of the AWS IoT Greengrass and AWS cloud account configuration is required. Follow the process described in "AWS amazon site"[2].

2.1. Hardware prerequisites[edit source]

The process has been verified with the STM32MP157C-DK2 Discovery kit More info green.png and STM32MP157F-DK2 Discovery kit More info green.png.


  • STM32MP157C-DK2
STM32MP157C-DK2

For more information about this STM32 Discovery board and how to start using it, jump to section Getting started with STM32MP157x-DK2

  • STPM4RasPI Expansion board[3]
STPM4RasPI

The STPM4RasPI is an official Extension board to connect the ST33 TPM products to the Raspberry Pi® device. It is designed for development, proof of concept or demonstration activities. The board is shipped with one trusted platform module soldered, the ST33TPHF20SPI, that implement TPM V2.0 specification.

2.2. Software prerequisites[edit source]

The STM32MP1 Distribution Package must be installed on your host. The process has been verified with ecosystem release v2.0.0 of the OpenSTlinux distribution.

3. Software update with meta-st-stm32mpu-app-aws[edit source]

Info white.png Information
The meta-st-stm32mpu-app-aws is based on AWS Greengrass Core v1.10.1

.

Info white.png Information
The AWS IoT Device Tester for AWS IoT Greengrass used for certification testing is IDT v3.2.0

.

Info white.png Information
The TPM2 recipes are included in a meta-security layer. Some Amazon Greengrass functionalities require to add a "docker" and "Java-jdk" software components to the OpenSTLinux distribution.

The process has been validated with the following Yocto meta layers releases:

- "git://git.yoctoproject.org/meta-security" the commit "c74cc97641fd93e0e7a4383255e9a0ab3deaf9d7" on branch "dunfell".
- "git://git.yoctoproject.org/meta-java" the commit "2cf52b0f32712a0bd567b34a4fbb8f998abac638" on branch "dunfell".
- "git://git.yoctoproject.org/meta-virtualization" the commit "5c2de3daedd3f65171b9debf938683ce6e7746ea" on branch "dunfell".

1.Clone the following STMicroelectronics git repository

 cd [your STM32MP1 Distribution path]/layers/meta-st
 git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-app-aws.git
 cd meta-st-stm32mpu-app-aws 
 git checkout remotes/origin/dunfell



2. Add TPM2 recipes

 cd [your STM32MP1 Distribution path]/layers
 git clone git://git.yoctoproject.org/meta-security
 cd meta-security
 git checkout remotes/origin/dunfell


3.Setup the build environment

Execute the following command on the host:

cd [your STM32MP1 Distribution path]
DISTRO=openstlinux-weston MACHINE=stm32mp1-demo-aws source layers/meta-st/scripts/envsetup.sh

4.Enable TPM build

Apply the following patch in the file ([your STM32MP1 Distribution path]/layers/meta-st/meta-st-openstlinux/conf/distro/include/openstlinux.in)

DISTRO_FEATURES_append = " tpm2 "

5.Add Virtualization (docker) to the OpenSTLinux distribution

Execute the following command on the host:

cd [your STM32MP1 Distribution path]/layers
git clone git://git.yoctoproject.org/meta-virtualization
git checkout remotes/origin/dunfell
cd [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws
bitbake-layers add-layer [your STM32MP1 Distribution path]/layers/meta-virtualization

Update the file ([your STM32MP1 Distribution path]/layers/meta-st/meta-st-openstlinux/conf/distro/openstlinux-weston.conf)

DISTRO_FEATURES_append = "virtualization"

6.Add Java-jdk

To do this, follow the installation process described in the article How to install JAVA JDK.

7.Increase the Rootfs partition size

Update the file ([your STM32MP1 Distribution path]/ layers/meta-st/meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc)

IMAGE_ROOTFS_MAXSIZE = "2097152"


8.Build the image

Info white.png Information
By default the image is configured to include elements for the execution of the AWS greengrass certification testing.

If you do not need this feature, delete it from the image: In the file meta-st-stm32mpu-app-aws/recipes-st/images/st-image-demo-aws.bb, delete ${IMAGE_AWSGREENGRASSTEST_PART} in CORE_IMAGE_EXTRA_INSTALL definition.

In the folder ([your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws), execute the following command :

bitbake st-image-demo-aws

9.Flash the SDcard

Use the programmer tool STM32CubeProgrammer.

For example, the tsv file (FlashLayout_sdcard_ stm32mp157c-demo-aws-mx-trusted.tsv) is located in ([your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws/tmp-glibc/deploy/images/stm32mp1-demo-aws/flashlayout_st-image-demo-aws)

4. AWS Greengrass target initialization[edit source]

1. WiFi configuration

An internet connection is required on the target. Refer to the article How to setup wifi connection for how to configure and activate the WiFi in order to connect the target to your WiFi access point.

2.Configuration of the target

If extra target configurations are required, run the following scripts (to be executed only once after the first boot):

source /greengrass/tpm_update.sh

If the image has been configured for the execution of the AWS Greengrass certification testing:

source /greengrass/awsgreengrass_certif.sh

3.TPM token initialization

Info white.png Information
For the demonstration, keep the values of the PINs (123456) and the PKCS11 STORE folder (usr/local/pkcs11_tpm), since the scripts and Greengrass config file examples use these values.
Info white.png Information
If you faced the error ModuleNotFoundError: No module named 'pyasn1_modules', at the execution of the tpm2_ptool command, use Python pip application to install the missing module:

cd /usr/bin

pip3 install pyasn1_modules

Note: If something goes wrong, reset the TPM and PKCS11 store using the following commands:

cd /usr/bin
./tpm2_clear -Q
rm -rf /usr/local/pkcs11_tpm/*

Execute the commands below on the target:

cd /tools
./tpm2_ptool init --primary-auth=123456 --path=$TPM2_PKCS11_STORE
./tpm2_ptool addtoken --pid=1 --sopin=123456 --userpin=123456 --label=greengrass --path $TPM2_PKCS11_STORE
./tpm2_ptool addkey --algorithm=rsa2048 --label="greengrass" --userpin=123456 --key-label=greenkey --path=$TPM2_PKCS11_STORE

Verify the toke using pkcs11-tool (optional)

Execute the following command on the target to verify the token created.

pkcs11-tool --module /usr/lib/libtpm2_pkcs11.so.0 -L

Example of expected output:

Available slots:
   Slot 0 (0x1): greengrass STMicro
     token label        : greengrass
     token manufacturer : STMicro
     token model        :
    token flags        : login required, rng, token initialized, PIN initialized
     hardware version   : 1.38
     firmware version   : 74.8
     serial num         : 0000000000000000
     pin min/max        : 5/128

AT THIS STEP, THE CONFIGURATION OF THE BOARD IS COMPLETE AND READY TO BE USED:

5. Process to execute the AWS Greengrass certification testing[edit source]

1.Install the AWS IoT Device Tester.

  Go to the AWS Amazon site to [AWS IoT Device Tester for AWS IoT Greengrass Versions] [4]

2.Configure your ssh connection (ssh keys)

  Go to the AWS Amazon site to [Configure Your Host Computer to Access Your Device Under Test][5]

3.Configure the IDT

  Example of the install config folder for Windows.
  C:\devicetester_greengrass_win\devicetester_greengrass_win\configs\
  Go to the AWS Amazon site [Setting Configuration to Run the AWS IoT Greengrass Qualification Suite][6]
  There is a  IDT configuration file example installed on your Host :
  /[your STM32MP1 Distribution path]/layers/meta-st/meta-st-demo-aws/recipes-aws/greengrasstests/greengrasstests/device-hsm.json
  Note : With this example the certification tests are performed in Root.

4.Execute the tests

  Go to the AWS Amazon site to [Running Tests][7]

6. Process to create a Certificat Signature Request using the hardware-protected private key[edit source]

1.Update openssl configuration to use module tpm2_pkcs11

add the following lines in /etc/ssl/openssl.cnf at the beginning of the file (after "HOME = . ")

openssl_conf = openssl_init
[openssl_init]
engines=engine_section
[engine_section]
pkcs11 = pkcs11_section
[pkcs11_section]
engine_id = pkcs11
dynamic_path = /usr/lib/engines-1.1/pkcs11.so
MODULE_PATH = /usr/lib/libtpm2_pkcs11.so.0
init = 0

2. How to create a CSR "Certificat Signature Request" with openssl (Prerequisite : openssl installed) Executes the command, on target :

openssl req -engine pkcs11 -new -key "pkcs11:token=greengrass;object=greenkey;type=private;pin-value=123456" -keyform engine -out /usr/local/req.csr

This CSR "/usr/local/req.csr" is used to create clients certificats on the AWS amazon Cloud to store on the board.

There is a greengrass configuration file example to update with your AWS account parameter and certificats created, on the target : /greengrass/config/config_secu_example.json

You need also to download the root CA on Amazon site and stored it on the target greengrass/certs/root.ca.pem.

For more information about HSM (Hardware Secure Module) integration for AWS greengrass, go to AWS Amazon site [Hardware Security Integration][8]

3.Connection to Amazon cloud

Before starting the greengrass core on the target you need to set the TPM2_PKCS11_STORE environment variable.

Executes the commands on the target :

export TPM2_PKCS11_STORE=/usr/local/pkcs11_tpm
cd /greengrass/ggc/core/
./greengrassd start

7. References[edit source]