This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article gives information about the Linux® RTC framework. The RTC framework is involved in precise time countdown.
1. Framework purpose[edit source]
The RTC is used in standby mode to keep system time up to date or wake up system at programmed time.
A general presentation of the RTC framework is available in the Linux RTC documentation [1].
2. System overview[edit source]
File:Contributors:rtc overview.png