1. Article purpose[edit source]
The purpose of this article is to explain how to integrate Amazon Web Service (AWS) IoT Greengrass [1] on top of OpenSTLinux, included the security part with the connection to a Hardware Security Module (a TPMv2.0).
This article explains step by step how to add the yocto "meta-demo-aws" on top of OpenSTLinux distribution, to configure build and install the image, to execute the AWS greengrass certification testing and to configure the target for a secure connection with the AWS cloud.
2. Prerequisites[edit source]
You need some knowledge of the AWS IoT Greengrass, and to configure your AWS cloud account, follow the process described in "AWS amazon site"[2]
2.1. Hardware prerequisites[edit source]
The process has been verified withe the board STM32MP157C-DK2 Discovery kit and STM32MP157F-DK2 Discovery kit
.
- STM32MP157C-DK2
For more information about the STM32 discovery board and how to start it up, jump to this section Getting started with STM32MP157x-DK2
- STPM4RasPI expansion board[3]
The STPM4RasPI is an official extension board to connect the ST33 TPM products to the Raspberry Pi® device. It is designed for development, proof of concept or demonstration activities. The board is shipped with one trusted platform module soldered. The ST33 TPM device soldered is the ST33TPHF20SPI, it is a TPM V2.0 specification implementation.
2.2. Software prerequisites[edit source]
The STM32MP1 Distribution Package must be installed on your host. The process has been verified with the delivery ecosystem release v2.0.0 of the OpenSTlinux distribution.
3. Software update with meta-st-demo-aws[edit source]
1.Clone following git repository into [your STM32MP1 Distribution path]/layers/meta-st/
PC $>git clone ssh://${USER}@gerrit.st.com:29418/stm32mpuapp/meta/meta-st-stm32mpu-app-aws.git t PC $>cd meta-st-stm32mpu-app-aws PC $>git checkout MMDV_V200
2.Enable TPM build
Apply the following patch in the file [your STM32MP1 Distribution path]/layers/meta-st/meta-st-openstlinux/conf/distro/include/openstlinux.inc
DISTRO_FEATURES_append = " tpm2 "
3.Add Virtualization (docker) in the OpenSTLinux distribution
Executes the command, on the host :
cd [your STM32MP1 Distribution path]/layers git clone git://git.yoctoproject.org/meta-virtualization git checkout remotes/origin/dunfell bitbake add-layer [your STM32MP1 Distribution path]/layers/meta-virtualization
Update the file [your STM32MP1 Distribution path]/layers/meta-st/meta-st-openstlinux/conf/distro/openstlinux-weston.conf.
DISTRO_FEATURES_append = "virtualization"
4.Add Java-jdk
Follow the install process define in the article How to install JAVA JDK article.
5.Increase the Rootfs partition size
Update the file [your STM32MP1 Distribution path]/ layers/meta-st/meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc
#IMAGE_ROOTFS_MAXSIZE ?= "763904" IMAGE_ROOTFS_MAXSIZE = "2097152"
6.Setup the build environment
Executes the command, on the host :
cd [your STM32MP1 Distribution path] DISTRO=openstlinux-weston MACHINE=stm32mp1-demo-aws source layers/meta-st/scripts/envsetup.sh
7.Build the image
In the folder [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws Executes the command :
bitbake st-image-demo-aws
8.Flash the sdcard
Use the programmer tool STM32CubeProgrammer
For example ,the tsv file FlashLayout_sdcard_ stm32mp157c-demo-aws-mx-trusted.tsv is located in [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws/tmp-glibc/deploy/images/stm32mp1-demo-aws/flashlayout_st-image-demo-aws
4. AWS greengrass target initialization[edit source]
1.Configuration of the target
Run the scripts for some extra configuration on the target (to execute only one time after the first boot).
source /greengrass/tpm_update.sh
If the image has been configured for the execution of the AWS greengrass certification testing.
source /greengrass/awsgreengrass_certif.sh
2.TPM token initialization
Note : if something goes wrong, you can reset the TPM and PKCS11 store with the following commands :
cd /usr/bin ./tpm2_clear -Q rm -rf /usr/local/pkcs11_tpm/*
Executes the commands, on the target :
cd /tools ./tpm2_ptool init --primary-auth=123456 --path=$TPM2_PKCS11_STORE ./tpm2_ptool addtoken --pid=1 --sopin=123456 --userpin=123456 --label=greengrass --path $TPM2_PKCS11_STORE ./tpm2_ptool addkey --algorithm=rsa2048 --label="greengrass" --userpin=123456 --key-label=greenkey --path=$TPM2_PKCS11_STORE
OPTIONAL : Verifications with pkcs11-tool
Executes this command on the target to verify the token created.
pkcs11-tool --module /usr/lib/libtpm2_pkcs11.so.0 -L
Example of output expected :
Available slots: Slot 0 (0x1): greengrass STMicro token label : greengrass token manufacturer : STMicro token model : token flags : login required, rng, token initialized, PIN initialized hardware version : 1.38 firmware version : 74.8 serial num : 0000000000000000 pin min/max : 5/128
AT THIS STEP, THE CONFIGURATION OF THE BOARD IS COMPLETED TO BE USED :
- With AWS IoT Device Tester to perform the AWS greengrass certification testing, see the paragraph Process to execute the AWS Greengrass certification testing
- For a secure connection with AWS cloud, see the paragraph Process to create a Certificat Signature Request using the hardware-protected private key
5. Process to execute the AWS Greengrass certification testing[edit source]
1.Install the AWS IoT Device Tester.
Go to the AWS Amazon site to [AWS IoT Device Tester for AWS IoT Greengrass Versions] [4]
2.Configure your ssh connection (ssh keys)
Go to the AWS Amazon site to [Configure Your Host Computer to Access Your Device Under Test][5]
3.Configure the IDT
Example of the install config folder for Windows. C:\devicetester_greengrass_win\devicetester_greengrass_win\configs\
Go to the AWS Amazon site [Setting Configuration to Run the AWS IoT Greengrass Qualification Suite][6]
There is a IDT configuration file example installed on your Host : /[your STM32MP1 Distribution path]/layers/meta-st/meta-st-demo-aws/recipes-aws/greengrasstests/greengrasstests/device-hsm.json
Note : With this example the certification tests are performed in Root.
4.Execute the tests
Go to the AWS Amazon site to [Running Tests][7]
6. Process to create a Certificat Signature Request using the hardware-protected private key[edit source]
1.Install the tool openssl on the target.
The packages are stored on your Host :
/[your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws/tmp-glibc/deploy/deb/cortexa7t2hf-neon-vfpv4
package openssl-bin_1.1.1a-r0_armhf.deb (usr/bin/openssl) package openssl_1.1.1a-r0_armhf.deb (usr/lib/ssl-1.1/openssl.cnf ....; etc/ssl/certs and private folder) package openssl-conf_1.1.1a-r0_armhf.deb (/etc/ssl/openssl.cnf)
Execute the commands, on the Host (the board is connected to your internet network) :
scp openssl-bin_1.1.1a-r0_armhf.deb root@IP address of the board://root scp openssl_1.1.1a-r0_armhf.deb root@IP address of the board://root scp openssl-conf_1.1.1a-r0_armhf.deb root@IP address of the board://root
Execute the commands, on the target:
cd /root dpkg -i openssl-bin_1.1.1a-r0_armhf.deb dpkg -i openssl-conf_1.1.1a-r0_armhf.deb dpkg -i openssl_1.1.1a-r0_armhf.deb sync
2.Update openssl configuration to use module tpm2_pkcs11
add the following lines in /etc/ssl/openssl.cnf :
openssl_conf = openssl_init [openssl_init] engines=engine_section [engine_section] pkcs11 = pkcs11_section [pkcs11_section] engine_id = pkcs11 dynamic_path = /usr/lib/engines-1.1/pkcs11.so MODULE_PATH = /usr/lib/libtpm2_pkcs11.so.0 init = 0
3. How to create a CSR "Certificat Signature Request" with openssl (Prerequisite : openssl installed) Executes the command, on target :
openssl req -engine pkcs11 -new -key "pkcs11:token=greengrass;object=greenkey;type=private;pin-value=123456" -keyform engine -out /usr/local/req.csr
This CSR "/usr/local/req.csr" is used to create clients certificats on the AWS amazon Cloud to store on the board.
There is a greengrass configuration file example to update with your AWS account parameter and certificats created, on the target : /greengrass/config/config_secu_example.json
You need also to download the root CA on Amazon site and stored it on the target greengrass/certs/root.ca.pem.
For more information about HSM (Hardware Secure Module) integration for AWS greengrass, go to AWS Amazon site [Hardware Security Integration][8]
4.Connection to Amazon cloud
Before starting the greengrass core on the target you need to set the TPM2_PKCS11_STORE environment variable.
Executes the commands on the target :
export TPM2_PKCS11_STORE=/usr/local/pkcs11_tpm cd /greengrass/ggc/core/ ./greengrassd start
7. References[edit source]
- ↑ https://aws.amazon.com/fr/greengrass/
- ↑ https://docs.aws.amazon.com/greengrass/latest/developerguide/what-is-gg.html
- ↑ STPM4RasPI expansion board
- ↑ https://docs.aws.amazon.com/greengrass/latest/developerguide/dev-test-versions.html
- ↑ https://docs.aws.amazon.com/greengrass/latest/developerguide/device-config-setup.html#configure-host
- ↑ https://docs.aws.amazon.com/greengrass/latest/developerguide/set-config.html
- ↑ https://docs.aws.amazon.com/greengrass/latest/developerguide/run-tests.html
- ↑ https://docs.aws.amazon.com/greengrass/latest/developerguide/hardware-security.html