1. Article Purpose[edit source]
The purposes of this article is to explain how to secure an STM32 MPU-based platform thanks to several hardware mechanisms, and to briefly introduce the software components responsible for the secure configuration.
2. Introduction[edit source]
The STM32 MPU is based on the Arm® Cortex-A® core, which is based on the Arm® TrustZone[1] architecture that enables context isolation: the normal world holds the applications whereas the secure world isolates all the trusted applications and core secure services so that they can safely manipulate platform secret data. The MPU includes Firewall mechanisms that allow the secure world to forbid read/write accesses from the normal world to given peripherals.
Armv7 defines PL0, PL1 and PL2 privilege levels:
- PL0 is the lowest software execution level (unprivileged calls allowed for applications).
- PL1 is the execution level for the OS.
- PL1 (secure) is also the privilege level for secure monitor execution, to switch from the secure to the normal world.
- PL2 is dedicated to the hypervisor (only non-secure).
The normal world is used to run rich OSs such as Linux Kernel and its applications framework.
The secure world runs a secure monitor with minimal services (i.e TF-A) or a Secure and non-secure worlds as secure OS (i.e OP-TEE OS).
The secure boot is a key feature of this multiple execution contexts environment. It allows the boot chain to be authenticated by the ROM code as well as the authentication of the components that are launched in the secure and normal worlds.
The TrustZone environment is a complete system solution that is not limited to the Cortex context. It provides a bus and peripheral infrastructure to the MPU in order to ensure that the secure world relies on a completely secured pipe when it controls a secure peripheral. The assignment of the peripherals to a given world is done thanks to a Firewall mechanism, which is set up during the secure world initialization.
Dedicated secure and normal contexts also impact the debugging facilities: depending on the targeted user, the debug can be opened to both worlds (e.g. for a secure aware developer), to normal world only (for a Linux® developer) or completely closed (for the end user). This is achieved by configuring the Debug control.
Some internal or external peripherals can be used by the secure world to support cryptographic operations. Refer to security peripherals for an introduction.
3. Secure boot[edit source]
The secure boot is essential to ensure the integrity and security of the platform at runtime.
The STM32 MPU trusted boot chain was design to guarantee such a secure boot sequence.
It performs the following tasks:
- Configuration of the platform firewall, which is the foundation for a safe execution of the platform
- Configuration of the platform debug capabilities
- Verification of the integrity (thanks to a hash algorithm) and authentication (using asymmetric cryptography algorithms) of the started software components, including the Secure and non-secure worlds.
TF-A is the recommended open source bootloader. Its implementation supports the trusted boot and peripheral access control with firewall.
3.1. STM32MP1 secure boot[edit source]
STM32MP1 secure boot implementation is described in the STM32MP15 secure boot article.
4. Firewall[edit source]
MPU firewalls comprise access filters for MPU peripherals and subsystems memory mapped interfaces, internal RAMs/ROMs and external memory (DDR). Depending on the assignment, an MPU interface can be dedicated or shared between several hardware execution context(s).
4.1. STM32MP1 firmwalls[edit source]
- ETZPC:
- assigns access rights to MPU peripherals from Cortex-A7 contexts (secure or normal) and Cortex-M4 context.
- assigns access rights to internal ROM/RAM from Cortex-A7 and Cortex-M4.
- TZC: assigns access rights to DDR regions.
- RCC: can restrict the access of some of its registers to the secure execution context.
- PWR: can restrict the access of some of its registers to the secure execution context.
- BSEC: The OTP memory can be fused to restrict the access to some of its content to the secure execution context.
- RTC: This MPU interface can restrict some of its interface registers to the secure execution context.
- GPIO: GPIO bank Z can be configured to restrict some GPIO configuration to the secure execution context.
- TAMP: can restrict the access of some of its registers to the secure execution context.
- EXTI: can restrict the access of some of its registers to the secure execution context.
- GIC: can restrict the access of some of its registers to the secure execution context.
- MDMA: can configure MDMA interrupt execution context.
5. Secure debug[edit source]
The STM32 MPU offers the possibility to manage the platform debug configuration.
It is indeed possible to enable/disable independently secure and non-secure debug accesses.
5.1. STM32MP1 secure debug[edit source]
Debug accesses are controlled through BSEC peripheral.
By default, the STM32 MPU is started by the ROM code with both secure and non-secure debug enabled.
When the trusted boot is enabled, the ROM code disables debug accesses and relies on the FSBL to configure them.
6. Secure and non-secure worlds[edit source]
Thanks to Arm® TrustZone, some portions of the executing code can be assigned to a non-secure world or to secure world.
The secure world offers an isolated context to guarantee code and data integrity. Secure world can be used to build a Trusted Execution Environment (TEE) that runs in parallel with the rich OS and provides secure services.
Firmware and more generally software executing in secure world implicitly use the TrustZone(r) NS signal/bit to be granted access to a sensitive resource. Resources can be DDR locations, SoC periheral interfaces, SoC internal resources as clocks, debug facilites, amd more.
6.1. TF-A runtime services: SP_MIN[edit source]
The TF-A configuration supports the installation of a minimal runtime secure service provider and peripheral access control with firewall. Run time services provided by TF-A includes not restricted, PSCI controls, SCMI resources, some SiP & OEM SMCCC services for power states transition and other platform facilities.
6.2. OP-TEE OS runtime services[edit source]
The OP-TEE is recommended by STMicroelectronics as it is an open source TEE solution. The package provides additional secure services to the platform since it can host core secure services and run trusted applications. OP-TEE provides the same level of services as TF-A listed above: PSCI, SCMI, SiP & OEM SMCCC. On top of that, OP-TEE, as a TEE, provides services to execute trusted applications. It also embeds platform services for the non-secure world as random number generation.
7. Security frameworks[edit source]
The platform non-secure world accesses to specific resources using generic frameworks. These operations are used to managed overall systems and must be implemented inside the TEE.
7.1. PSCI[edit source]
PSCI[2] manages the power state of the CPU and the overall system. This framework is an Arm® generic implementation targeting CPU related power management services among which secondary CPUs boot up, dynamic addition and removal of CPUs, CPU idle management and system shutdown and reset.
7.1.1. STM32MP1 PSCI support[edit source]
Both TF-A and OP-TEE implement PSCI v1.0 [3] and offers standard services for:
- Core idle management
- Boot up for secondary boot core
- Dynamic addition and removal of cores
- System shutdown and reset
7.2. SCMI[edit source]
SCMI[4] specification defines a standard to access resources for power, performance and system management. This framework is an ARM® generic implementation.
Interfaces are designed for:
- Power domain management
- Performance management
- Clock management
- Sensor management
- Reset management
7.2.1. STM32MP1 SCMI support[edit source]
Both TF-A and OP-TEE implement SCMI v2.0 [5] in STM32MP1 to expose secure clock and reset controllers to non-secure world. Enabled STM32MP1 security hardening configurations make such resources reachable only from secure world in RCC despite the related peripheral may be assigned to non-secure world in ETZPC, hence an SCMI abstraction interface.
In STM32MP1, SCMI exposes resource for the peripheral interfaces listed below. Note that when a related device is assigned to secure world by system configuration (see How to assign an internal peripheral to a runtime context for further information), the SCMI controls, even if exposed, will not allow non-secure world to effectively access the resource.
</nowiki>}}
- SCMI exposes CRYP1 clock and controllers to non-secure world.
- SCMI exposes HASH1 clock and controllers to non-secure world.
- SCMI exposes RNG1 clock and reset controllers to non-secure world.
- SCMI exposes BSEC clock controller to non-secure world.
- SCMI exposes GPIOZ bank clock and reset controllers to non-secure world.
- SCMI exposes I2C4 and I2C6 clock and reset controllers to non-secure world.
- SCMI exposes SPI6 clock and reset controllers to non-secure world.
- SCMI exposes USART1 clock and reset controllers to non-secure world.
- SCMI exposes IWDG1 bus clock controller to non-secure world.
- SCMI exposes RTC clock controller to non-secure world.
- SCMI exposes MDMA reset controller to non-secure world.
- SCMI exposes MCU clock and reset controllers to non-secure world, used for coprocessor startup whether via Linux remoteproc framework or U-Boot bootloader.
In STM32MP1, SCMI also exposes some system clocks to the non-secure world. As these clocks may be shared by both secure and non-secure world, secure world handles both worlds requests on a clock controller to consolidate the related clock effective state.
- SCMI exposes internal root clocks LSI, HSI and CSI.
- SCMI exposes external root clocks LSE and HSE.
- SCMI exposes PLL output clocks PLL2Q, PLL2R, PLL3Q and PLL3R.
7.3. Platform SiP and OEM SMCCC services[edit source]
7.3.1. STM32MP1[edit source]
STM32MP1 embeds SiP and OEM SMCCC services for non-secure world to access low power transition facilities, clock calibration facilities, BSEC OTP access, possibly also some test facilities. Both TF-A and OP-TEE implement the same level of services aside possibly test facilities.
8. Security peripherals[edit source]
8.1. Cryptographic hardware acceleration[edit source]
The STM32 MPU embeds multiple peripherals for cryptographic acceleration:
8.2. Trusted platform module (TPM)[edit source]
The STM32 MPU can be associated to an external trusted platform module (TPM).
It provides secret data storage capabilities as well as cryptographic capabilities allowing to use them.
9. Secure Secret Provisioning[edit source]
The STM32 MPU allows to provision secrets in BSEC fuses in a secure way. This is the Secure Secret Provisioning (SSP) feature.
This feature is a secure process which runs between the software programmer (including a HSM), the ROM Code and a customized TF-A BL2. The security relies on the chip attestation and a package encryption exchange between the programmer and the STM32 MPU.
This feature is fully describes in a dedicated application note.
9.1. BSEC provisioning in STM32MP1[edit source]
The build process for the TF-A SSP firmware is described here.
10. References[edit source]
- ↑ https://www.arm.com/why-arm/technologies/trustzone-for-cortex-a
- ↑ https://developer.arm.com/architectures/system-architectures/software-standards/psci
- ↑ https://developer.arm.com/docs/den0022/latest
- ↑ https://developer.arm.com/architectures/system-architectures/software-standards/scmi
- ↑ https://developer.arm.com/docs/den0056/latest