1. Activation of traces in the Gcnano kernel driver[edit source]
Kernel driver sources are available.
In order to activate traces, 2 steps are required :
- activation of trace
- selection of the debugZone & setting of the trace level (depending on what traces are expected)
- regeneration of the module : galcore.ko
1.1. Step 1 : trace activation[edit source]
In the file hal/kernel/inc/gc_hal_types.h, define gcdDEBUG
#define gcdDEBUG gcdDEBUG_TRACE
1.2. Step 2 : selection of the debugZone & trace level setting[edit source]
In the file gcnano-driver/hal/kernel/gc_hal_kernel_debug.c
- search and update the init value of _debugZones variable.(default value is gcvZONE_NONE)
Possible values are listed below. OR should be done in order to activate several traces.
_debugZones Values | activated trace |
---|---|
gcvZONE_NONE | None |
gcvZONE_ALL | All |
gcvZONE_OS | OS |
gcvZONE_HARDWARE | HARDWARE |
gcvZONE_HEAP | HEAP |
gcvZONE_SIGNAL | SIGNAL |
gcvZONE_KERNEL | KERNEL |
gcvZONE_VIDMEM | VIDMEM |
gcvZONE_COMMAND | COMMAND |
gcvZONE_DRIVER | DRIVER |
gcvZONE_CMODEL | CMODEL |
gcvZONE_MMU | MMU |
gcvZONE_EVENT | EVENT |
gcvZONE_DEVICE | DEVICE |
gcvZONE_DATABASE | DATABASE |
gcvZONE_INTERRUPT | INTERRUPT |
gcvZONE_POWER | POWER |
List of define available here : gcnano-driver/hal/inc/gc_hal_base.h
- search and update the init value of _debugLevel variable.
possible values are :
gcvLEVEL_NONE |
gcvLEVEL_ERROR |
gcvLEVEL_WARNING |
gcvLEVEL_INFO |
gcvLEVEL_VERBOSE |
1.3. Step 3 : regeneration of the module[edit source]
bitbake gcnano-driver
copy the generated module galcore.ko on the target
2. Activation of traces in the Gcnano userland libraries[edit source]
First of all, redefine the symbolic links of the Gcnano libs in order to point on the debug version of the libs.
export GC_VERSION=6.2.4 cd /usr/lib rm libEGL.so ln -s libEGL.${GC_VERSION}.multi.debug.so libEGL.so rm libGAL.so ln -s libGAL.${GC_VERSION}.multi.debug.so libGAL.so rm libgbm.so ln -s libgbm.${GC_VERSION}.multi.debug.so libgbm.so rm libGLESv1_CM.so ln -s libGLESv1_CM.${GC_VERSION}.multi.debug.so libGLESv1_CM.so rm libGLESv2.so ln -s libGLESv2.${GC_VERSION}.multi.debug.so libGLESv2.so rm libGLSLC.so ln -s libGLSLC.${GC_VERSION}.multi.debug.so libGLSLC.so rm libOpenVG.so ln -s libOpenVG.${GC_VERSION}.multi.debug.so libOpenVG.so rm libVDK.so ln -s libVDK.${GC_VERSION}.multi.debug.so libVDK.so rm libVSC.so ln -s libVSC.${GC_VERSION}.multi.debug.so libVSC.so
Then, there are 2 methods to activate traces :
- Dynamic activation by usage of dedicated Vivante debug API
- Activation by setting of dedicated env variables (more complete) (not yet available in current BL)
2.1. Usage of dedicated Vivante debug API[edit source]
Primitive | Usage |
---|---|
gcoOS_SetDebugFile | open or close the debug dump file |
gcoOS_ReplaceDebugFile | replace the debug dump file to a new FILE pointer |
gcoOS_SetDebugLevel | sets the debug level |
gcoOS_GetDebugLevel | Retrieve the debug level |
gcoOS_SetDebugZone | Sets a single debug zone. A define is provided for each debug zone :
cf. driver/Khronos/libEGL/source/gc_egl.h
cf. driver/Khronos/libGLESv11/gc_glff_basic_defines.h
cf. driver/Khronos/libGLESv2/driver/gc_glsh.h (not available)
cf. driver/Khronos/libglesv3/include/chip/chip_base.h
cf. driver/hronos/libOpenVG_3D/vg11/driver/gc_vgsh_defs.h |
gcoOS_GetDebugZone | Retrieve the debug zone |
gcoOS_SetDebugZones | Enable or disable debug of multiple zones |
gcoOS_SetDebugLevelZone | Sets both the debug level and zone. |
Detailed description of this API is provided in the documentation : VIVANTE Debug API and Guide.
2.2. Setting of dedicated env variables[edit source]
2.2.1. Setting of debug level[edit source]
export LIBGAL_DEBUG_LEVEL=value
Possible value are :
-1 | No message |
0 | error debug info message |
1 | warning & error message |
2 | info, warning & error message |
3 | all debug info |
2.2.2. Filename definition of the debug file[edit source]
export LIBGAL_DEBUG_FILE=debug_trace.txt
2.2.3. Activation of the debug zone tracing[edit source]
Debug zone tracing can be activated for the following modules :
- EGL module
- ES11 module
- ES30 module (ES20 in also handled here)
- VG11
2.2.3.1. EGL module debug zones[edit source]
Activation of debug zones :
export LIBGAL_DEBUG_ZONE_EGL=value
value is OR result of the zone IDs listed below :
Zone | ID |
---|---|
API | (1 << 0) |
SURFACE | (1 << 1) |
CONTEXT | (1 << 2) |
CONFIG | (1 << 3) |
OS | (1 << 4) |
IMAGE | (1 << 5) |
SWAP | (1 << 6) |
INIT | (1 << 7) |
SYNC | (1 << 8) |
COMPOSE | (1 << 9) |
RENDER_THREAD | (1 << 10) |
Deactivation of all debug zones :
export LIBGAL_DEBUG_ZONE_EGL=
2.2.3.2. ES11 module debug zones[edit source]
Activation of debug zones :
export LIBGAL_DEBUG_ZONE_ES11=value
value is OR result of the zone IDs listed below :
Zone | ID |
---|---|
BUFFER | (1 << 0) |
CLEAR | (1 << 1) |
CLIP | (1 << 2) |
CONTEXT | (1 << 3) |
DRAW | (1 << 4) |
ENABLE | (1 << 5) |
EXTENTION | (1 << 6) |
FOG | (1 << 7) |
FRAGMENT | (1 << 8) |
LIGHT | (1 << 9) |
MATRIX | (1 << 10) |
PIXEL | (1 << 11) |
POLIGON | (1 << 12) |
LINE | (1 << 13) |
QUERY | (1 << 14) |
TEXTURE | (1 << 15) |
STATES | (1 << 16) |
STREAM | (1 << 17) |
VIEWPORT | (1 << 18) |
SHADER | (1 << 19) |
HASH | (1 << 20) |
TRACE | (1 << 21) |
Deactivation of all debug zones :
export LIBGAL_DEBUG_ZONE_ES11=
2.2.3.3. ES30 module debug zones[edit source]
Activation of debug zones :
export LIBGAL_DEBUG_ZONE_ES30=value
value is OR result of the zone IDs listed below :
Zone | ID |
---|---|
BUFFER | (1 << 0) |
CLEAR | (1 << 1) |
CLIP | (1 << 2) |
CONTEXT | (1 << 3) |
DRAW | (1 << 4) |
ENABLE | (1 << 5) |
EXTENTION | (1 << 6) |
FOG | (1 << 7) |
FRAGMENT | (1 << 8) |
LIGHT | (1 << 9) |
MATRIX | (1 << 10) |
PIXEL | (1 << 11) |
POLIGON | (1 << 12) |
LINE | (1 << 13) |
QUERY | (1 << 14) |
TEXTURE | (1 << 15) |
STATES | (1 << 16) |
STREAM | (1 << 17) |
VIEWPORT | (1 << 18) |
SHADER | (1 << 19) |
HASH | (1 << 20) |
TRACE | (1 << 21) |
Deactivation of all debug zones :
export LIBGAL_DEBUG_ZONE_ES30=
2.2.3.4. VG11 module debug zones[edit source]
Activation of debug zones :
export LIBGAL_DEBUG_ZONE_VG11=value
value is OR result of the zone IDs listed below :
Zone | ID |
---|---|
TRACE | (1 << 0) |
STATE | (1 << 1) |
FONT | (1 << 2) |
HARDWARE | (1 << 3) |
IMAGE | (1 << 4) |
MASK | (1 << 5) |
MATRIX | (1 << 7) |
PATH | (1 << 8) |
PAINT | (1 << 9) |
TESSELLATOR | (1 << 10) |
VGU | (1 << 11) |
Deactivation of all debug zones :
export LIBGAL_DEBUG_ZONE_VG11=
2.2.4. Debug by call stack[edit source]
2 parameters should be set :
- specification of modules that should be traces : dump API zones
- specification of call stack depth : dump API depth
Debug level should be also be set accordingly :
export LIBGAL_DEBUG_LEVEL=3
2.2.4.1. Setting of API dump zone[edit source]
export LIBGAL_DUMP_API_ZONES=value
value is the OR result of the following value :
Module | ID |
---|---|
Others | (1 << 0) |
HAL | (1 << 1) |
EGL | (1 << 2) |
ES11 | (1 << 3) |
ES20 | (1 << 4) |
VG11 | (1 << 5) |
GL | (1 << 6) |
DFB | (1 << 7) |
GDI | (1 << 8) |
D3D | (1 << 9) |
CL | (1 << 10) |
VX | (1 << 11) |
2.2.4.2. Setting of dump API depth[edit source]
In order to increase stack trace depth :
export LIBGAL_DUMP_API_DEPTH=2
Default value is 1.
2.3. Log redirection to terminal[edit source]
In order to see log in terminal, start weston with tty enabled:
weston --tty=1
Add before the wanted trace levels :
LIBGAL_DEBUG_LEVEL=3 LIBGAL_DEBUG_ZONE_EGL=255 LIBGAL_DUMP_API_ZONES=255 VIV_TRACE=1 weston --tty=1 &
Then launch your use-case
weston-simple-egl
When done kill weston which run in background:
kill %1
3. Activation of GLES API traces[edit source]
To activate traces :
export VIV_TRACE=1
To deactivate traces :
export VIV_TRACE=0