This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleProposedVersion
Touchscreen is more precise after a calibration, but this action is not mandatory.
Calibration data are erased after each firmware download into STMicroelectronics boards. The steps described below have to performed on a running board.
- Edit and change the value of the touchscreen_calibrator in the libinput section ot the weston.ini Weston configuration file[1]
vi /etc/xdg/weston/weston.ini [...] [libinput] touchscreen_calibrator=true calibration_helper=/bin/echo [...]
- Restart weston
systemctl restart weston
- List all the touchscreen devices
weston-touch-calibrator
could not load cursor 'dnd-move'
could not load cursor 'dnd-copy'
could not load cursor 'dnd-none'
device "/sys/devices/platform/soc/40012000.i2c/i2c-0/0-002a/input/input1/event1" - head "DSI-1"
- Launch calibration with the input of the touch panel
weston-touch-calibrator /sys/devices/platform/soc/40012000.i2c/i2c-0/0-002a/input/input1/event1
If the calibration succeeds, no message will be displayed on the console. If it fails, the following message will appear
weston-touch-calibrator error: Calibration verification failed, too large error.
Touchscreen identifier may vary, depending on the devices that are connected to the board. Recommendation is to unplug all the additional input devices before booting. Otherwise, it is up to You to adapt the command line.