1. Article purpose[edit source]
This article provides basic information needed to start using the Linux® kernel tool: perf[1].
2. Introduction[edit source]
The following table provides a brief description of the tool, as well as its availability depending on the software packages:
: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.
: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.
Tool | STM32MPU Embedded Software distribution | STM32MPU Embedded Softwaredistribution for Android™ | ||||||
---|---|---|---|---|---|---|---|---|
Name | Category | Purpose | Starter Package | Developer Package | Distribution Package | Starter Package | Developer Package | Distribution Package |
perf | Monitoring tools | perf[1] is a Linux user space tool, which allows getting system performance figures | ![]() |
![]() |
![]() |
![]() |
![]() |
![]() |
3. Installing the trace and debug tool on your target board[edit source]
3.1. Using the STM32MPU Embedded Software distribution[edit source]
perf is installed by default and ready to be used in all the STM32MPU Embedded Software Packages.
which perf /usr/bin/perf
It is integrated in the weston image distribution through openembedded-core package: openembedded-core/meta/recipes-core/packagegroups/packagegroup-core-tools-profile.bb.
RRECOMMENDS_${PN} = "\ ${PERF} \ trace-cmd \ blktrace \ ${PROFILE_TOOLS_X} \ ${PROFILE_TOOLS_SYSTEMD} \ " ... PERF = "perf"
4. Getting started[edit source]
4.1. Perf commands[edit source]
usage: perf [--version] [--help] [OPTIONS] COMMAND [ARGS] The most commonly used perf commands are: annotate Reads perf.data (created by perf record) and displays annotated code archive Creates archive with object files with build-ids found in perf.data file bench General framework for benchmark suites buildid-cache Manages build-id cache. buildid-list Lists the buildids in a perf.data file c2c Shared Data C2C/HITM Analyzer. config Gets and sets variables in a configuration file. data Data file related processing diff Reads perf.data files and displays the differential profile evlist Lists the event names in a perf.data file ftrace simple wrapper for kernel's ftrace functionality inject Filters to augment the events stream with additional information kallsyms Searches running kernel for symbols kmem Tool to trace/measure kernel memory properties kvm Tool to trace/measure kvm guest os list Lists all symbolic event types lock Analyzes lock events mem Profiles memory accesses record Runs a command and records its profile into perf.data report Reads perf.data (created by perf record) and displays the profile sched Tool to trace/measure scheduler properties (latencies) script Reads perf.data (created by perf record) and displays trace output stat Runs a command and gathers performance counter statistics test Runs sanity tests. timechart Tool to visualize total system behavior during a workload top System profiling tool. probe Defines new dynamic tracepoints See 'perf COMMAND -h' for more information on a specific command.
4.2. Most useful commands with simple to use interface[edit source]
- perf top (Linux kernel documentation[2]): provides the CPU load by counting the number of cycles events; the default order is descending the number of samples per symbol:
perf top 40.62% [kernel] [k] v7_dma_inv_range 18.65% [kernel] [k] _raw_spin_unlock_irqrestore 17.01% [kernel] [k] arch_cpu_idle 8.27% [kernel] [k] v7_dma_clean_range 5.00% [kernel] [k] rcu_idle_exit 1.70% [kernel] [k] cpu_startup_entry 0.52% [kernel] [k] trace_graph_return 0.48% [kernel] [k] finish_task_switch 0.48% libc-2.18.so [.] memcpy 0.47% [kernel] [k] trace_graph_entry
- Means that CPU is spending 40% of time in function v7_dma_inv_range, and 18.65% in _raw_spin_unlock_irqrestore.
- More information and examples are available in perf.wiki.kernel.org[3]
- This is also possible to display the result in a specified sorting:
Usage: perf top [<options>] -s, --sort <key[,key2...]> sort by key(s): pid, comm, dso, symbol, parent, cpu, srcline, ... Please refer to the main page for the complete list.
- perf stat (Linux kernel documentation[4]): obtains event counts
perf stat hello_world_example User space example: hello world from STMicroelectronics 10 9 8 7 6 5 4 3 2 1 0 User space example: goodbye from STMicroelectronics Performance counter stats for 'hello_world_example': 4.328249 task-clock (msec) # 0.000 CPUs utilized 11 context-switches # 0.003 M/sec 0 cpu-migrations # 0.000 K/sec 38 page-faults # 0.009 M/sec 2710036 cycles # 0.626 GHz 640856 instructions # 0.24 insn per cycle 75644 branches # 17.477 M/sec 21764 branch-misses # 28.77% of all branches 11.109859338 seconds time elapsed
- More information and examples are available in perf.wiki.kernel.org[5].
- perf list (Linux kernel documentation[6]): supported symbolic event types
perf list branch-instructions OR branches [Hardware event] branch-misses [Hardware event] bus-cycles [Hardware event] cache-misses [Hardware event] cache-references [Hardware event] cpu-cycles OR cycles [Hardware event] instructions [Hardware event] alignment-faults [Software event] bpf-output [Software event] context-switches OR cs [Software event] cpu-clock [Software event] cpu-migrations OR migrations [Software event] dummy [Software event] emulation-faults [Software event] major-faults [Software event] minor-faults [Software event] page-faults OR faults [Software event] task-clock [Software event] L1-dcache-load-misses [Hardware cache event] L1-dcache-loads [Hardware cache event] L1-dcache-store-misses [Hardware cache event] L1-dcache-stores [Hardware cache event] L1-icache-load-misses [Hardware cache event] L1-icache-loads [Hardware cache event] LLC-load-misses [Hardware cache event] LLC-loads [Hardware cache event] LLC-store-misses [Hardware cache event] LLC-stores [Hardware cache event] branch-load-misses [Hardware cache event] branch-loads [Hardware cache event] dTLB-load-misses [Hardware cache event] dTLB-store-misses [Hardware cache event] iTLB-load-misses [Hardware cache event] armv7_cortex_a7/br_immed_retired/ [Kernel PMU event] armv7_cortex_a7/br_mis_pred/ [Kernel PMU event] armv7_cortex_a7/br_pred/ [Kernel PMU event] armv7_cortex_a7/br_return_retired/ [Kernel PMU event] armv7_cortex_a7/bus_access/ [Kernel PMU event] armv7_cortex_a7/bus_cycles/ [Kernel PMU event] armv7_cortex_a7/cid_write_retired/ [Kernel PMU event] armv7_cortex_a7/cpu_cycles/ [Kernel PMU event] armv7_cortex_a7/exc_return/ [Kernel PMU event] armv7_cortex_a7/exc_taken/ [Kernel PMU event] armv7_cortex_a7/inst_retired/ [Kernel PMU event] armv7_cortex_a7/inst_spec/ [Kernel PMU event] armv7_cortex_a7/l1d_cache/ [Kernel PMU event] armv7_cortex_a7/l1d_cache_refill/ [Kernel PMU event] armv7_cortex_a7/l1d_cache_wb/ [Kernel PMU event] armv7_cortex_a7/l1d_tlb_refill/ [Kernel PMU event] armv7_cortex_a7/l1i_cache/ [Kernel PMU event] armv7_cortex_a7/l1i_cache_refill/ [Kernel PMU event] armv7_cortex_a7/l1i_tlb_refill/ [Kernel PMU event] armv7_cortex_a7/l2d_cache/ [Kernel PMU event] armv7_cortex_a7/l2d_cache_refill/ [Kernel PMU event] armv7_cortex_a7/l2d_cache_wb/ [Kernel PMU event] armv7_cortex_a7/ld_retired/ [Kernel PMU event] armv7_cortex_a7/mem_access/ [Kernel PMU event] armv7_cortex_a7/memory_error/ [Kernel PMU event] armv7_cortex_a7/pc_write_retired/ [Kernel PMU event] armv7_cortex_a7/st_retired/ [Kernel PMU event] armv7_cortex_a7/sw_incr/ [Kernel PMU event] armv7_cortex_a7/ttbr_write_retired/ [Kernel PMU event] armv7_cortex_a7/unaligned_ldst_retired/ [Kernel PMU event] rNNN [Raw hardware event descriptor] cpu/t1=v1[,t2=v2,t3 ...]/modifier [Raw hardware event descriptor] mem:<addr>[/len][:access] [Hardware breakpoint] alarmtimer:alarmtimer_cancel [Tracepoint event] alarmtimer:alarmtimer_fired [Tracepoint event] alarmtimer:alarmtimer_start [Tracepoint event] alarmtimer:alarmtimer_suspend [Tracepoint event] asoc:snd_soc_bias_level_done [Tracepoint event] asoc:snd_soc_bias_level_start [Tracepoint event] asoc:snd_soc_dapm_connected [Tracepoint event] asoc:snd_soc_dapm_done [Tracepoint event] asoc:snd_soc_dapm_path [Tracepoint event] asoc:snd_soc_dapm_start [Tracepoint event] asoc:snd_soc_dapm_walk_done [Tracepoint event] asoc:snd_soc_dapm_widget_event_done [Tracepoint event] asoc:snd_soc_dapm_widget_event_start [Tracepoint event] ... xhci-hcd:xhci_inc_enq [Tracepoint event] xhci-hcd:xhci_queue_trb [Tracepoint event] xhci-hcd:xhci_ring_alloc [Tracepoint event] xhci-hcd:xhci_ring_expansion [Tracepoint event] xhci-hcd:xhci_ring_free [Tracepoint event] xhci-hcd:xhci_setup_addressable_virt_device [Tracepoint event] xhci-hcd:xhci_setup_device [Tracepoint event] xhci-hcd:xhci_setup_device_slot [Tracepoint event] xhci-hcd:xhci_stop_device [Tracepoint event] xhci-hcd:xhci_urb_dequeue [Tracepoint event] xhci-hcd:xhci_urb_enqueue [Tracepoint event] xhci-hcd:xhci_urb_giveback [Tracepoint event]
- perf record (Linux kernel documentation[7]): records events for later reporting
perf record hello_world_example User space example: hello world from STMicroelectronics 10 9 8 7 6 5 4 3 2 1 0 User space example: goodbye from STMicroelectronics [ perf record: Woken up 1 time to write data ] [ perf record: Captured and wrote 0.004 MB perf.data (28 samples) ]
- This is possible to filter events (given by perf list command). More information, options and examples are available in perf.wiki.kernel.org[8].
- By default, the events are recorded in the perf.data file. If you want to specify another output file name you have to add -o, --output <file> option.
- perf report (Linux kernel documentation[9]): breaks down the events by process, function, etc.
Example after previous command "perf record hello_world_example" perf report Samples: 28 of event 'cycles:ppp', Event count (approx.):2737925 Overhead Command Shared Object Symbol 12.66% hello_world_exa ld-2.26.so [.] _dl_relocate_object 11.71% hello_world_exa [kernel.kallsyms] [k] filemap_map_pages 10.65% hello_world_exa [kernel.kallsyms] [k] n_tty_write 6.43% hello_world_exa [kernel.kallsyms] [k] percpu_counter_add_batch 6.43% hello_world_exa ld-2.26.so [.] sbrk 6.24% hello_world_exa [kernel.kallsyms] [k] cpu_v7_set_pte_ext 5.56% hello_world_exa [kernel.kallsyms] [k] alloc_set_pte 5.56% hello_world_exa libc-2.26.so [.] __sbrk 5.37% hello_world_exa [kernel.kallsyms] [k] __vma_link_file 5.32% hello_world_exa [kernel.kallsyms] [k] __fput 5.32% hello_world_exa [kernel.kallsyms] [k] ldsem_up_read 5.32% hello_world_exa [kernel.kallsyms] [k] unmap_page_range 5.32% hello_world_exa libc-2.26.so [.] printf 5.24% hello_world_exa [kernel.kallsyms] [k] _raw_spin_unlock_irqrestore 2.23% hello_world_exa [kernel.kallsyms] [k] perf_event_mmap 0.48% hello_world_exa [kernel.kallsyms] [k] perf_output_begin 0.13% perf [kernel.kallsyms] [k] perf_event_exec
- By default, report file perf.data is read as input file. If you want to specify another input file name you have to add -i, --input <file> option.
- More information and examples are available in perf.wiki.kernel.org[10].
- perf bench (Linux kernel documentation[11]): runs different kernel microbenchmarks:
# List of all available benchmark collections:
sched: Scheduler and IPC benchmarks
mem: Memory access benchmarks
futex: Futex stressing benchmarks
all: All benchmarks
Example of getting memcpy benchmark for 100MB: perf bench mem memcpy --size 100MB # Running 'mem/memcpy' benchmark: # function 'default' (Default memcpy() provided by glibc) # Copying 100MB bytes ... 1.426138 GB/sec
- More information and examples are available in perf.wiki.kernel.org[12].
5. To go further[edit source]
5.1. Visualizing trace using Flame Graphs[edit source]
As part of Flame Graphs[13], this is possible to visualize trace coming from perf.
The Flame graphs are generated using Flame graphs tool suite[14].
- Install the Flame Graph tool suite on host PC side
cd <your_local_path> git clone https://github.com/brendangregg/FlameGraph.git cd FlameGraph
- Generate a Flame graph from perf tool
- When generating perf record, -g option must be added.
As example for a top command:
- Perform perf record command on board side perf record -a -g top perf script > perf_top.out - Copy perf_top.out on your host PC (i.e. in the FlameGraph directory) - Perform the flame graph generation on host PC side using stackcollapse-perf.pl script ./stackcollapse-perf.pl perf_top.out > out.top_folded - Use flamegraph.pl to render a SVG (Scalable Vector Graphics) file. ./flamegraph.pl out.top_folded > top.svg - Visualize SVG using web browser for example firefox top.svg
6. References[edit source]
- ↑ 1.0 1.1 https://perf.wiki.kernel.org/index.php/Main_Page
- ↑ tools/perf/Documentation/perf-top.txt
- ↑ https://perf.wiki.kernel.org/index.php/Tutorial#Live_analysis_with_perf_top
- ↑ tools/perf/Documentation/perf-stat.txt
- ↑ https://perf.wiki.kernel.org/index.php/Tutorial#Counting_with_perf_stat
- ↑ tools/perf/Documentation/perf-list.txt
- ↑ tools/perf/Documentation/perf-record.txt
- ↑ https://perf.wiki.kernel.org/index.php/Tutorial#Sampling_with_perf_record
- ↑ tools/perf/Documentation/perf-report.txt
- ↑ https://perf.wiki.kernel.org/index.php/Tutorial#Sample_analysis_with_perf_report
- ↑ tools/perf/Documentation/perf-bench.txt
- ↑ https://perf.wiki.kernel.org/index.php/Tutorial#Benchmarking_with_perf_bench
- ↑ http://www.brendangregg.com/flamegraphs.html
- ↑ https://github.com/brendangregg/FlameGraph
- Useful external links
Document link | Document Type | Description |
---|---|---|
perf tutorial | User Guide | perf.wiki.kernel.org |
perf (wikipedia.org) | Standard | wikipedia.org |
Brendan Gregg's perf page | Perf example | From Brendan Gregg |
Eclipse perf plugin page | Eclipse perf plugin | Eclipse.org |