This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User (Merge articles) |
||
Line 19: | Line 19: | ||
** the [[STM32MP15 RAM mapping]] allows to see how STM32 MPU Embedded Software distribution maps the various software memory needs in internal and external volatile memories, | ** the [[STM32MP15 RAM mapping]] allows to see how STM32 MPU Embedded Software distribution maps the various software memory needs in internal and external volatile memories, | ||
** the [[STM32MP15 backup registers]] article shows which backup registers are used for system aspects in STM32 MPU Embedded Software distribution and so, which ones remain free for the application needs, | ** the [[STM32MP15 backup registers]] article shows which backup registers are used for system aspects in STM32 MPU Embedded Software distribution and so, which ones remain free for the application needs, | ||
** the [[STM32MP15 device tree]] shows how the [[Device tree|device tree]] files for STM32MP15 are organized for Linux, U-Boot and TF-A but also how they are organized when they are generated from STM32CubeMX, | ** the [[STM32MP15 device tree]] shows how the [[Device tree|device tree]] files for STM32MP15 are organized for Linux, U-Boot and TF-A but also how they are organized when they are generated from STM32CubeMX, | ||
* The [[:Category:Device tree configuration|device tree configuration]] category gathers the description of the [[Device tree|device tree]] bindings for all STMicroelectronics internal peripherals, that are listed in [[STM32MP15 peripherals overview]] article for STM32MP15. | * The [[:Category:Device tree configuration|device tree configuration]] category gathers the description of the [[Device tree|device tree]] bindings for all STMicroelectronics internal peripherals, that are listed in [[STM32MP15 peripherals overview]] article for STM32MP15. |
Latest revision as of 16:54, 18 March 2021
The platform configuration category contains two sub-categories:
- The STM32MP15 platform configuration category is about all the peripherals (MPU and board related) that should be configured by software to make it running on a board:
- the STM32MP15 clock tree ensures that all the peripherals receive clocks with characteristics compatible with the specification (frequency, duty cycle, precision) on each ST board,
- the STM32MP15 Flash mapping shows the mapping used in STM32 MPU Embedded Software distribution for ST boards, that can be used as starting point in other boards,
- the STM32MP15 RAM mapping allows to see how STM32 MPU Embedded Software distribution maps the various software memory needs in internal and external volatile memories,
- the STM32MP15 backup registers article shows which backup registers are used for system aspects in STM32 MPU Embedded Software distribution and so, which ones remain free for the application needs,
- the STM32MP15 device tree shows how the device tree files for STM32MP15 are organized for Linux, U-Boot and TF-A but also how they are organized when they are generated from STM32CubeMX,
- The device tree configuration category gathers the description of the device tree bindings for all STMicroelectronics internal peripherals, that are listed in STM32MP15 peripherals overview article for STM32MP15.