Registered User m (→Bare Environment: fix typo in internal info: missing ' in command line) |
Registered User m (→Build with the Developer Package or a Bare Environment: Ack Olivier's comment) |
||
(20 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
== Purpose == | == Purpose == | ||
This article describes the process used for building several OP-TEE components from sources and deploying them the target.<br> | This article describes the configuration and process used for building several OP-TEE components from sources and deploying them the target.<br> | ||
The build example is based on the OpenSTLinux [[STM32MP1_Developer_Package|Developer Package]] or [[STM32MP1_Distribution_Package|Distribution Package]], and also presents build instructions for a bare environment. | The build example is based on the OpenSTLinux [[STM32MP1_Developer_Package|Developer Package]] or [[STM32MP1_Distribution_Package|Distribution Package]], and also presents build instructions for a bare environment. | ||
Line 10: | Line 10: | ||
OP-TEE components generate boot images and files stored in the filesystem embedded in the target. | OP-TEE components generate boot images and files stored in the filesystem embedded in the target. | ||
* OP-TEE OS generates 3 boot image files to be loaded in the platform boot media, in the predefined partitions. The generated boot images include a [[ | * OP-TEE OS generates 3 boot image files to be loaded in the platform boot media, in the predefined partitions. The generated boot images include a [[STM32_header_for_binary_files|STM32 binary header]] enabling the use of the authenticated boot and flash programming facilities. | ||
* OP-TEE client (package optee_client) can be built to generate non-secure services for the OP-TEE OS. The files generated from optee_client build are stored in the embedded filesystem. | * OP-TEE client (package optee_client) can be built to generate non-secure services for the OP-TEE OS. The files generated from optee_client build are stored in the embedded filesystem. | ||
Line 16: | Line 16: | ||
* OP-TEE project releases other packages intended for test and demonstration. These can be built and embedded in the target filesystem. Building optee_examples and optee_test generates client and trusted applications together with libraries which are all stored in the target filesystem. Note the OP-TEE Linux driver is built into the Linux kernel image and is part of the OP-TEE ecosystem. | * OP-TEE project releases other packages intended for test and demonstration. These can be built and embedded in the target filesystem. Building optee_examples and optee_test generates client and trusted applications together with libraries which are all stored in the target filesystem. Note the OP-TEE Linux driver is built into the Linux kernel image and is part of the OP-TEE ecosystem. | ||
OP-TEE can be embedded in the | OP-TEE can be embedded as BL32 in the STM32 MPU platforms for the ST trusted configuration.<br> | ||
{{Warning | OP-TEE boot images must be embedded in the [[How to configure TF-A FIP|FIP binary]] that is loaded by BL2 and can be automatically authentified}} | |||
== OP-TEE core configuration == | |||
=== STM32MP15 === | |||
OP-TEE OS requires more than 256Ko RAM. [[SYSRAM_internal_memory|SYSRAM]] is only 256Ko, the OP-TEE core must use the pager mode to extends memory using DDR. | |||
OP-TEE OS is loaded at the beginning of the [[SYSRAM_internal_memory|SYSRAM]] by the FSBL. The OP-TEE could extend the memory to the full [[SYSRAM_internal_memory|SYSRAM]]. | |||
As pager is used, a second part of the code is loaded in DDR (pageable part) in a restricted secure accessible area. | |||
OP-TEE OS manages low power mode by saving its context in DDR (encrypted area) that is restored by a protected execution code saved in secured [[BKPSRAM_internal_memory|backup SRAM]]. | |||
OP-TEE OS implements the following secure services: | |||
* PSCI services | |||
** System reset | |||
** CPU hotplug | |||
** Low power | |||
* [[SCMI_overview|SCMI services]] | |||
** Clock management | |||
** Reset management | |||
* OTP access services | |||
* [[PWR_internal_peripheral|PWR services]] | |||
** PWR regulator access for non secure IPs | |||
** Wakeup source management | |||
* [[RCC_internal_peripheral|RCC services]] Limited access | |||
** OPP request management | |||
** Calibration triggering | |||
== Build with the Distribution Package == | == Build with the Distribution Package == | ||
Line 53: | Line 80: | ||
{{PC$}} | {{PC$}} | ||
{{Warning|The | {{ReviewsComments|-- [[User:Olivier Gallien|Olivier Gallien]] ([[User talk:Olivier Gallien|talk]]) 09:28, 12 January 2022 (CET)<br />complete git clone command with correct tag for 3.1 and/or add below warning }} | ||
{{ReviewsComments|-- [[User:Etienne Carriere|Etienne Carriere]] ([[User talk:Etienne Carriere|talk]]) 10:42, 17 January 2022 (CET)<br />That is right. I've fixed warning sentence: s/3.12/3.12.0/.}} | |||
{{Warning|Pay attention to use a consistent tag version for all optee components eg 3.12.0 for DV3.1 }} | |||
{{Warning|The STM32 MPU platform may not be fully merged in the official OP-TEE repository <ref name=OP-TEE/optee_os>https://github.com/OP-TEE/optee_os</ref> hence the URL provided above refers to the ST distribution <ref name=STMicroelectronics/optee_os>https://github.com/STMicroelectronics/optee_os</ref>}} | |||
{{InternalInfo | | {{InternalInfo | | ||
Line 73: | Line 105: | ||
The OP-TEE OS can be built from the [[STM32MP1_Developer_Package|Developer Package]] '''Makefile.sdk''' script that is present in the tarball. It automatically sets the proper configuration for the OP-TEE OS build. To build from shell command:<br> | The OP-TEE OS can be built from the [[STM32MP1_Developer_Package|Developer Package]] '''Makefile.sdk''' script that is present in the tarball. It automatically sets the proper configuration for the OP-TEE OS build. To build from shell command:<br> | ||
{{PC$}} make -f Makefile.sdk CFG_EMBED_DTB_SOURCE_FILE=<board_dts_file_name>.dts | {{PC$}} make -f Makefile.sdk CFG_EMBED_DTB_SOURCE_FILE=<board_dts_file_name>.dts | ||
{{ReviewsComments|-- [[User:Olivier Gallien|Olivier Gallien]] ([[User talk:Olivier Gallien|talk]]) 11:44, 6 January 2022 (CET)<br /> correct command syntax is make -f $PWD/../Makefile.sdk [..] and as such generate an out-tree /build folder instead of in-tree /out as used in rest of article }} | |||
==== Bare Environment ==== | ==== Bare Environment ==== | ||
Alternatively one can also build OP-TEE OS based a bare cross compilation toolchains, for example for the stm32mp157c-ev1 board: | Alternatively one can also build OP-TEE OS based a bare cross compilation toolchains, for example for the stm32mp157c-ev1 board: | ||
{{PC$}} cd <optee-os> | {{PC$}} cd <optee-os> | ||
Line 94: | Line 117: | ||
==== Generated Files ==== | ==== Generated Files ==== | ||
The 3 OP-TEE boot images are generated at following paths: | The 3 OP-TEE boot images are generated at following paths: | ||
<optee-os>/out/core/tee-header_v2. | <optee-os>/out/core/tee-header_v2.bin | ||
<optee-os>/out/core/tee-pageable_v2. | <optee-os>/out/core/tee-pageable_v2.bin | ||
<optee-os>/out/core/tee-pager_v2. | <optee-os>/out/core/tee-pager_v2.bin | ||
One can get the configuration directives used for the build are available in this file: | One can get the configuration directives used for the build are available in this file: | ||
Line 107: | Line 130: | ||
Mandatory directives to build OP-TEE OS: | Mandatory directives to build OP-TEE OS: | ||
* '''PLATFORM= | * '''PLATFORM=<platform>''' | ||
* '''CFG_EMBED_DTB_SOURCE_FILE=<device-tree-source-file>''': in-tree (core/arch/arm/dts/) device tree filename with its '''.dts''' extension. | ** Ex: '''PLATFORM=stm32mp1''' | ||
* '''CFG_EMBED_DTB_SOURCE_FILE=<device-tree-source-file>''': in-tree ({{CodeSource | OP-TEE_OS | core/arch/arm/dts/}}) device tree filename with its '''.dts''' extension. | |||
Common optional directives: | Common optional directives: | ||
Line 114: | Line 138: | ||
* '''CFG_TEE_CORE_LOG_LEVEL={0|1|2|3|4}''': define the trace level (0: no trace, 4: overflow of traces) | * '''CFG_TEE_CORE_LOG_LEVEL={0|1|2|3|4}''': define the trace level (0: no trace, 4: overflow of traces) | ||
* '''CFG_UNWIND={n|y}''': disable/enable stack unwind support | * '''CFG_UNWIND={n|y}''': disable/enable stack unwind support | ||
* '''CFG_STM32_BSEC_WRITE=1''': Enable the program/write fuses capabilities (default disabled to avoid briking the chip) | |||
For {{EcosystemRelease | revision=3.0.0 | range=and before}} compatibility | |||
<div class="mw-collapsible mw-collapsed"> | |||
It is still possible to generate the the STM32 binary files with an option flag:<br> | |||
* CFG_STM32MP15x_STM32IMAGE=1: Generate the STM32 files for {{EcosystemRelease | revision=3.0.0 | range=and before}} compatibility. | |||
</div> | |||
<br> | |||
Note: internal memory size constrains the debug support level that can be provided. | Note: internal memory size constrains the debug support level that can be provided. | ||
Line 119: | Line 151: | ||
==== Troubleshoot ==== | ==== Troubleshoot ==== | ||
The [[STM32MP1_Developer_Package|Developer Package]] toolchain may report dependency error in the traces such as: | The [[STM32MP1_Developer_Package|Developer Package]] toolchain may report dependency error in the traces such as: | ||
{{PC$}} make PLATFORM=stm32mp1 ... | |||
arm-ostl-linux-gnueabi-ld.bfd: unrecognized option '-Wl,-O1' | |||
arm-ostl-linux-gnueabi-ld.bfd: use the --help option for usage information | |||
core/arch/arm/kernel/link.mk:165: recipe for target 'out/arm-plat-stm32mp1/core/tee.elf' failed | |||
make: *** [out/arm-plat-stm32mp1/core/tee.elf] Error 1 | |||
This is linked to default CFLAGS and LDFLAGS exported by SDK. Just remove them from the environment and rebuild | |||
{{PC$}} unset -v CFLAGS LDFLAGS | |||
Other reported issues: | |||
{{PC$}} make PLATFORM=stm32mp1 ... | {{PC$}} make PLATFORM=stm32mp1 ... | ||
arm-openstlinux_weston-linux-gnueabi-ld.bfd: cannot find libgcc.a: No such file or directory | arm-openstlinux_weston-linux-gnueabi-ld.bfd: cannot find libgcc.a: No such file or directory | ||
To overcome the issue, add the directive ''' | To overcome the issue, add the directive '''LIBGCC_LOCATE_CFLAGS=--sysroot=$SDKTARGETSYSROOT'''. I.e: | ||
{{PC$}} cd <optee-os> | {{PC$}} cd <optee-os> | ||
{{PC$}} make PLATFORM=stm32mp1 \ | {{PC$}} make PLATFORM=stm32mp1 \ | ||
CFG_EMBED_DTB_SOURCE_FILE=stm32mp157c-ev1.dts \ | CFG_EMBED_DTB_SOURCE_FILE=stm32mp157c-ev1.dts \ | ||
CFG_TEE_CORE_LOG_LEVEL=2 \ | CFG_TEE_CORE_LOG_LEVEL=2 \ | ||
LIBGCC_LOCATE_CFLAGS=--sysroot=${SDKTARGETSYSROOT} \ | |||
O=out all | O=out all | ||
Line 141: | Line 184: | ||
It is recommended to use CMake for building the Linux userland part whereas secure world binaries (TAs) must be build from their GNU makefiles as the OP-TEE project has not yet ported the secure world binaries build process over CMake. | It is recommended to use CMake for building the Linux userland part whereas secure world binaries (TAs) must be build from their GNU makefiles as the OP-TEE project has not yet ported the secure world binaries build process over CMake. | ||
==== Build the secure components==== | ==== Build the secure components ==== | ||
Build the TAs: This step expects OP-TEE OS is built to generate the 32bit TA development kit. Assuming OP-TEE OS was built at path <optee-os>/out, the TA development kit is available from path <optee-os>/out/export-ta_arm32/. | Build the TAs: This step expects OP-TEE OS is built to generate the 32bit TA development kit. Assuming OP-TEE OS was built at path <optee-os>/out, the TA development kit is available from path <optee-os>/out/export-ta_arm32/. | ||
Line 160: | Line 203: | ||
target | target | ||
└── lib | └── lib | ||
└── optee_armtz | |||
├── 614789f2-39c0-4ebf-b235-92b32ac107ed.ta | |||
├── 731e279e-aafb-4575-a771-38caa6f0cca6.ta | |||
└── (...) | └── (...) | ||
Line 194: | Line 237: | ||
'''DESTDIR=target''' makes the embedded files be populated in the local '''./target/''' directory. | '''DESTDIR=target''' makes the embedded files be populated in the local '''./target/''' directory. | ||
Note also that | Note also that stm32mp1 expects tool '''tee-supplicant''' to be located in directory '''/usr/bin''' whereas CMake installs it in directory '''/usr/sbin'''. To overcome this issue, one can build a link to the effective location, i.e: | ||
{{PC$}} ln -s ../bin/tee-supplicant target/sbin/tee-supplicant | {{PC$}} ln -s ../bin/tee-supplicant target/sbin/tee-supplicant | ||
Line 203: | Line 246: | ||
target/ | target/ | ||
├── bin | ├── bin | ||
│ ├── benchmark | |||
│ ├── optee_example_acipher | |||
│ ├── optee_example_aes | |||
│ ├── optee_example_hello_world | |||
│ ├── optee_example_hotp | |||
│ ├── optee_example_random | |||
│ ├── optee_example_secure_storage | |||
│ ├── tee-supplicant | |||
│ └── xtest | |||
├── include | ├── include | ||
│ ├── tee_bench.h | |||
│ ├── tee_client_api_extensions.h | |||
│ ├── tee_client_api.h | |||
│ └── teec_trace.h | |||
├── lib | ├── lib | ||
│ ├── libteec.so -> libteec.so.1 | |||
│ ├── libteec.so.1 -> libteec.so.1.0.0 | |||
│ └── libteec.so.1.0.0 | |||
│ └── optee_armtz | |||
│ └── (...) # This directory was previously filled with TAs | |||
└── sbin | └── sbin | ||
└── tee-supplicant -> ../bin/tee-supplicant | |||
== Update | == Update OP-TEE boot images == | ||
OP-TEE boot images are part of the [[How to configure TF-A FIP|FIP binary]].<br> | |||
The next step to deploy the OP-TEE OS is to update the FIP binary following the [[How to configure TF-A FIP#Updating_OP-TEE|FIP update process]]. | |||
== Update OP-TEE Linux files == | |||
=== Update on board === | |||
The other OP-TEE images are stored in the target filesystem.<br> | The other OP-TEE images are stored in the target filesystem.<br> | ||
For example, if using an SD card as target boot media, the card can be plugged in its PC card reader and the images copied. | For example, if using an SD card as target boot media, the card can be plugged in its PC card reader and the images copied. | ||
The files can be simply copied into the mounted rootfs. | |||
=== Update | === Update in a SD card === | ||
The OP-TEE files that need to be copied to the target filesystem were installed in a local directory '''./target/'''. | The OP-TEE files that need to be copied to the target filesystem were installed in a local directory '''./target/'''. | ||
Line 263: | Line 286: | ||
{{PC$}} cp -ar target/* /media/$USERNAME/rootfs/ | {{PC$}} cp -ar target/* /media/$USERNAME/rootfs/ | ||
== Update your boot device (including SD card on the target) == | |||
Refer to the [[STM32CubeProgrammer]] documentation to update your target. | Refer to the [[STM32CubeProgrammer]] documentation to update your target. | ||
Latest revision as of 11:47, 17 January 2022
1. Purpose[edit source]
This article describes the configuration and process used for building several OP-TEE components from sources and deploying them the target.
The build example is based on the OpenSTLinux Developer Package or Distribution Package, and also presents build instructions for a bare environment.
2. Overview[edit source]
OP-TEE is a trusted execution environment for Arm®v7-A and Arm®v8-A platforms.
OP-TEE is made of several components described in OP-TEE architecture overview.
OP-TEE components generate boot images and files stored in the filesystem embedded in the target.
- OP-TEE OS generates 3 boot image files to be loaded in the platform boot media, in the predefined partitions. The generated boot images include a STM32 binary header enabling the use of the authenticated boot and flash programming facilities.
- OP-TEE client (package optee_client) can be built to generate non-secure services for the OP-TEE OS. The files generated from optee_client build are stored in the embedded filesystem.
- OP-TEE project releases other packages intended for test and demonstration. These can be built and embedded in the target filesystem. Building optee_examples and optee_test generates client and trusted applications together with libraries which are all stored in the target filesystem. Note the OP-TEE Linux driver is built into the Linux kernel image and is part of the OP-TEE ecosystem.
OP-TEE can be embedded as BL32 in the STM32 MPU platforms for the ST trusted configuration.
![]() |
OP-TEE boot images must be embedded in the FIP binary that is loaded by BL2 and can be automatically authentified |
3. OP-TEE core configuration[edit source]
3.1. STM32MP15[edit source]
OP-TEE OS requires more than 256Ko RAM. SYSRAM is only 256Ko, the OP-TEE core must use the pager mode to extends memory using DDR.
OP-TEE OS is loaded at the beginning of the SYSRAM by the FSBL. The OP-TEE could extend the memory to the full SYSRAM. As pager is used, a second part of the code is loaded in DDR (pageable part) in a restricted secure accessible area.
OP-TEE OS manages low power mode by saving its context in DDR (encrypted area) that is restored by a protected execution code saved in secured backup SRAM.
OP-TEE OS implements the following secure services:
- PSCI services
- System reset
- CPU hotplug
- Low power
- SCMI services
- Clock management
- Reset management
- OTP access services
- PWR services
- PWR regulator access for non secure IPs
- Wakeup source management
- RCC services Limited access
- OPP request management
- Calibration triggering
4. Build with the Distribution Package[edit source]
The Distribution Package provides means to build the following OP-TEE components from their related bitbake target:
OP-TEE core firmware PC $> bitbake optee-os-sdk-stm32mp # OP-TEE development kit for Trusted Applications PC $> bitbake optee-client # OP-TEE client PC $> bitbake optee-test # OP-TEE test suite (optional) PC $> bitbake optee-examples # TA and CA examplesPC $> bitbake optee-os-stm32mp #
Distribution Package build process includes fetching the source files, compiling them and installing them to the target images.
The Yocto recipes for the OP-TEE packages can be found in:
meta-st/meta-st-stm32mp/recipes-security/optee/optee-os-stm32mp*
meta-st/meta-st-openstlinux/recipes-security/optee/optee-client*
meta-st/meta-st-openstlinux/recipes-security/optee/optee-examples*
meta-st/meta-st-openstlinux/recipes-security/optee/optee-test*
5. Build with the Developer Package or a Bare Environment[edit source]
Both Developer Package and bare build environments expect you to fetch/download the OP-TEE package source file trees in order to build the embedded binary images.
The instruction set below assumes all OP-TEE package source trees are available in the base directory referred as <sources>/. The source files are available from the github repositories:
https://github.com/STMicroelectronics/optee_os.git PC $> git clone https://github.com/OP-TEE/optee_client.git PC $> git clone https://github.com/OP-TEE/optee_test.git PC $> git clone https://github.com/linaro-swg/optee_examples.git PC $> ls -1 <sources>/ optee_client optee_examples optee_os optee_test PC $>PC $> cd <sources>/ PC $> git clone
![]() |
Pay attention to use a consistent tag version for all optee components eg 3.12.0 for DV3.1 |
![]() |
The STM32 MPU platform may not be fully merged in the official OP-TEE repository [1] hence the URL provided above refers to the ST distribution [2] |
5.1. Initialize the cross compile environment[edit source]
The compilation toolchain provided by the Developer Package can be used, refer to Setup Cross Compile Environment.
Alternatively other bare toolchains can be used to build the OP-TEE secure parts. In such case, the instructions below expect the toolchain to be part of the PATH and its prefix is defined by CROSS_COMPILE. One can use something like:
PC $> export PATH=<path-to-toolchain>:$PATH
PC $> export CROSS_COMPILE=<toolchain-prefix>-
5.2. Build OP-TEE OS[edit source]
5.2.1. Developer Package SDK[edit source]
The OP-TEE OS can be built from the Developer Package Makefile.sdk script that is present in the tarball. It automatically sets the proper configuration for the OP-TEE OS build. To build from shell command:
DTB_SOURCE_FILE=<board_dts_file_name>.dtsPC $> make -f Makefile.sdk CFG_EMBED_
5.2.2. Bare Environment[edit source]
Alternatively one can also build OP-TEE OS based a bare cross compilation toolchains, for example for the stm32mp157c-ev1 board:
DTB_SOURCE_FILE=stm32mp157c-ev1.dts \ CFG_TEE_CORE_LOG_LEVEL=2 O=out allPC $> cd <optee-os> PC $> make PLATFORM=stm32mp1 \ CFG_EMBED_
5.2.3. Generated Files[edit source]
The 3 OP-TEE boot images are generated at following paths:
<optee-os>/out/core/tee-header_v2.bin
<optee-os>/out/core/tee-pageable_v2.bin
<optee-os>/out/core/tee-pager_v2.bin
One can get the configuration directives used for the build are available in this file:
<optee-os>/out/conf.mk
The build also generates a development kit used to build Trusted Application binaries:
<optee-os>/out/export-ta_arm32/
5.2.4. Details on build directives[edit source]
Mandatory directives to build OP-TEE OS:
- PLATFORM=<platform>
- Ex: PLATFORM=stm32mp1
- CFG_EMBED_DTB_SOURCE_FILE=<device-tree-source-file>: in-tree (core/arch/arm/dts/ ) device tree filename with its .dts extension.
Common optional directives:
- CFG_TEE_CORE_DEBUG={n|y}: disable/enable debug support
- CFG_TEE_CORE_LOG_LEVEL={0|1|2|3|4}: define the trace level (0: no trace, 4: overflow of traces)
- CFG_UNWIND={n|y}: disable/enable stack unwind support
- CFG_STM32_BSEC_WRITE=1: Enable the program/write fuses capabilities (default disabled to avoid briking the chip)
For ecosystem release ≤ v3.0.0 compatibility
Note: internal memory size constrains the debug support level that can be provided.
5.2.5. Troubleshoot[edit source]
The Developer Package toolchain may report dependency error in the traces such as:
PC $> make PLATFORM=stm32mp1 ...
arm-ostl-linux-gnueabi-ld.bfd: unrecognized option '-Wl,-O1'
arm-ostl-linux-gnueabi-ld.bfd: use the --help option for usage information
core/arch/arm/kernel/link.mk:165: recipe for target 'out/arm-plat-stm32mp1/core/tee.elf' failed
make: *** [out/arm-plat-stm32mp1/core/tee.elf] Error 1
This is linked to default CFLAGS and LDFLAGS exported by SDK. Just remove them from the environment and rebuild
PC $> unset -v CFLAGS LDFLAGS
Other reported issues:
PC $> make PLATFORM=stm32mp1 ...
arm-openstlinux_weston-linux-gnueabi-ld.bfd: cannot find libgcc.a: No such file or directory
To overcome the issue, add the directive LIBGCC_LOCATE_CFLAGS=--sysroot=$SDKTARGETSYSROOT. I.e:
DTB_SOURCE_FILE=stm32mp157c-ev1.dts \ CFG_TEE_CORE_LOG_LEVEL=2 \ LIBGCC_LOCATE_CFLAGS=--sysroot=${SDKTARGETSYSROOT} \ O=out allPC $> cd <optee-os> PC $> make PLATFORM=stm32mp1 \ CFG_EMBED_
5.3. Build commands for other OP-TEE components[edit source]
This section describes how the several OP-TEE components (excluding OP-TEE OS described in above section) can be built. All those components generate files targeting the embedded Linux OS based filesystem (i.e the rootfs). These files are the secure Trusted Applications (TAs) binaries as well as non-secure Client Applications (CAs), libraries and test files.
There are several ways to build the OP-TEE components. The examples given below refer to OP-TEE client, test and examples source file tree paths as <optee-client>, <optee-test> and <optee-examples>.
Building these components expect, at least for the trusted applications, that the OP-TEE OS was built and the generated TA development kit is available at <optee-os>/out/export-ta_arm32/.
It is recommended to use CMake for building the Linux userland part whereas secure world binaries (TAs) must be build from their GNU makefiles as the OP-TEE project has not yet ported the secure world binaries build process over CMake.
5.3.1. Build the secure components[edit source]
Build the TAs: This step expects OP-TEE OS is built to generate the 32bit TA development kit. Assuming OP-TEE OS was built at path <optee-os>/out, the TA development kit is available from path <optee-os>/out/export-ta_arm32/.
Instructions below build and copy the Trusted Application binaries to a local ./target/ directory that can be used to populate the target filesystem.
TA_DEV_KIT_DIR=$PWD/optee_os/out/export-ta_arm32 PC $> mkdir -p ./target/lib/optee_armtz PC $> for f in optee_test/ta/*/Makefile; do \ make -C `dirname $f` O=out; \ cp -f `dirname $f`/out/*.ta ./target/lib/optee_armtz; \ donePC $> export
Content in local directory ./target/ are the TA binary files:
PC $> tree target/
target
└── lib
└── optee_armtz
├── 614789f2-39c0-4ebf-b235-92b32ac107ed.ta
├── 731e279e-aafb-4575-a771-38caa6f0cca6.ta
└── (...)
These files need to be copied to the the target filesystem.
5.3.2. Build the non-secure components[edit source]
Download the OP-TEE source files in a base directory and create a CMakeLists.txt file in the base directory that lists all package to be built through CMake. For example:
PC $> ls
optee_client
optee_examples
optee_os
optee_test
CMakeLists.txt
PC $> cat CMakeLists.txt
add_subdirectory (optee_client)
add_subdirectory (optee_test)
add_subdirectory (optee_examples)
PC $>
From base directory, run cmake then make. The example below also creates the tree file system ./target/ that is populated with files generated that need to be installed in the target file system.
Note this examples also sets the toolchain environment:
SDK=$PWD/optee_os/out/export-ta_arm32 \ -DCMAKE_INSTALL_PREFIX= -DCMAKE_BUILD_TYPE=Release -DBUILD_SHARED_LIBS=y PC $> make PC $> make DESTDIR=target installPC $> cmake -DOPTEE_TEST_
Note the empty CMAKE_INSTALL_PREFIX value to get thing installed from root /, not from /usr/. DESTDIR=target makes the embedded files be populated in the local ./target/ directory.
Note also that stm32mp1 expects tool tee-supplicant to be located in directory /usr/bin whereas CMake installs it in directory /usr/sbin. To overcome this issue, one can build a link to the effective location, i.e:
PC $> ln -s ../bin/tee-supplicant target/sbin/tee-supplicant
Once done, local directory ./target/ contains the files to be copied in the target filesystem.
PC $> tree target/
target/
├── bin
│ ├── benchmark
│ ├── optee_example_acipher
│ ├── optee_example_aes
│ ├── optee_example_hello_world
│ ├── optee_example_hotp
│ ├── optee_example_random
│ ├── optee_example_secure_storage
│ ├── tee-supplicant
│ └── xtest
├── include
│ ├── tee_bench.h
│ ├── tee_client_api_extensions.h
│ ├── tee_client_api.h
│ └── teec_trace.h
├── lib
│ ├── libteec.so -> libteec.so.1
│ ├── libteec.so.1 -> libteec.so.1.0.0
│ └── libteec.so.1.0.0
│ └── optee_armtz
│ └── (...) # This directory was previously filled with TAs
└── sbin
└── tee-supplicant -> ../bin/tee-supplicant
6. Update OP-TEE boot images[edit source]
OP-TEE boot images are part of the FIP binary.
The next step to deploy the OP-TEE OS is to update the FIP binary following the FIP update process.
7. Update OP-TEE Linux files[edit source]
7.1. Update on board[edit source]
The other OP-TEE images are stored in the target filesystem.
For example, if using an SD card as target boot media, the card can be plugged in its PC card reader and the images copied. The files can be simply copied into the mounted rootfs.
7.2. Update in a SD card[edit source]
The OP-TEE files that need to be copied to the target filesystem were installed in a local directory ./target/.
They can now be copied to the target SD card rootfs partition once the SD card is plugged to the host computer and its filesystems are mounted in the host, i.e
PC $> cp -ar target/* /media/$USERNAME/rootfs/
8. Update your boot device (including SD card on the target)[edit source]
Refer to the STM32CubeProgrammer documentation to update your target.
9. References[edit source]