Registered User mNo edit summary |
Registered User mNo edit summary |
||
(4 intermediate revisions by the same user not shown) | |||
Line 1: | Line 1: | ||
[[File: | <div class="res-img"> | ||
[[File: AI_X-LINUX-AI-logo.png|center]] | |||
</div> | |||
X-LINUX-AI is an STM32 MPU OpenSTLinux Expansion Package that targets artificial intelligence for STM32MP1 Series devices. | <center> | ||
X-LINUX-AI is an STM32 MPU OpenSTLinux Expansion Package that targets artificial intelligence for STM32MP1 Series devices. It contains Linux AI frameworks, as well as application examples to get started with some basic use cases such as computer vision (CV). It is composed of an OpenEmbedded meta layer, named '''meta-st-stm32mpu-ai''', to be added on top of the [[STM32MP1_Distribution_Package | STM32MP1 Distribution Package]]. It brings a complete and coherent easy-to-build / install environment to take advantage of AI on STM32MP1 Series devices. | |||
It contains Linux AI frameworks, as well as application examples to get started with some basic use cases such as computer vision (CV). | </center> | ||
<div class="res-img"> | |||
It is composed of an OpenEmbedded meta layer, named '''meta-st-stm32mpu-ai''', to be added on top of the [[STM32MP1_Distribution_Package | STM32MP1 Distribution Package]]. | [[File: AI_Expansion_Package_In_STM32MPU_Embedded_Software.png|center]] | ||
</div> | |||
It brings a complete and coherent easy-to-build / install environment to take advantage of AI on STM32MP1 Series devices. | |||
==Versions== | ==Versions== | ||
===X-LINUX-AI v2.1.1=== | ===X-LINUX-AI v2.1.1=== | ||
{{Info| This version is compatible with Yocto Project<sup>®</sup> build system Dunfell and has been validated against the OpenSTLinux {{EcosystemRelease | revision=3.1.0}}, {{EcosystemRelease | revision=3.0.0}}, {{EcosystemRelease | revision=2.1.0}} and validated on STM32MP157x-DKx, STM32MP157x-EV1 and STM32MP157 boards.}} | {{Info| This version is compatible with Yocto Project<sup>®</sup> build system Dunfell and has been validated against the OpenSTLinux {{EcosystemRelease | revision=3.1.0}}, {{EcosystemRelease | revision=3.0.0}}, {{EcosystemRelease | revision=2.1.0}} and validated on STM32MP157x-DKx, STM32MP157x-EV1 and STM32MP157 boards.}} | ||
====Contents==== | ====Contents==== | ||
* [[File:New.png|30px|link=]] '''TensorFlow Lite<ref name=tensorflowlite_url>[https://www.tensorflow.org/lite TensorFlow Lite]</ref> 2.5.0''' | * [[File:New.png|30px|link=]] '''TensorFlow Lite<ref name=tensorflowlite_url>[https://www.tensorflow.org/lite TensorFlow Lite]</ref> 2.5.0''' | ||
Line 221: | Line 223: | ||
With the following procedure, you can re-generate the complete distribution enabling the X-LINUX-AI expansion package.<br> | With the following procedure, you can re-generate the complete distribution enabling the X-LINUX-AI expansion package.<br> | ||
This procedure is mandatory if you want to update frameworks by yourself, or if you want to modify the application samples.<br> | This procedure is mandatory if you want to update frameworks by yourself, or if you want to modify the application samples.<br> | ||
===Download the STM32MP1 Distribution Package=== | ===Download the STM32MP1 Distribution Package=== | ||
Line 266: | Line 265: | ||
===Flash the built image=== | ===Flash the built image=== | ||
Follow this link to see how to [[STM32MP1_Distribution_Package#Flashing_the_built_image | flash the built image]]. | Follow this link to see how to [[STM32MP1_Distribution_Package#Flashing_the_built_image | flash the built image]]. | ||
==How to use the X-LINUX-AI Expansion Package == | ==How to use the X-LINUX-AI Expansion Package == |
Latest revision as of 12:22, 14 January 2022
X-LINUX-AI is an STM32 MPU OpenSTLinux Expansion Package that targets artificial intelligence for STM32MP1 Series devices. It contains Linux AI frameworks, as well as application examples to get started with some basic use cases such as computer vision (CV). It is composed of an OpenEmbedded meta layer, named meta-st-stm32mpu-ai, to be added on top of the STM32MP1 Distribution Package. It brings a complete and coherent easy-to-build / install environment to take advantage of AI on STM32MP1 Series devices.
1. Versions[edit source]
1.1. X-LINUX-AI v2.1.1[edit source]
1.1.1. Contents[edit source]
TensorFlow Lite[1] 2.5.0
- Coral Edge TPU[2] accelerator support
libedgetpu 2.5.0 aligned with TensorFlow Lite 2.5.0 (built from master branch source code)
armNN[3] 21.05
- OpenCV[4] 4.1.x
- Python[5] 3.8.x (enabling Pillow module)
- Support STM32MP15xF[6] devices operating at up to 800MHz
- Application samples
- C++ / Python image classification using TensorFlow Lite based on MobileNet v1 quantized model
- C++ / Python object detection using TensorFlow Lite based on COCO SSD MobileNet v1 quantized model
- C++ / Python image classification using Coral Edge TPU based on MobileNet v1 quantized model and compiled for the Coral Edge TPU
- C++ / Python object detection using Coral Edge TPU based on COCO SSD MobileNet v1 quantized model and compiled for the Coral Edge TPU
- C++ image classification using armNN TensorFlow Lite parser based on MobileNet v1 float model
- C++ object detection using armNN TensorFlow Lite parser based on COCO SSD MobileNet v1 quantized model
- C++ face recognition using TensorFlow Lite models capable of recognizing the face of a known (enrolled) user (available on demand)
Application support the 720p, 480p and 272p display configurations
Application user interface with updated look and feel
1.1.2. Validated hardware[edit source]
As any software expansion package, the X-LINUX-AI is supported on all STM32MP1 Series and it has been validated on the following boards:
1.1.3. Software structure[edit source]
1.2. X-LINUX-AI v2.1.0[edit source]
X-LINUX-AI v2.1.0 description.
1.3. X-LINUX-AI v2.0.0[edit source]
X-LINUX-AI v2.0.0 description.
2. Install from the OpenSTLinux AI package repository[edit source]
All the generated X-LINUX-AI packages are available from the OpenSTLinux AI package repository service hosted at the non-browsable URL http://extra.packages.openstlinux.st.com/AI.
This repository contains AI packages that can be simply installed using apt-* utilities, which the same as those used on a Debian system:
- the main group contains the selection of AI packages whose installation is automatically tested by STMicroelectronics
- the updates group is reserved for future uses such as package revision update.
You can install them individually or by package group.
2.1. Prerequisites[edit source]
- Flash the Starter Package on your SDCard
- For OpenSTLinux ecosystem release v3.1.0
and ecosystem release v3.0.0
:
- For OpenSTLinux ecosystem release v3.1.0
- For OpenSTLinux ecosystem release v2.1.0 :
- Your board has an internet connection either through the network cable or through a WiFi connection.
2.2. Configure the AI OpenSTLinux package repository[edit source]
Once the board is booted, execute the following command in the console in order to configure the AI OpenSTLinux package repository:
v3.1.0For ecosystem release: Board $> wget http://extra.packages.openstlinux.st.com/AI/3.1/pool/config/a/apt-openstlinux-ai/apt-openstlinux-ai_1.0_armhf.deb Board $> dpkg -i apt-openstlinux-ai_1.0_armhf.deb
v3.0.0For ecosystem release:Expand
ExpandFor ecosystem release v2.1.0 :
Then synchronize the AI OpenSTLinux package repository.
Board $> apt-get update
2.3. Install AI packages[edit source]
2.3.1. Install all X-LINUX-AI packages[edit source]
Command | Description |
---|---|
apt-get install packagegroup-x-linux-ai |
Install all the X-LINUX-AI packages (TensorFlow Lite, Edge TPU, armNN, application samples and tools) |
2.3.3. Install individual packages[edit source]
3. Re-generate X-LINUX-AI OpenSTLinux distribution[edit source]
With the following procedure, you can re-generate the complete distribution enabling the X-LINUX-AI expansion package.
This procedure is mandatory if you want to update frameworks by yourself, or if you want to modify the application samples.
3.1. Download the STM32MP1 Distribution Package[edit source]
For ecosystem release v3.1.0 :
Install the STM32MP1 Distribution Package v3.1.0, but do not initialize the OpenEmbedded environment (do not source the envsetup.sh).
For ecosystem release v3.0.0 :
For ecosystem release v2.1.0 :
3.2. Install X-LINUX-AI environment[edit source]
- Clone the meta-st-stm32mpu-ai git repositories
AI v2.1.1: PC $> cd <Distribution Package installation directory>/layers/meta-st PC $> git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-ai.git -b v2.1.1 For X-LINUX-AI v2.1.0:ExpandFor X-LINUX-
- Set up the build environment
BSP_DEPENDENCY='layers/meta-st/meta-st-stm32mpu-ai' source layers/meta-st/scripts/envsetup.shPC $> cd ../.. PC $> DISTRO=openstlinux-weston MACHINE=stm32mp1
3.3. Build the image[edit source]
PC $> bitbake st-image-ai
3.4. Flash the built image[edit source]
Follow this link to see how to flash the built image.
4. How to use the X-LINUX-AI Expansion Package[edit source]
4.1. Material needed[edit source]
To use the X-LINUX-AI OpenSTLinux Expansion Package, choose one of the following materials:
- STM32MP157C-DK2[7] + an UVC USB WebCam
- STM32MP157C-EV1[8] with the built in OV5640 parallel camera
- STM32MP157A-EV1[9] with the built in OV5640 parallel camera
Optional:
- Coral USB Edge TPU[2] accelerator
4.2. Boot the OpenSTlinux Starter Package[edit source]
At the end of the boot sequence, the demo launcher application appears on the screen.
4.3. Install the X-LINUX-AI[edit source]
After having configured the AI OpenSTLinux package you can install the X-LINUX-AI components.
Board $> apt-get install packagegroup-x-linux-ai
And restart the demo launcher
Board $> systemctl restart weston@root
4.4. Launch an AI application sample[edit source]
Once the demo launcher is restarted, notice that it is slightly different because new AI application samples have been installed.
The demo laucher has the following appearance, and you can navigate into the different screens by using the NEXT or BACK buttons.
Screens 2, 3 and 4 contain AI application samples that are described within dedicated article available in the X-LINUX-AI application samples zoo page.
4.5. Enjoy running your own NN models[edit source]
The above examples provide application samples to demonstrate how to execute models easily on the STM32MP1.
You are free to update the C/C++ application or Python scripts for your own purposes, using your own NN models.
Source code locations are provided in application sample pages.
5. References[edit source]