This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User |
||
(16 intermediate revisions by 4 users not shown) | |||
Line 3: | Line 3: | ||
STM32CubeProgrammer is the '''official''' STMicroelectronics tool '''to download firmware into STMicroelectronics boards'''. | STM32CubeProgrammer is the '''official''' STMicroelectronics tool '''to download firmware into STMicroelectronics boards'''. | ||
==STM32CubeProgrammer - Version 2. | ==STM32CubeProgrammer - Version 2.9.0== | ||
<onlyinclude> | <onlyinclude> | ||
{| class=" | {| class="st-table" width=98% | ||
|- | |- | ||
! !! STM32CubeProgrammer for Linux<sup>®</sup> host PC!! STM32CubeProgrammer for Windows<sup>®</sup> host PC | ! !! style="text-align:center;"|STM32CubeProgrammer for Linux<sup>®</sup> host PC!! style="text-align:center;"|STM32CubeProgrammer for Windows<sup>®</sup> host PC | ||
|- | |- | ||
| '''Download''' | | '''Download''' | ||
| colspan="2" | | | colspan="2" | | ||
'''Version 2. | '''Version 2.9.0''' | ||
* | * Browse [https://www.st.com/en/development-tools/stm32cubeprog.html SetupSTM32CubeProgrammer] link and follow instructions to download the package, you need a myST account. | ||
* Download the archive file on your host PC in a temporary directory | * Download the archive file on your host PC in a temporary directory | ||
* Uncompress the archive file to get the STM32CubeProgrammer installers: | * Uncompress the archive file to get the STM32CubeProgrammer installers: | ||
Line 24: | Line 24: | ||
* Execute the Linux installer, which guides you through the installation process. | * Execute the Linux installer, which guides you through the installation process. | ||
<pre>./SetupSTM32CubeProgrammer-2. | <pre>$> ./SetupSTM32CubeProgrammer-2.9.0.linux</pre> | ||
* The path to the STM32CubeProgrammer binary must be added to the PATH environment variable | * The path to the STM32CubeProgrammer binary must be added to the PATH environment variable | ||
** either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command: | ** either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command: | ||
<pre style="white-space: pre-wrap"> | <pre style="white-space: pre-wrap"> | ||
export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH | $> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH | ||
</pre> | </pre> | ||
:* or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command: | :* or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command: | ||
<pre style="white-space: pre-wrap"> | <pre style="white-space: pre-wrap"> | ||
ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI | $> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI | ||
</pre> | </pre> | ||
|| | || | ||
Line 41: | Line 41: | ||
| colspan="2" | | | colspan="2" | | ||
* Instructions to follow for using the STM32CubeProgrammer can be found in user manual, [ | * Instructions to follow for using the STM32CubeProgrammer can be found in user manual, [[STM32MP15 resources#UM2237|UM2237]] available from ST web site, or in [[STM32CubeProgrammer#How to flash with STM32CubeProgrammer]] article. | ||
|- | |- | ||
| '''Detailed release note''' | | '''Detailed release note''' |
Latest revision as of 10:11, 16 November 2021
STM32CubeProgrammer is the official STMicroelectronics tool to download firmware into STMicroelectronics boards.
1. STM32CubeProgrammer - Version 2.9.0[edit source]
STM32CubeProgrammer for Linux® host PC | STM32CubeProgrammer for Windows® host PC | |
---|---|---|
Download |
Version 2.9.0
| |
Installation |
$> ./SetupSTM32CubeProgrammer-2.9.0.linux
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
|
|
User manual |
| |
Detailed release note |
|