Registered User |
Registered User m (Update for DV-3.1) |
||
(9 intermediate revisions by 5 users not shown) | |||
Line 1: | Line 1: | ||
==Disclaimers== | ==Disclaimers== | ||
STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.<br/> | STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.<br/> | ||
The package licenses hosted in these repositories can be found here: [[OpenSTLinux_licenses]]. | The package licenses hosted in these repositories can be found here: [[OpenSTLinux_licenses|OpenSTLinux licenses]].<br/> | ||
Command outputs described in this document may slightly vary depending on tools version. | |||
==Description== | ===Description=== | ||
OpenSTLinux provides a package repository service hosted at | OpenSTLinux provides a package repository service hosted at the non-browsable URL <nowiki>http://packages.openstlinux.st.com</nowiki>. | ||
The package repository service is designed for ''STM32MP157C-DK2'' boards and is enabled by default in the [[STM32MP15_Discovery_kits_-_Starter_Package|Starter Package]]. | The package repository service is designed for ''STM32MP157C-DK2'' boards and is enabled by default in the [[STM32MP15_Discovery_kits_-_Starter_Package|Starter Package]]. | ||
===Organization=== | ===Organization=== | ||
Within each repository, packages are organized in three groups (a.k.a ''components'' in the APT terminology): | |||
* the '''main''' group contains a wide selection of packages whose installation is automatically tested by STMicroelectronics | |||
* the '''untested''' group contains all the other packages that can be built using the <code>bitbake world</code> command. However their installation is not guaranteed. | |||
* the | * the '''updates''' group contains additional packages not included in the [[OpenSTLinux_distribution|OpenSTLinux distribution releases]] and updated packages. This group is managed by a dedicated layer available through github®. Further details are available by following the github® link: https://github.com/STMicroelectronics/meta-st-pkgrepo-updates. | ||
* the | |||
===Limitations=== | ===Limitations=== | ||
Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They can be installed only from the [[STM32MP15_Discovery_kits_-_Starter_Package|Starter Package]] using the [[STM32CubeProgrammer]]. | Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They can be installed only from the [[STM32MP15_Discovery_kits_-_Starter_Package|Starter Package]] using the [[STM32CubeProgrammer]]. | ||
''rootfs'' available space is about 60MB by default. For a better experience it is | ''rootfs'' available space is about 60MB by default. For a better experience it is recommended to [[STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer|flash]] the [[STM32MP15_Discovery_kits_-_Starter_Package|Starter Package]] using the "extensible" flashlayout (''*-extensible.tsv'').<br/> | ||
{{Grey|'''''Extensible flashlayout''''' does not flash userfs partition to extend the rootfs partition to the size of the sdcard.}} | {{Grey|'''''Extensible flashlayout''''' does not flash userfs partition to extend the rootfs partition to the size of the sdcard.}} | ||
==Usage== | ==Usage== | ||
===Prequisite=== | |||
We assume your board has an internet connection either through the network cable or through a WiFi connection. | |||
{{InternalInfo| | |||
If your internet access depends on a proxy server, you should define the http_proxy environment variable with the following command before any <code>apt-*</code> commands: | |||
{{Board$}} export http_proxy='http://<proxy url>:<proxy port>/' | |||
}} | |||
===Apt === | ===Apt === | ||
Line 31: | Line 37: | ||
OpenSTLinux packages can be handled using <code>apt-*</code> utilities, which are the same utilities used on a [https://manpages.debian.org/stable/apt/apt-get.8.en.html Debian system]. The first <code>apt-*</code> command that must be run before any other is: | OpenSTLinux packages can be handled using <code>apt-*</code> utilities, which are the same utilities used on a [https://manpages.debian.org/stable/apt/apt-get.8.en.html Debian system]. The first <code>apt-*</code> command that must be run before any other is: | ||
{{Board$}} apt-get update | |||
The software package is provided AS IS, and by downloading it, you agree to be | |||
bound to the terms of the software license agreement (SLA). | |||
The detailed content licenses can be found at | |||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | |||
Get:1 <nowiki>http://packages.openstlinux.st.com/3.1</nowiki> dunfell InRelease [3455 B] | |||
Get:2 <nowiki>http://packages.openstlinux.st.com/3.1</nowiki> dunfell/main armhf Packages [779 kB] | |||
Get:3 <nowiki>http://packages.openstlinux.st.com/3.1</nowiki> dunfell/updates armhf Packages [32.1 kB] | |||
Get:4 <nowiki>http://packages.openstlinux.st.com/3.1</nowiki> dunfell/untested armhf Packages [1450 kB] | |||
Fetched 2264 kB in 3s (635 kB/s) | |||
Reading package lists... Done | |||
This command synchronizes the local packages index from the repositories enumerated in [https://manpages.debian.org/stable/apt/sources.list.5.en.html <code>/etc/apt/sources.list{,.d}</code>]. Once it is updated, [https://manpages.debian.org/stable/apt/apt-cache.8.en.html <code>apt-cache</code>] can be used to get the list of all available packages: | This command synchronizes the local packages index from the repositories enumerated in [https://manpages.debian.org/stable/apt/sources.list.5.en.html <code>/etc/apt/sources.list{,.d}</code>]. Once it is updated, [https://manpages.debian.org/stable/apt/apt-cache.8.en.html <code>apt-cache</code>] can be used to get the list of all available packages: | ||
{{Board$}} apt-cache search . | |||
a52dec - ATSC A/52 surround sound stream decoder | |||
a52dec-doc - ATSC A/52 surround sound stream decoder | |||
acl - Utilities for managing POSIX Access Control Lists | |||
... | |||
xserver-xorg - The X.Org X server | |||
xserver-xorg-xwayland - The X.Org X server | |||
xterm - xterm is the standard terminal emulator for the X Window System | |||
xvinfo - Print out X-Video extension adaptor information | |||
xz - Utilities for managing LZMA compressed files | |||
It is possible to list only packages that match a given pattern, for example: | |||
{{Board$}} apt-cache search emacs | |||
libreadline-doc - Library for editing typed command lines - Documentation files | |||
zile - | gpm - Console mouse driver | ||
gpm-doc - Console mouse driver - Documentation files | |||
zile - Zile is lossy Emacs | |||
zile-doc - Zile is lossy Emacs - Documentation files | |||
libreadline8 - Library for editing typed command lines | |||
The desired package(s) can then be easily installed: | The desired package(s) can then be easily installed: | ||
{{Board$}} apt-get install zile | |||
Reading package lists... Done | |||
Building dependency tree | |||
Reading state information... Done | |||
The following additional packages will be installed: | |||
bdwgc | |||
The following NEW packages will be installed: | |||
bdwgc zile | |||
0 upgraded, 2 newly installed, 0 to remove and 0 not upgraded. | |||
Need to get 148 kB of archives. | |||
After this operation, 0 B of additional disk space will be used. | |||
Do you want to continue? [Y/n] | |||
Get:1 <nowiki>http://packages.openstlinux.st.com/3.1</nowiki> dunfell/untested armhf bdwgc armhf 8.0.4-r0 [69.2 kB] | |||
Get:2 <nowiki>http://packages.openstlinux.st.com/3.1</nowiki> dunfell/untested armhf zile armhf 2.4.14-r0 [79.3 kB] | |||
Fetched 148 kB in 0s (465kB/s) | |||
The software package is provided AS IS, and by downloading it, you agree to be | |||
bound to the terms of the software license agreement (SLA). | |||
The detailed content licenses can be found at | |||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | |||
Selecting previously unselected package bdwgc. | |||
(Reading database ... 14204 files and directories currently installed.) | |||
Preparing to unpack .../bdwgc_8.0.4-r0_armhf.deb ... | |||
Unpacking bdwgc (8.0.4-r0) ... | |||
Selecting previously unselected package zile. | |||
Preparing to unpack .../zile_2.4.14-r0_armhf.deb ... | |||
Unpacking zile (2.4.14-r0) ... | |||
Setting up bdwgc (8.0.4-r0) ... | |||
Setting up zile (2.4.14-r0) ... | |||
... or removed: | ... or removed: | ||
{{Board$}} apt-get remove zile | |||
Reading package lists... Done | |||
Building dependency tree | |||
Reading state information... Done | |||
The following package was automatically installed and is no longer required: | |||
bdwgc | |||
Use 'apt autoremove' to remove it. | |||
The following packages will be REMOVED: | |||
zile | |||
0 upgraded, 0 newly installed, 1 to remove and 0 not upgraded. | |||
After this operation, 0 B of additional disk space will be used. | |||
Do you want to continue? [Y/n] | |||
The software package is provided AS IS, and by downloading it, you agree to be | |||
bound to the terms of the software license agreement (SLA). | |||
The detailed content licenses can be found at | |||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | |||
(Reading database ... 14209 files and directories currently installed.) | |||
Removing zile (2.4.14-r0) ... | |||
This command only removes the files that were installed from this package. It does not remove the package from the <code>apt</code> download cache. If there is not enough space available on the system, it is recommended to clean the cache: | This command only removes the files that were installed from this package. It does not remove the package from the <code>apt</code> download cache. If there is not enough space available on the system, it is recommended to clean the cache: | ||
{{Board$}} apt-get clean | |||
Likewise, some packages may have been automatically installed to respect dependencies with other packages. If they are no longer required, they can be removed to free space: | Likewise, some packages may have been automatically installed to respect dependencies with other packages. If they are no longer required, they can be removed to free space: | ||
{{Board$}} apt-get autoremove | |||
Reading package lists... Done | |||
Building dependency tree | |||
Reading state information... Done | |||
The following packages will be REMOVED: | |||
bdwgc | |||
0 upgraded, 0 newly installed, 1 to remove and 0 not upgraded. | |||
After this operation, 0 B of additional disk space will be used. | |||
Do you want to continue? [Y/n] | |||
The software package is provided AS IS, and by downloading it, you agree to be | |||
bound to the terms of the software license agreement (SLA). | |||
The detailed content licenses can be found at | |||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | |||
(Reading database ... 14208 files and directories currently installed.) | |||
Removing bdwgc (8.0.4-r0) ... | |||
== How to activate a local package repository == | |||
===Prerequisite=== | |||
Even if ''Package repository for OpenSTLinux'' offers lots of and various packages, you may need to use a local and personnal package repository. To use a local and personnal package repository is a 'smart' and 'quick' way to update the [[STM32MP15_Discovery_kits_-_Starter_Package]] with your developments. | |||
A local package repository is a collection of *.deb organized such <code>apt</code> needs it. The local repository should provide ''Packages'' metafiles. | |||
Natively OpenEmbedded/Yocto build system is able to generate a valid package repository (by using <code>bitbake package-index</code> command listed below). | |||
So first [[STM32MP1 Distribution Package - OpenSTLinux distribution#Download|Install the STM32MP1 OpenSTLinux distribution]]. | |||
===Update the repo package indexes=== | |||
Execute the <code>bitbake package-index</code> command: | |||
{{PC$}} cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE> | |||
{{PC$}} bitbake package-index | |||
===HTTP server execution on the computer=== | |||
'''SimpleHTTPserver''' python application is already installed on the board with the OpenSTLinux distribution. You just need to launch this application on your host computer, in the "[your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb" folder: | |||
{{PC$}} cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb | |||
{{PC$}} python -m SimpleHTTPServer& | |||
===How to use the local OpenSTLinux Distribution=== | |||
We use the physical IP address of the HTTP server we launched above to configure APT. That means this {{<IP>}} address should be defined as static on the host computer.<br/> | |||
You can now configure the APT tool directly on the target via a Linux console: | |||
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/stm32mp1 /" > /etc/apt/sources.list.d/my_custom.list | |||
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list | |||
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list | |||
In the above example, | In the above example, '''[trusted=yes]''' has been specified because the package manifest '''Release''' is not signed.<br/> | ||
Then you can run the command to synchronize the local packages index: | |||
{{Board$}} apt-get update | |||
The software package is provided AS IS, and by downloading it, you agree to be | |||
bound to the terms of the software license agreement (SLA). | |||
The detailed content licenses can be found at | |||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | |||
Ign:1 http://<IP>:8000/all InRelease | |||
Ign:2 http://<IP>:8000/stm32mp1 InRelease | |||
Ign:3 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 InRelease | |||
Get:4 http://<IP>:8000/all Release [1213 B] | |||
Get:5 http://<IP>:8000/stm32mp1 Release [1218 B] | |||
Get:6 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release [1233 B] | |||
Ign:7 http://<IP>:8000/all Release.gpg | |||
Ign:8 http://<IP>:8000/stm32mp1 Release.gpg | |||
Ign:9 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release.gpg | |||
Get:10 http://<IP>:8000/all Packages [82.8 kB] | |||
Get:11 http://<IP>:8000/stm32mp1 Packages [173 kB] | |||
Get:12 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Packages [1734 kB] | |||
Fetched 1994 kB in 3s (662 kB/s) | |||
Reading package lists... Done | |||
The other <code>apt-*</code> commands are now available as described above. | |||
==Support== | ==Support== | ||
Line 91: | Line 213: | ||
Bug reports, request for new packages, or any other kind of support | Bug reports, request for new packages, or any other kind of support | ||
requests can be submitted through https://community.st.com. | requests can be submitted through https://community.st.com. | ||
==Further readings== | ==Further readings== | ||
* [[Dpkg]] | |||
* https://manpages.debian.org/stable/apt/apt-get.8.en.html | * https://manpages.debian.org/stable/apt/apt-get.8.en.html | ||
* https://manpages.debian.org/stable/apt/sources.list.5.en.html | * https://manpages.debian.org/stable/apt/sources.list.5.en.html | ||
Line 100: | Line 224: | ||
* https://wiki.debian.org/DebianRepository/SetupWithReprepro | * https://wiki.debian.org/DebianRepository/SetupWithReprepro | ||
* https://wiki.debian.org/SecureApt | * https://wiki.debian.org/SecureApt | ||
* | * [[STM32MP15 Discovery kits - Starter Package]] | ||
* | * [[STM32MP15_Evaluation boards - Starter Package]] | ||
* | * [[STM32MP1 Developer Package]] | ||
<noinclude> | <noinclude> |
Latest revision as of 17:06, 10 November 2021
1. Disclaimers[edit source]
STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.
The package licenses hosted in these repositories can be found here: OpenSTLinux licenses.
Command outputs described in this document may slightly vary depending on tools version.
1.1. Description[edit source]
OpenSTLinux provides a package repository service hosted at the non-browsable URL http://packages.openstlinux.st.com.
The package repository service is designed for STM32MP157C-DK2 boards and is enabled by default in the Starter Package.
1.2. Organization[edit source]
Within each repository, packages are organized in three groups (a.k.a components in the APT terminology):
- the main group contains a wide selection of packages whose installation is automatically tested by STMicroelectronics
- the untested group contains all the other packages that can be built using the
bitbake world
command. However their installation is not guaranteed. - the updates group contains additional packages not included in the OpenSTLinux distribution releases and updated packages. This group is managed by a dedicated layer available through github®. Further details are available by following the github® link: https://github.com/STMicroelectronics/meta-st-pkgrepo-updates.
1.3. Limitations[edit source]
Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They can be installed only from the Starter Package using the STM32CubeProgrammer.
rootfs available space is about 60MB by default. For a better experience it is recommended to flash the Starter Package using the "extensible" flashlayout (*-extensible.tsv).
Extensible flashlayout does not flash userfs partition to extend the rootfs partition to the size of the sdcard.
2. Usage[edit source]
2.1. Prequisite[edit source]
We assume your board has an internet connection either through the network cable or through a WiFi connection.
2.2. Apt[edit source]
OpenSTLinux packages can be handled using apt-*
utilities, which are the same utilities used on a Debian system. The first apt-*
command that must be run before any other is:
apt-get update
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Get:1 http://packages.openstlinux.st.com/3.1 dunfell InRelease [3455 B]
Get:2 http://packages.openstlinux.st.com/3.1 dunfell/main armhf Packages [779 kB]
Get:3 http://packages.openstlinux.st.com/3.1 dunfell/updates armhf Packages [32.1 kB]
Get:4 http://packages.openstlinux.st.com/3.1 dunfell/untested armhf Packages [1450 kB]
Fetched 2264 kB in 3s (635 kB/s)
Reading package lists... Done
This command synchronizes the local packages index from the repositories enumerated in /etc/apt/sources.list{,.d}
. Once it is updated, apt-cache
can be used to get the list of all available packages:
POSIX Access Control Lists ... xserver-xorg - The X.Org X server xserver-xorg-xwayland - The X.Org X server xterm - xterm is the standard terminal emulator for the X Window System xvinfo - Print out X-Video extension adaptor information xz - Utilities for managing LZMA compressed filesapt-cache search . a52dec - ATSC A/52 surround sound stream decoder a52dec-doc - ATSC A/52 surround sound stream decoder acl - Utilities for managing
It is possible to list only packages that match a given pattern, for example:
apt-cache search emacs
libreadline-doc - Library for editing typed command lines - Documentation files
gpm - Console mouse driver
gpm-doc - Console mouse driver - Documentation files
zile - Zile is lossy Emacs
zile-doc - Zile is lossy Emacs - Documentation files
libreadline8 - Library for editing typed command lines
The desired package(s) can then be easily installed:
apt-get install zile
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following additional packages will be installed:
bdwgc
The following NEW packages will be installed:
bdwgc zile
0 upgraded, 2 newly installed, 0 to remove and 0 not upgraded.
Need to get 148 kB of archives.
After this operation, 0 B of additional disk space will be used.
Do you want to continue? [Y/n]
Get:1 http://packages.openstlinux.st.com/3.1 dunfell/untested armhf bdwgc armhf 8.0.4-r0 [69.2 kB]
Get:2 http://packages.openstlinux.st.com/3.1 dunfell/untested armhf zile armhf 2.4.14-r0 [79.3 kB]
Fetched 148 kB in 0s (465kB/s)
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Selecting previously unselected package bdwgc.
(Reading database ... 14204 files and directories currently installed.)
Preparing to unpack .../bdwgc_8.0.4-r0_armhf.deb ...
Unpacking bdwgc (8.0.4-r0) ...
Selecting previously unselected package zile.
Preparing to unpack .../zile_2.4.14-r0_armhf.deb ...
Unpacking zile (2.4.14-r0) ...
Setting up bdwgc (8.0.4-r0) ...
Setting up zile (2.4.14-r0) ...
... or removed:
apt-get remove zile
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following package was automatically installed and is no longer required:
bdwgc
Use 'apt autoremove' to remove it.
The following packages will be REMOVED:
zile
0 upgraded, 0 newly installed, 1 to remove and 0 not upgraded.
After this operation, 0 B of additional disk space will be used.
Do you want to continue? [Y/n]
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
(Reading database ... 14209 files and directories currently installed.)
Removing zile (2.4.14-r0) ...
This command only removes the files that were installed from this package. It does not remove the package from the apt
download cache. If there is not enough space available on the system, it is recommended to clean the cache:
apt-get clean
Likewise, some packages may have been automatically installed to respect dependencies with other packages. If they are no longer required, they can be removed to free space:
apt-get autoremove
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following packages will be REMOVED:
bdwgc
0 upgraded, 0 newly installed, 1 to remove and 0 not upgraded.
After this operation, 0 B of additional disk space will be used.
Do you want to continue? [Y/n]
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
(Reading database ... 14208 files and directories currently installed.)
Removing bdwgc (8.0.4-r0) ...
3. How to activate a local package repository[edit source]
3.1. Prerequisite[edit source]
Even if Package repository for OpenSTLinux offers lots of and various packages, you may need to use a local and personnal package repository. To use a local and personnal package repository is a 'smart' and 'quick' way to update the STM32MP15_Discovery_kits_-_Starter_Package with your developments.
A local package repository is a collection of *.deb organized such apt
needs it. The local repository should provide Packages metafiles.
Natively OpenEmbedded/Yocto build system is able to generate a valid package repository (by using bitbake package-index
command listed below).
So first Install the STM32MP1 OpenSTLinux distribution.
3.2. Update the repo package indexes[edit source]
Execute the bitbake package-index
command:
cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>
bitbake package-index
3.3. HTTP server execution on the computer[edit source]
SimpleHTTPserver python application is already installed on the board with the OpenSTLinux distribution. You just need to launch this application on your host computer, in the "[your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb" folder:
cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb
python -m SimpleHTTPServer&
3.4. How to use the local OpenSTLinux Distribution[edit source]
We use the physical IP address of the HTTP server we launched above to configure APT. That means this {{<IP>}} address should be defined as static on the host computer.
You can now configure the APT tool directly on the target via a Linux console:
echo "deb [trusted=yes] http://<IP>:8000/stm32mp1 /" > /etc/apt/sources.list.d/my_custom.list
echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list
echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list
In the above example, [trusted=yes] has been specified because the package manifest Release is not signed.
Then you can run the command to synchronize the local packages index:
apt-get update
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Ign:1 http://<IP>:8000/all InRelease
Ign:2 http://<IP>:8000/stm32mp1 InRelease
Ign:3 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 InRelease
Get:4 http://<IP>:8000/all Release [1213 B]
Get:5 http://<IP>:8000/stm32mp1 Release [1218 B]
Get:6 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release [1233 B]
Ign:7 http://<IP>:8000/all Release.gpg
Ign:8 http://<IP>:8000/stm32mp1 Release.gpg
Ign:9 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release.gpg
Get:10 http://<IP>:8000/all Packages [82.8 kB]
Get:11 http://<IP>:8000/stm32mp1 Packages [173 kB]
Get:12 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Packages [1734 kB]
Fetched 1994 kB in 3s (662 kB/s)
Reading package lists... Done
The other apt-*
commands are now available as described above.
4. Support[edit source]
Bug reports, request for new packages, or any other kind of support requests can be submitted through https://community.st.com.
5. Further readings[edit source]
- Dpkg
- https://manpages.debian.org/stable/apt/apt-get.8.en.html
- https://manpages.debian.org/stable/apt/sources.list.5.en.html
- https://manpages.debian.org/stable/apt/apt-cache.8.en.html
- https://wiki.debian.org/DebianRepository/Setup
- https://wiki.debian.org/DebianRepository/SetupWithReprepro
- https://wiki.debian.org/SecureApt
- STM32MP15 Discovery kits - Starter Package
- STM32MP15_Evaluation boards - Starter Package
- STM32MP1 Developer Package