Registered User mNo edit summary |
Registered User mNo edit summary |
||
(20 intermediate revisions by 2 users not shown) | |||
Line 3: | Line 3: | ||
== Overview == | == Overview == | ||
To load and execute U-Boot in DDR with [[STM32CubeProgrammer]], you need first to follow the steps described in [[STM32MP15 resources#AN5275|AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders]] | To load and execute U-Boot (the programming service) in DDR with [[STM32CubeProgrammer]], you need first to follow the steps described in [[STM32MP15 resources#AN5275|AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders]]: | ||
# phase 0x1 | # Download phase {{Highlight|0x1}} by ROM code, the FSBL = [[TF-A_overview|TF-A]] BL2 | ||
# phase 0x3 | # Download phase {{Highlight|0x0}} by FSBL = flashlayout (mandatory on STM32MP15x) | ||
# Download phase {{Highlight|0x3}} by FSBL, the FIP file including the SSBL image: [[U-Boot_overview|U-Boot]] | |||
The FSBL, SSBL and FIP definitions can be found in the [[Boot chain overview]] (FIP includes the required SSBL). | The FSBL, SSBL and FIP definitions can be found in the [[Boot chain overview]] (FIP includes the required SSBL). | ||
Line 12: | Line 13: | ||
See [[STM32CubeProgrammer#FAQs| FAQ of STM32CubeProgrammer]] for answers to questions specific to this tool. | See [[STM32CubeProgrammer#FAQs| FAQ of STM32CubeProgrammer]] for answers to questions specific to this tool. | ||
For information, the required '''DFU detach''' is automatically managed by STM32CubeProgrammer when flashlayout is used or with start command in CLI mode. | |||
== Prepare U-Boot to use the console == | == Prepare U-Boot to use the console == | ||
Line 20: | Line 23: | ||
* For USB boot, you can easily interrupt this command <code>stm32prog usb 0</code>by pressing <code>Ctr</code> + <code>C</code> in the console without U-Boot modification. | * For USB boot, you can easily interrupt this command <code>stm32prog usb 0</code>by pressing <code>Ctr</code> + <code>C</code> in the console without U-Boot modification. | ||
* For UART boot, the U-Boot console is deactivated to execute the <code>stm32prog serial ${boot_instance}</code> command in the [[U-Boot_overview#bootcmd|bootcmd]].<br/>To use the U-Boot console after STM32CubeProgrammer load, you can deactivate this behavior by: | * For UART boot, the U-Boot console is deactivated to execute the <code>stm32prog serial ${boot_instance}</code> command in the [[U-Boot_overview#bootcmd|bootcmd]].<br/>To use the U-Boot console after STM32CubeProgrammer load, you can deactivate this behavior by: | ||
** deactivate CONFIG_CMD_STM32PROG_SERIAL: | ** deactivate CONFIG_CMD_STM32PROG_SERIAL using one of the following method: | ||
*** use <code>make menuconfig</code> as explained in [[U-Boot_overview#Kbuild|Kbuild]] | *** use <code>make menuconfig</code> as explained in [[U-Boot_overview#Kbuild|Kbuild]] | ||
*** add the line <code> # CONFIG_CMD_STM32PROG_SERIAL is not set</code> in your defconfig (for example stm32mp15_trusted_defconfig) | *** add the line <code> # CONFIG_CMD_STM32PROG_SERIAL is not set</code> in your defconfig (for example stm32mp15_trusted_defconfig) | ||
Line 37: | Line 40: | ||
== Load U-Boot using Flashlayout == | == Load U-Boot using Flashlayout == | ||
You can use a minimal [[STM32CubeProgrammer_flashlayout#FlashLayout_file_to_load_and_start_U-Boot|"FlashLayout.tsv"]] files for <dev> serial boot (see [[STM32CubeProgrammer_flashlayout]] for file format details): | You can use a minimal [[STM32CubeProgrammer_flashlayout#FlashLayout_file_to_load_and_start_U-Boot|"FlashLayout.tsv"]] files for {{Highlight|<dev>}} serial boot, {{Highlight|<dev>}}=usb or uart (see [[STM32CubeProgrammer_flashlayout]] for file format details): | ||
#Opt id Name Type IP Offset Binary | #Opt id Name Type IP Offset Binary | ||
- 0x01 fsbl Binary none 0x00000000 tf-a_{{Highlight|<dev>}}.stm32 | - {{Highlight|0x01}} fsbl Binary none 0x00000000 tf-a_{{Highlight|<dev>}}.stm32 | ||
- 0x03 fip Binary none 0x00000000 fip.bin | - {{Highlight|0x03}} fip Binary none 0x00000000 fip.bin | ||
You can then use this with STM32CubeProgrammer command: | You can then use this with STM32CubeProgrammer command: | ||
Line 53: | Line 56: | ||
== Load U-Boot using CLI == | == Load U-Boot using CLI == | ||
You can also use the '''-d''' | You can also use the CLI interface with the options '''-d''' and '''-s''' to load and start U-Boot. | ||
{{PC$}} STM32_Programmer_CLI --help | |||
Available commands for STM32 MPU: | |||
.. | |||
-s, --start | |||
-g, --go : Run the code at the specified partition ID. | |||
[<partitionID>] : Partition ID | |||
If not specified, last loaded partition | |||
will be started | |||
.. | |||
-d, --download : Download the content of a file into device memory | |||
<file_path> : File path name to be downloaded: (bin, stm32 file | |||
<partition_id> : Partition ID to be downloaded | |||
For serial USB boot, {{Highlight|<dev>}}={{Highlight|usb}} device with port={{HighlightParam|usb1}}. | For serial USB boot, {{Highlight|<dev>}}={{Highlight|usb}} device with port={{HighlightParam|usb1}}. | ||
{{PC$}} STM32_Programmer_CLI -c port={{HighlightParam|usb1}} \ | {{PC$}} STM32_Programmer_CLI -c port={{HighlightParam|usb1}} \ | ||
-d tf-a_{{Highlight|usb}}.stm32 0x1 -s 0x1 \ | -d tf-a_{{Highlight|usb}}.stm32 {{Highlight|0x1}} -s {{Highlight|0x1}} \ | ||
-d flashlayout.stm32 0x0 -s 0x0 \ | -d {{HighlightParam|flashlayout.stm32}} {{Highlight|0x0}} -s {{Highlight|0x0}} \ | ||
-d fip.bin 0x3 -s 0x3 | -d fip.bin {{Highlight|0x3}} -s {{Highlight|0x3}} | ||
It is the same for serial UART boot with {{Highlight|<dev>}} ={{Highlight|uart}} and {{HighlightParam|port}} = the UART Interface identifier. | It is the same for serial UART boot with {{Highlight|<dev>}}={{Highlight|uart}} and {{HighlightParam|port}}= the UART Interface identifier. | ||
For information, loading a flashlayout file with [[STM32_header_for_binary_files|STM32 header]] for phase 0x0, even empty, is mandatory today but | For information, loading a flashlayout file {{HighlightParam|flashlayout.stm32}} with [[STM32_header_for_binary_files|STM32 header]] for phase 0x0, even empty, is mandatory today but will be removed in future release. | ||
You can generate this empty flashlayout.stm32 file with U-Boot mkimage with the following Linux shell commands: | You can generate this empty {{HighlightParam|flashlayout.stm32}} file with U-Boot mkimage with the following Linux shell commands: | ||
{{PC$}} echo "" > flashlayout.tsv | {{PC$}} echo "" > flashlayout.tsv | ||
{{PC$}} mkimage -T stm32image -a 0xC0000000 -e 0xC0000000 -d flashlayout.tsv flashlayout.stm32 | {{PC$}} mkimage -T stm32image -a 0xC0000000 -e 0xC0000000 -d flashlayout.tsv {{HighlightParam|flashlayout.stm32}} | ||
== Load U-Boot script using CLI == | |||
When the .stm32 file {{HighlightParam|flashlayout.stm32}} is replaced by a U-Boot script {{HighlightParam|script.stm32}} with U-Boot image header added by <code>mkimage</code> U-Boot tool, this script will be executed automatically by U-Boot. | |||
Example for a simple script to start U-Boot in dfu mode and then reset : | |||
dfu 0 | |||
reset | |||
{{PC$}} echo "dfu 0; reset" > script.cmd | |||
{{PC$}} mkimage -C none -A arm -T script -d script.cmd script.uimg | |||
{{PC$}} mkimage -T stm32image -a 0xC0000000 -e 0xC0000000 -d script.uimg {{HighlightParam|script.stm32}} | |||
{{PC$}} STM32_Programmer_CLI -c port={{HighlightParam|usb1}} \ | |||
-d tf-a_{{Highlight|usb}}.stm32 {{Highlight|0x1}} -s {{Highlight|0x1}} \ | |||
-d {{HighlightParam|script.stm32}} {{Highlight|0x0}} -s {{Highlight|0x0}} \ | |||
-d fip.bin {{Highlight|0x3}} -s {{Highlight|0x3}} | |||
<noinclude> | <noinclude> |
Latest revision as of 13:13, 1 October 2021
This page explains how to load and start U-Boot with STM32CubeProgrammer over a UART or USB port.
1. Overview[edit source]
To load and execute U-Boot (the programming service) in DDR with STM32CubeProgrammer, you need first to follow the steps described in AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders:
- Download phase 0x1 by ROM code, the FSBL = TF-A BL2
- Download phase 0x0 by FSBL = flashlayout (mandatory on STM32MP15x)
- Download phase 0x3 by FSBL, the FIP file including the SSBL image: U-Boot
The FSBL, SSBL and FIP definitions can be found in the Boot chain overview (FIP includes the required SSBL).
This feature can be used to debug U-Boot features required for the programming service (USB support, Flash device support, and so on) during board bring-up.
See FAQ of STM32CubeProgrammer for answers to questions specific to this tool.
For information, the required DFU detach is automatically managed by STM32CubeProgrammer when flashlayout is used or with start command in CLI mode.
2. Prepare U-Boot to use the console[edit source]
By default in the STM32 boot command the stm32prog
command is executed when the boot device is UART or USB to allow U-Boot (the programming service) to communicate with STM32CubeProgrammer.
To access to U-Boot console when U-Boot is loaded with STM32CubeProgrammer:
- For USB boot, you can easily interrupt this command
stm32prog usb 0
by pressingCtr
+C
in the console without U-Boot modification. - For UART boot, the U-Boot console is deactivated to execute the
stm32prog serial ${boot_instance}
command in the bootcmd.
To use the U-Boot console after STM32CubeProgrammer load, you can deactivate this behavior by:- deactivate CONFIG_CMD_STM32PROG_SERIAL using one of the following method:
- use
make menuconfig
as explained in Kbuild - add the line
# CONFIG_CMD_STM32PROG_SERIAL is not set
in your defconfig (for example stm32mp15_trusted_defconfig)
- use
- recompile U-Boot
- deactivate CONFIG_CMD_STM32PROG_SERIAL using one of the following method:
Before ecosystem release <span title="Main software components:
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision">v3.0.0 :
3. Load U-Boot using Flashlayout[edit source]
You can use a minimal "FlashLayout.tsv" files for <dev> serial boot, <dev>=usb or uart (see STM32CubeProgrammer_flashlayout for file format details):
0x01 fsbl Binary none 0x00000000 tf-a_<dev>.stm32 - 0x03 fip Binary none 0x00000000 fip.bin#Opt id Name Type IP Offset Binary -
You can then use this with STM32CubeProgrammer command:
<dev_port> -w FlashLayout.tsvPC $> STM32_Programmer_CLI -c port=
With
- For USB: <dev> = usb and <dev_port>=usb1
- For UART: <dev> =uart and <dev_port>= UART Interface identifier (ex COM1, /dev/ttyS0,...)
4. Load U-Boot using CLI[edit source]
You can also use the CLI interface with the options -d and -s to load and start U-Boot.
MPU: .. -s, --start -g, --go : Run the code at the specified partition ID. [<partitionID>] : Partition ID If not specified, last loaded partition will be started .. -d, --download : Download the content of a file into device memory <file_path> : File path name to be downloaded: (bin, stm32 file <partition_id> : Partition ID to be downloadedPC $> STM32_Programmer_CLI --help Available commands for STM32
For serial USB boot, <dev>=usb device with port=usb1.
usb1 \ -d tf-a_usb.stm32 0x1 -s 0x1 \ -d flashlayout.stm32 0x0 -s 0x0 \ -d fip.bin 0x3 -s 0x3PC $> STM32_Programmer_CLI -c port=
It is the same for serial UART boot with <dev>=uart and port= the UART Interface identifier.
For information, loading a flashlayout file flashlayout.stm32 with STM32 header for phase 0x0, even empty, is mandatory today but will be removed in future release.
You can generate this empty flashlayout.stm32 file with U-Boot mkimage with the following Linux shell commands:
flashlayout.stm32PC $> echo "" > flashlayout.tsv PC $> mkimage -T stm32image -a 0xC0000000 -e 0xC0000000 -d flashlayout.tsv
5. Load U-Boot script using CLI[edit source]
When the .stm32 file flashlayout.stm32 is replaced by a U-Boot script script.stm32 with U-Boot image header added by mkimage
U-Boot tool, this script will be executed automatically by U-Boot.
Example for a simple script to start U-Boot in dfu mode and then reset :
dfu 0
reset
script.stm32PC $> echo "dfu 0; reset" > script.cmd PC $> mkimage -C none -A arm -T script -d script.cmd script.uimg PC $> mkimage -T stm32image -a 0xC0000000 -e 0xC0000000 -d script.uimg
usb1 \ -d tf-a_usb.stm32 0x1 -s 0x1 \ -d script.stm32 0x0 -s 0x0 \ -d fip.bin 0x3 -s 0x3PC $> STM32_Programmer_CLI -c port=