Registered User m (Update LUCK reference) |
Registered User mNo edit summary |
||
(2 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
The Crypto API is a cryptography framework in the Linux<sup>®</sup> kernel. It is dedicated to the parts of the kernel that deal with cryptography, such as IPsec and dm-crypt. | The Crypto API is a cryptography framework in the Linux<sup>®</sup> kernel. It is dedicated to the parts of the kernel that deal with cryptography, such as IPsec and dm-crypt. | ||
Line 48: | Line 36: | ||
*'''hash''', '''cryp''' and '''crc32''' (Kernel space) | *'''hash''', '''cryp''' and '''crc32''' (Kernel space) | ||
These are the cryptographic Linux drivers handling the | These are the cryptographic Linux drivers handling the internal peripherals. | ||
*'''HASH''', '''CRYP''' and '''CRC''' (Hardware) | *'''HASH''', '''CRYP''' and '''CRC''' (Hardware) | ||
Line 54: | Line 42: | ||
===API description=== | ===API description=== | ||
The Crypto API is documented in the Linux Kernel Crypto API section of the Linux Kernel documentation<ref> | The Crypto API is documented in the Linux Kernel Crypto API section of the Linux Kernel documentation<ref>{{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API}} the official crypto API kernel documentation</ref>. It offers both a kernel and a userland interface: | ||
*kernel internal interface, used in particular by dm-crypt. | *kernel internal interface, used in particular by dm-crypt. | ||
*userland algorithm interface (socket) named AF_ALG<ref> | *userland algorithm interface (socket) named AF_ALG<ref>{{DocSource | domain=Linux kernel | path=crypto/userspace-if.html | text=Crypto API Userland interface}} specification of the userland API</ref>. OpenSSL can use this interface. | ||
In addition to the socket user interface, a more friendly interface, the cryptodev, can be used. It offers the /dev/crypto ioctl API. It is roughly described by the cryptodev.h<ref>[https://github.com/nmav/cryptodev-linux/blob/master/crypto/cryptodev.h cryptodev.h] cryptodev header file specifying the userland API</ref> header file. OpenSSL can be configured to use this interface as an alternative to the historical AF_ALG interface. | In addition to the socket user interface, a more friendly interface, the cryptodev, can be used. It offers the /dev/crypto ioctl API. It is roughly described by the cryptodev.h<ref>[https://github.com/nmav/cryptodev-linux/blob/master/crypto/cryptodev.h cryptodev.h] cryptodev header file specifying the userland API</ref> header file. OpenSSL can be configured to use this interface as an alternative to the historical AF_ALG interface. | ||
==Configuration == | ==Configuration == | ||
===Kernal configuration === | |||
The Crypto API is activated by default in ST deliveries. Nevertheless, if a specific configuration is required, you can use Linux Menuconfig tool: [[Menuconfig or how to configure kernel | Menuconfig or how to configure kernel ]] and select: | The Crypto API is activated by default in ST deliveries. Nevertheless, if a specific configuration is required, you can use Linux Menuconfig tool: [[Menuconfig or how to configure kernel | Menuconfig or how to configure kernel ]] and select: | ||
Line 70: | Line 59: | ||
[*] Support for STM32 crypto accelerators | [*] Support for STM32 crypto accelerators | ||
</pre> | </pre> | ||
===Devicetree configuration === | |||
By default the drivers are not enabled, so this needs to be added if you want to use HW accelerators. | |||
* crc: [[CRC_device_tree_configuration]]. | |||
* hash: [[HASH_device_tree_configuration]]. | |||
* crypto: [[CRYP_device_tree_configuration]]. | |||
== How to use the Crypto API framework== | == How to use the Crypto API framework== | ||
The Crypto API framework can be used by other kernel modules. | The Crypto API framework can be used by other kernel modules. | ||
The Crypto API documentation provides kernel code examples<ref> | The Crypto API documentation provides kernel code examples<ref>{{DocSource | domain=Linux kernel | path=crypto/api-samples.html | text=Crypto API kernel code examples}} some kernel code examples using the Crypto API framework</ref>: | ||
* Symmetric-key cipher operation. | * Symmetric-key cipher operation. | ||
* Operational state memory with SHASH. | * Operational state memory with SHASH. | ||
Line 113: | Line 108: | ||
==References== | ==References== | ||
<references /> | |||
< | <noinclude> | ||
[[Category:Crypto|0]] | |||
{{PublicationRequestId | 7954 | 2018-06-29 | AnneJ}} | |||
{{ArticleBasedOnModel | Framework overview article model}} | |||
{{ReviewsComments|JCT 1840: alignment needed with the last version of the model | |||
[[Category:ToBeAlignedWithModel]] | |||
}} | |||
</noinclude> |
Latest revision as of 11:52, 19 October 2020
The Crypto API is a cryptography framework in the Linux® kernel. It is dedicated to the parts of the kernel that deal with cryptography, such as IPsec and dm-crypt.
1. Framework purpose[edit source]
The purpose of this article is to introduce the Crypto API framework:
- general information
- main component/stakeholders
- how to use the Crypto API
- use cases
The Crypto API framework mainly includes all popular hash and block ciphers (encryption) functions.
A hash is a string or number generated from a text string. The length of the resulting string or number is fixed and widely varies with small variations of the input. The best hashing algorithms are designed so that it is impossible to turn a hash back into its original string. Hashing is particularly useful to compare a value with a stored value. However it cannot store its plain representation for security reasons. This makes hashing an ideal solution to store passwords.
Encryption turns data into a series of unreadable characters which length is not fixed. The encrypted strings can reversed back into their original decrypted form if the right key is not provided. Encrypting a confidential file is a good way to prevent anyone from accessing its content.
Drivers for CRYP (block cipher), HASH (hash) and CRC (cyclic redundancy check) are integrated within the Crypto API kernel service.
2. System overview[edit source]
2.1. Description of the components[edit source]
From User space to hardware
- OpenSSL (User space)
OpenSSL[1] is a software library supporting the TLS and SSL protocols as well as cryptographic functions. Openssl is available in OpenSTLinux distribution.
- dm-crypt (Kernel space)
dm-crypt[2] is a kernel disk encryption subsystem. It is natively available in the standard Linux kernel.
- Cryptodev (Kernel space)
Cryptodev[3] is a device driver which provides a general interface for userland applications. Although it is not part of the standard Linux kernel, it is available in OpenSTLinux distribution.
- CryptoAPI core (Kernel space)
This layer represents the standard Linux kernel cryptographic framework.
- hash, cryp and crc32 (Kernel space)
These are the cryptographic Linux drivers handling the internal peripherals.
- HASH, CRYP and CRC (Hardware)
These HW blocks handle hash, ciphering, and CRC checksum.
2.2. API description[edit source]
The Crypto API is documented in the Linux Kernel Crypto API section of the Linux Kernel documentation[4]. It offers both a kernel and a userland interface:
- kernel internal interface, used in particular by dm-crypt.
- userland algorithm interface (socket) named AF_ALG[5]. OpenSSL can use this interface.
In addition to the socket user interface, a more friendly interface, the cryptodev, can be used. It offers the /dev/crypto ioctl API. It is roughly described by the cryptodev.h[6] header file. OpenSSL can be configured to use this interface as an alternative to the historical AF_ALG interface.
3. Configuration[edit source]
3.1. Kernal configuration[edit source]
The Crypto API is activated by default in ST deliveries. Nevertheless, if a specific configuration is required, you can use Linux Menuconfig tool: Menuconfig or how to configure kernel and select:
API ---> [*] Hardware crypto devices ---> [*] Support for STM32 crc accelerators [*] Support for STM32 hash accelerators [*] Support for STM32 crypto accelerators[*] Cryptographic
3.2. Devicetree configuration[edit source]
By default the drivers are not enabled, so this needs to be added if you want to use HW accelerators.
- crc: CRC_device_tree_configuration.
- hash: HASH_device_tree_configuration.
- crypto: CRYP_device_tree_configuration.
4. How to use the Crypto API framework[edit source]
The Crypto API framework can be used by other kernel modules.
The Crypto API documentation provides kernel code examples[7]:
- Symmetric-key cipher operation.
- Operational state memory with SHASH.
5. Use cases[edit source]
- Disk encryption
This is a typical example of Crypto API framework usage. Refer to LUKS[8] for a standard disk encryption process.
6. How to trace and debug the framework[edit source]
6.1. How to monitor[edit source]
The list of available ciphers is given in /proc/crypto:
cat /proc/crypto
Output part showing that an STM32 driver provides with the CRC32 cipher:
...
name : crc32
driver : stm32-crc32
module : kernel
priority : 200
refcnt : 1
selftest : passed
internal : no
type : shash
blocksize : 1
digestsize : 4
...
6.2. How to trace[edit source]
There are no specific traces for this framework.
6.3. How to debug[edit source]
There are no specific debug means for this framework.
7. Generic source code location[edit source]
8. References[edit source]
- ↑ OpenSSL a software library supporting the TLS and SSL protocols as well as cryptographic functions.
- ↑ dm-crypt a kernel disk encryption subsystem
- ↑ Cryptodev a device driver which provides a general interface for userland applications
- ↑ Linux Kernel Crypto API the official crypto API kernel documentation
- ↑ Crypto API Userland interface specification of the userland API
- ↑ cryptodev.h cryptodev header file specifying the userland API
- ↑ Crypto API kernel code examples some kernel code examples using the Crypto API framework
- ↑ LUKS (Linux Unified Key Setup ) a disk encryption specification