This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.deleted>Frq08942 mNo edit summary |
Registered User mNo edit summary |
||
Line 1: | Line 1: | ||
When a GPU animation is running on the display, the related GCNANO estimated GPU load can be monitored from the [[Vivante GCNANO GPU overview | GCNANO driver]] level, by using the following command: | When a GPU animation is running on the display, the related GCNANO estimated GPU load can be monitored from the [[Vivante GCNANO GPU overview | GCNANO driver]] level, by using the following command: | ||
{{Board$}} (while true; do (tr -d '\n' < /sys/kernel/debug/gc/idle | awk -F" " '{printf("gpu load %.0f%%\n", $6*100/($4-$2));}'); sleep 4; done) & | {{Board$}} (while true; do (tr -d '\n' < /sys/kernel/debug/gc/idle | awk -F" " '{printf("gpu load %.0f%%\n", $6*100/($4-$2));}'); sleep 4; done) & | ||
Line 30: | Line 21: | ||
Off: 0 ns | Off: 0 ns | ||
... | ... | ||
<noinclude> | |||
{{PublicationRequestId | 10256 | 2019-01-15 | PhilipS}} | |||
[[Category:GPU]] | |||
[[Category:How to trace and debug]] | |||
</noinclude> |
Revision as of 17:32, 4 October 2019
When a GPU animation is running on the display, the related GCNANO estimated GPU load can be monitored from the GCNANO driver level, by using the following command:
Template:Board$ (while true; do (tr -d '\n' < /sys/kernel/debug/gc/idle | awk -F" " '{printf("gpu load %.0f%%\n", $6*100/($4-$2));}'); sleep 4; done) &
The GCNANO estimated GPU load is then periodically output in the user console as a percentage "%":
gpu load 75%
gpu load 75%
gpu load 75%
Notes:
- Stop monitoring the GPU load with the command "kill -9 `ps -o ppid= -C sleep`".
- Adjust the GPU load update period by modifying the "sleep" value (4 seconds in the example).
- Use the command "dmesg -n8" to mix both user and kernel console outputs.
- Debugfs configuration needs to be enabled.
- The detailed calculation is: GPU load = On/(End-Start) with "On, End & Start" coming from the command:
Template:Board$ cat /sys/kernel/debug/gc/idle Start: 3488941301162 ns End: 3549591148649 ns On: 26672154276 ns Off: 0 ns ...