Revision as of 16:51, 5 October 2020 by Registered User

1. Test purpose

Received Signal Strength Indicator (RSSI) is a measurement of the power level of the received radio signal.

The TX/RX page allows user to transmit a continuous wave RF signal and in same time to receive the signal and display dynamically the RSSI on the chart.

2. Explaining the dashboard

The TX RX dashboard is divided in three areas :

  • The left part is for TX transmission that allows the user to choose the RF frequency and the power level of emission (between -9 to 22 dBm). User can start and stop emission with the buttons. when board is connected, the LED is green. When transmission is ongoing, the signal indicator is green.
  • The right part is for RX reception that allows the user to choose the RF frequency. User can start and stop reception. when reception is started, the signal icon is green.
  • The bottom area is showing the RSSI level in a gauge and a chart that is refreshed each 250 ms when reception is started.
RXTX Dashboard.png

3. Explaining the flow

The TXRX flow is a combination of TX and RX flows. The TX flow is in charge of handling emission of signal while the RX flow is handling reception.

The emitter must be connected to Serial Port A. The receiver must be connected to Serial Port B.

3.1. TX flow

TX flow manages the sequence of AT commands to the emitter. A finite state machine (FSM) is used to manage the sequence of AT command and target response. The parameters (RF Frequency and TX Power) are stored in flow variables when they are edited. The FSM status and transitions are corresponding to the normal sequence of AT command and abnormal response from target is also handled. The steps are to configure the board with stored parameters, and then start transmission. When stop button is pressed, board is stopped and FSM goes to STOPPED state. The LED indicating that the TX board is connected to the application is also managed by this flow.

TX Flow.png

3.2. RX flow

RX flow manages the sequence of AT commands to the receiver. A finite state machine (FSM) is used to manage the sequence and the target responses. The FSM configures the board, then starts a first RSSI measurement. After each measurement, the flow waits 250 ms and then starts a new measurement. (This time between measurements can be changed in the flow with the delay node). The LED indicating that the RX board is connected to the application is also managed by this flow. The measurement results are decoded and displayed in the "RSSI" gauge and in the "RSSI" chart.

RX Flow.png

4. AT commands for TX RX commands

AT commands listed below are used by emitter and receiver flows

4.1. Emitter :

ATZ Reset the board

AT+TCONF=freq:pow:bw:sf:cr:lna:pa:modulation:payloadLen:fskDeviation:lowDrOpt:BTproduct. Sets the configuration for RF test.

For example : AT+TCONF=868000000:14:4:12:4/6:0:0:1:16:25000:2:3

AT+TTONE Start the TX transmission

AT+TOFF Stop the TX transmission


4.2. Receiver:

AT+Z Reset

AT+TCONF=freq:pow:bw:sf:cr:lna:pa:modulation:payloadLen:fskDeviation:lowDrOpt:BTproduct. Sets the configuration for RF test.

For example : AT+TCONF=868000000:14:4:12:4/6:0:0:1:16:25000:2:3

AT+TRRSSI Start the RX reception and RSSI measurement

AT+TOFF Stop the RX reception