1. Fixed issues
ID | Summary |
---|---|
134507 | Unable to install STM32CubeIDE on Fedora 37. |
154575 | Could not rebuild a Non secure project when switch between project structure. |
156010 | The first connection to target sometimes fails, next connections are OK. This impact Cortex-M debug in production mode and Linux deployment and user space debug . |
158342 | Once the LTO optimization feature is enabled for WBA project BLE_SerialCom_Peripheral, the linker file fails and STM32CubeIDE fails to produce the binary file as output. |
159215 | Post build commands generation issue in secure manager projects is detected once the Sign Binary is unselected and selected again. |
160474 | Wrong value displayed in SFR view of ADC_CALFACT while using STM32U5A5 board. |
163129 | On macOS 14.0 Sonoma we noticed this behavior :
The splash screen issue on eclipse is already reported in this thread: https://github.com/eclipse-platform/eclipse.platform.swt/issues/772 and also here https://github.com/eclipse-platform/eclipse.platform.swt/issues/751.
|
164737 | Memory content is not updated correctly if a global variable is added mid debug session. |
165302 | Build error for board H563ZI due to missing stm32h5xx_hal_usart.h. |
165526 | Post Build commands failure for H5 board in secure project with trust zone enabled. |
165850 | Failed to build a static library project from STM32cubeIDE for the STEVAL-MKBOXPRO board with an unknown type name "GFXTIM_TypeDef" because the hal_conf_template has all IPs enabled. |
166705 | When installing two different versions of STM32CubeCLT under Fedora 36, the second installation is failed with the error “Fedora_error_Installation”. |
166792 | USB device error "libusb couldn't open usb device /dev/bus/usb/.../..." when trying to Upgrade STLink firmware via command line on Fedora 36, to hijack this behavior you need to do the following:
> sudo chmod o+w /dev/bus/usb/.../... |
167678 | Display issue detected when reducing the size of the interface. |
169188 | Disassembly view doesn't show assembly instructions after adding the view and restarting the debug session. |
170446 | Crush in STM32CubeIDE while searching for NVIC in SFR view. |
171950 | Wrong definition of the PNB bits. The missing bits are :
BKER MER2 SEC_PROT2 |
174840 | When installing two different versions of STM32CubeCLT on Ubuntu, the second installation failed with and error “Error_Second_Installation_Ubuntu”. |
2. Limitations
ID | Summary |
---|---|
138771 | To start debugging in the NS zone when the product status is TZ-Closed for the STM32H5 using ST-Link GDBServer, add the following script to "Run Commands" in the debugging configuration.
set breakpoint always-inserted on tbreak Reset_Handler monitor reset set breakpoint always-inserted off si For the "Reset & Restart" button to work: |
156539 | If the user needs to set a proxy to be authenticated, a check for connection should be done: Windows > Preferences > STM32Cube > Firmware Updater and then Check Connection. |
166245 | When using the STM32CubeMP13 bare-metal firmware and activating Azure® RTOS
ThreadX, the STM32CubeIDE linker file must contain the following section to avoid compilation issues: .stack : { _stack_bottom = ABSOLUTE(.) ; /* Allocate room for stack. This must be big enough for the IRQ, FIQ, and SYS stack if nested interrupts are enabled.*/ . = ALIGN(8) ; . += 32768 ; _sp = . - 16 ; _stack_top = ABSOLUTE(.) ; } >RAM _end = .; |
168716 | In Order to debug an application project for STM32H7RS board, the debug config, startup tab and both elf files app.elf need to be added first and Boot.elf second. |
174727 | STM32CubeIDE cannot make the project build automatically after having changed the IP configuration, it cannot automatically control this configuration, the user needs to increase Flash size manually when needed depending on his configuration. |
3. Known issues
The known issues are split into general, STM32CubeCLT, OS-specific, and target-specific issues.
3.1. General issues
ID | Summary |
---|---|
59435 | Having a space or non-ASCII character in the project/workspace path or installation path is not fully supported. |
63624 | Some STM32CubeMX pop-up dialogs are not opened in front of the STM32CubeIDE workbench on all OS's. |
68184 | Hierarchical projects cannot be imported with the option Copy into workspace. |
68440 | Hierarchical projects cannot be renamed. |
89454 | Restart configuration only works for flash memory projects and not for RAM projects. Program Counter register is not set correctly. Manual work-around: In Restart configuration, manually set PC to the ResetHandler() in RAM: set $pc = 0x20000xxx. |
109764 | FreeRTOS™ kernel-aware debugging: Full stack traces off all tasks do not work if configUSE_PORT_OPTIMISED_TASK_SELECTION 1 |
115928 | Editing live expressions while target is running does not work with SEGGER J-Link. |
124062- 152549 | GCC-10 is more strict with respect to declaration of global variables in header files. Read the GCC-10 porting guide, so many warnings and errors result. |
133183 | STM32CubeIDE cannot debug using FreeRTOS aware with J-LINK.
Work-arounds, if: Reset strategy == Connect under reset, requires Initialization commands: info threads info threads thread 2 Work-arounds, if: Reset strategy == None (attach mode), requires Initialization commands: info threads info threads thread 2 stepi |
159507 | Issues detected when updating STM23CubeIDE version from 1.9.0 to 1.13.1. |
165998- 170209 | To successfully run the Debug Authentication using STM32CubeIDE. STMCubeProgrammer needs to be installed as well. |
169316 | When building an existing project, using GCC11 or GCC12, a warning should be noticed : “elf has a LOAD segment with RWX permissions”.
This warning highlights a vulnerability, to correct it and secure the data section, we suggest to update the linker files: From this kind of section : .preinit_array : { … } >FLASH To: .preinit_array (READONLY) : { … } >FLASH But it’s incompatible with GCC10 and earlier versions. |
170279 | Failure to compile embOS due to missing stack variable as a new section defining _stack_start__ and __stack_end__ in linker file need to be added in linker file once it is required by ThreadX. |
3.2. OS-specific issues
3.2.1. Linux®
ID | Summary |
---|---|
139617 | The CAD view in the ioc-editor may not render. A restart of STM32CubeIDE is required. |
3.2.2. Mac®
ID | Summary |
---|---|
163129 | On macOS 14.0 Sonoma we noticed this behavior
-The "splash" screen during startup gets displayed upside down. The the splash screen issue on eclipse is already reported in this thread: https://github.com/eclipse-platform/eclipse.platform.swt/issues/772 and also here https://github.com/eclipse-platform/eclipse.platform.swt/issues/751 |
3.3. Target-specific issues
3.3.1. STM32H7
ID | Summary |
---|---|
73552 | Serial Wire Viewer configuration is not reset for STM32H7 devices on the next launch if it was terminated with record active when using ST-LINK GDB server. |
79658 | ST-LINK GDB server reports being suspended on address: 0x05F0001 when debugging STM32H7 dual-core devices and the core under debug goes to sleep. |
81763 | OpenOCD does not support debugging STM32H7 dual-core devices when the core under debug goes to sleep. |
175966 | H7RS project with ExtMemLoader context configured: Postbuild commands cannot be passed successfully if STM32CubeIDE is installed with sudo.
Workarounds:
|
3.3.2. STM32MP1
ID | Summary |
---|---|
73895 | Debugging in production mode requires a network connection. If STM32CubeIDE is configured to use a network proxy, then the IP address of the STM32MP1 board needs to be added to the "Proxy bypass" list. |
73896 | The synchronization check between the IP-address entered in launch configuration and the IP-address of the target does not abort the launch in case of mismatch. |
3.3.3. STM32WBA
ID | Summary |
---|---|
158985 | “Connect Under Reset” is not working with STM32WBA. |
4. Upgrades
ID | Summary |
---|---|
162901 | Update SEGGER J-Link to version 7.94h. |
166922 | Update GCC12 binaries to v12.3.rel1.20240306-1730. |
166924 | Update STLinkGDBServer to version 7.6.0. |
166925 | Update OpenOCD to version 0.12.0-00029-gf77e7cb03 (2023-12-15-13:25). |
166927 | Update STM32CubeProgrammer to version 2.16.0. |
166929 | Update the STM32CubeMX to version 6.11.0. |
166920 | Update the Make Version to 4.4.1_st_20231030-1220. |
166921 | Update the BusyBox Version to 1.31.0.st_20240131-1810. |
166932 | Update the Eclipse and CDT Version to Eclipse 2023-12 and CDT 11.4.0. |