Revision as of 11:13, 21 February 2024 by Registered User
This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or
pending task to finish installation of
Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Fixed issues
ID |
Summary
|
116898 |
STM32CubeIDE project converter do not work properly when using it from the MX example importer.
|
145859 |
Failure to import some projects due to their nominations.
|
147750 |
STM32CubeIDE G0 project Build fails after migrating on the latest versions of STM32CubeIDE.
|
148103 |
National / local characters used in the folder / file names leads to wrong path and not found files.
|
158617 |
Build projects fail in headless mode from STM32CubeIDE v1.13.0 due to new initUserAuthMenu() method.
|
160082 |
In GCC11 additional warnings are created at compile time, those warning are sent on stderr and considers as errors
|
162320 |
Version 11.3.rel1 of the GNU toolchain published on STM32CubeIDE 1.13.1 causes compilation errors after calling printf in projects reported in the community "https://community.st.com/t5/stm32-mcus-embedded-software/error-after-calling-printf/td-p/574044".
|
164005 |
Project for NUCLEO-L552ZE Build fails.
|
2. Limitations
ID |
Summary
|
138771 |
To start debugging in the NS zone when the product status is TZ-Closed for the STM32H5 using ST-Link GDBServer, add the following script to "Run Commands" in the debugging configuration.
set breakpoint always-inserted on
tbreak Reset_Handler
monitor reset
set breakpoint always-inserted off
si
For the "Reset & Restart" button to work:
- Add the same script
- Select "None" as the type.
|
156539 |
If the user needs to set a proxy to be authenticated, a check for connection should be done: Windows > Preferences > STM32Cube > Firmware Updater and then Check Connection.
|
159215 |
In certain cases, we may encounter a post-construction generation problem which results as follows.
1. If you want to deactivated firmware signing after build
a. Untick Sign binary in STM32CubeMX.
b. Generate Code.
c. Edit STM32CubeIDE properties and manually remove the “Postbuild” command: This is the workaround for the limitation.
2. After previous changes, if you can enable again the signature.
a. Tick Sign binary in STM32CubeMX.
b. Generate code.
|
166245 |
When using the STM32CubeMP13 bare-metal firmware and activating Azure® RTOS
ThreadX, the STM32CubeIDE linker file must contain the following section to avoid
compilation issues:
.stack :
{
_stack_bottom = ABSOLUTE(.) ;
/* Allocate room for stack. This must be big enough for the
IRQ, FIQ, and SYS stack if nested interrupts are
enabled.*/
. = ALIGN(8) ;
. += 32768 ;
_sp = . - 16 ;
_stack_top = ABSOLUTE(.) ;
} >RAM
_end = .;
|
3. Known issues
The known issues are split into general, STM32CubeCLT, OS-specific, and target-specific issues.
3.1. General issues
ID |
Summary
|
59435 |
Having a space or non-ASCII character in the project/workspace path or installation path is not fully supported.
|
63624 |
Some STM32CubeMX pop-up dialogs are not opened in front of the STM32CubeIDE workbench on all OS's.
|
68184 |
Hierarchical projects cannot be imported with the option Copy into workspace.
|
68440 |
Hierarchical projects cannot be renamed.
|
89454 |
Restart configuration only works for flash memory projects and not for RAM projects. Program Counter register is not set correctly. Manual work-around: In Restart configuration, manually set PC to the ResetHandler() in RAM: set $pc = 0x20000xxx.
|
109764 |
FreeRTOS™ kernel-aware debugging: Full stack traces off all tasks do not work if configUSE_PORT_OPTIMISED_TASK_SELECTION 1
|
115928 |
Editing live expressions while target is running does not work with SEGGER J-Link.
|
124062 - 152549 |
GCC-10 is more strict with respect to declaration of global variables in header files. Read the GCC-10 porting guide, so many warnings and errors result.
|
133183 |
STM32CubeIDE cannot debug using FreeRTOS aware with J-LINK.
Work-arounds, if: Reset strategy == Connect under reset, requires Initialization commands:
info threads
info threads
thread 2
Work-arounds, if: Reset strategy == None (attach mode), requires Initialization commands:
info threads
info threads
thread 2
stepi
|
154575 |
Could not rebuild a Non secure project when switch between Project Structure.
|
159507 |
Issues detected when updating STM23CubeIDE version from 1.9.0 to 1.13.1.
|
3.2. STM32CubeCLT issues
ID |
Summary
|
166792 |
USB device error "libusb couldn't open usb device /dev/bus/usb/.../..." when trying to Upgrade STLink firmware via command line on Fedora 36, to hijack this behavior you need to do the following:
> sudo chmod o+w /dev/bus/usb/.../...
|
3.3. OS-specific issues
3.3.1. Linux®
ID |
Summary
|
134507 |
Unable to install CubeIDE on Fedora 37. |
139617 |
The CAD view in the ioc-editor may not render. A restart of STM32CubeIDE is required. |
3.3.2. Mac®
3.4. Target-specific issues
3.4.1. STM32H7
ID |
Summary
|
73552 |
Serial Wire Viewer configuration is not reset for STM32H7 devices on the next launch if it was terminated with record active when using ST-LINK GDB server.
|
79658 |
ST-LINK GDB server reports being suspended on address: 0x05F0001 when debugging STM32H7 dual-core devices and the core under debug goes to sleep.
|
81763 |
OpenOCD does not support debugging STM32H7 dual-core devices when the core under debug goes to sleep.
|
3.4.2. STM32U5
ID |
Summary
|
163837 |
Failed to build a static library project from STM32cubeIDE for the STEVAL-STWINBX1 board with an unknown type name "GFXTIM_TypeDef" because the hal_conf_template has all IPs enabled.
|
165850 |
Failed to build a static library project from STM32cubeIDE for the STEVAL-MKBOXPRO board with an unknown type name "GFXTIM_TypeDef" because the hal_conf_template has all IPs enabled.
|
3.4.3. STM32MP1
ID |
Summary
|
73895 |
Debugging in production mode requires a network connection. If STM32CubeIDE is configured to use a network proxy, then the IP address of the STM32MP1 board needs to be added to the "Proxy bypass" list.
|
73896 |
The synchronization check between the IP-address entered in launch configuration and the IP-address of the target does not abort the launch in case of mismatch.
|
156010 |
First connection to target sometimes fails, next connections are OK. This impact Cortex-M debug in production mode and Linux deployment and user space debug.
|
4. Upgrades
ID |
Summary
|
162901 |
Update SEGGER J-Link to version 7.92n.
|