Getting started with MMT

Revision as of 16:38, 10 July 2023 by Registered User (→‎MMT)

This article explains what the Memory Mapping Tool (MMT) is and how to use it through examples.

1. What is MMT ?

MMT stands for Memory Management Tool. This STM32CubeMX feature handle the memory mapping in a more visual way. The tool goal is to make easy the creation, the partition and the deletion of memory blocks in RAM, FLASH or external memory (thanks to connectivity IP : OctoSPI & FMC). In fact, the MMT abstracts the difficulty from the linker file by providing a simple use.

2. Visual presentation

The MMT is under Tools > Memory Management.

2.1. Secure application

Let's introduce the Memory Management Tool with the picture below.

Screen S&NS MMT.png

The MMT pannel is split in 6 parts:
1. The main pannel is a memory view by the CPU and the application with addresses on the left.
2. The second point is the legend indicating the corresponding color from memory.
3. The third block is composed of two toggle buttons which indicates the Code Generation Configuration :

  • if the application regions settings are applied to peripherals
  • if the application regions settings will be applied into linker files during code generation.

4. This Search bar allows to easily find an application region
5. This fifth section shows the selected Application Region in the main pannel. It lists many useful information. (Code Name, Start address, Size, Security, Access Permission, Code execution, Shareability and Cacheability)
6. The Display Settings and Reset View handle the memory view and allow to hide Security or Reseved regions

2.2. Non Secure application

The Non Secure (NS) application have exactly the same interface except there aren't Secure (S) and Non Secure Callable (NSC) region. However, the principle remains strictly the same.

3. Configure MMT to handle memory

3.1. Objectives

  • Create a simple project with a Secure (S) and a Non-Secure (NS) application.​
  • Learn how to configure the memory through the tool.
  • Verify the correct functionality by checking the linker file.

3.2. Create the project in STM32CubeMX

  • File > New Project > Board Selector in the main panel or click on the shortcut Access to Board Selector.

Start Board.png

The example uses the NUCLEO-U575ZI-Q board.

  • Enter NUCLEO-U575ZI-Q in the Commercial Part Number as shown in the figure below.
  • Select the NUCLEO-U575ZI-Q in the Board List
  • And then click on Start Project.

Start Project.png

  • Select Yes in the pop-up window to initialize all peripherals with their default mode.

Initialize.png

  • Answer with TrustZone activated to the question "Do you want to create a new project ?" and OK

TZ activated.png

Info white.png Information
The project is by default neither saved nor named. You might save it in File > Save Project or Ctrl + S. Then, choose the name (eg: Test_MMT) and the location before clicking on Save

3.3. Memory zone definition

Go to the Memory Management Tool located under Tools > Memory Management. The memory is in the default case, we create two Application Regions :

3.3.1. Secure Application Region

  • Select the RAM (S) region at the address 0x30000000.
  • Change the size to 192kB.

Add Zone RAM S.png

  • A new Application Region appears in white, when you mouse over it, a green cross appears.

Add Zone Sec.png

  • Click on this green cross section and the popup below pops up.
  • In the Name field, enter App_Secure.
  • The Address is the base address from the selected memory block, you can keep it by default.
  • Change the Size to 64 kB.
  • Click on Add

Popup Secure.png

Info white.png Information
Note that a Reserved Alias Region (S) have been created in addition to the App_Secure

3.3.2. Non Secure Application Region

  • Select the RAM (NS) region at the address 0x20040000.
  • Change the size to 256 kB.

Add Zone RAM NS.png

  • A new Application Region appears in white, when you mouse over it, a green cross appears.

Add Zone MMT.png

  • Click on this green cross section and the popup below pops up.
  • In the Name field, enter App_NonSecure.
  • The Address is the base address from the selected memory block, you can keep it by default.
  • Change the Size to 128 kB.
  • Click on Add

Popup NonSecure.png

Info white.png Information
Note that a Reserved Alias Region (NS) have been created in addition to the App_NonSecure


Warning white.png Warning
Check that both memory areas have been created

3.3.3. Apply MMT

Go to code generation configuration as below:

  • Click on the first toggle button to apply Application Regions to Peripherals :

Apply periph.png

  • And Click on the second button to apply Application Regions into linker files during the code generation :

Apply linker.png

Warning white.png Warning
If you don't apply applications regions settings to peripherals or linker files, all changes will remain local to STM32CubeMx
Info white.png Information
Linker files (.ld) are accessible (Flash & RAM) once the project is generate

3.4. Pinout & Configuration

  • Now, go to Pinout & Configuration > System Core > SAU, the SAU is under MMT control and is Read Only.

Configure aplication.png

Info white.png Information
CORTEX_M33, FLASH and GTZC are also in Read Only. That means the MMT change has been applied correctly

3.5. Generate project and edit linker file

The easiest way to generate the code is to :

  • Click on Project Manager > Project > Project Settings
  • Enter a Project Name and select STM32CubeIDE in the ToolChain / IDE

Generate Project.png

  • Then select the Code Generator menu
  • Check the box to Generate peripheral initialization as a pair of '.c/.h' files per peripheral
  • Click on Generate Code

Generate CodeGenerator.png

Info white.png Information
Keep all the other settings in their default mode !
  • Click on Open Project

Open Project.png

  • On the left side of the screen in the project explorer, expand the tree structure (NS & S project).

Tree project.png

  • Open the linker files (.ld)
Info white.png Information
Linker files are the mapping source file for Secure and Non-Secure application.

Look at the memory definition :

  • Check that "App_Secure" has been declared in the Secure world and the "App_NonSecure" in the Non Secure world.

Memory definition.png

4. External memory

To go further, it's possible to manage external memory through MMT.
Go to Pinout & Configuration > Connectivity to configure interfaces.

Info white.png Information
For both OctoSPI & FMC, the setup is arbitrary.

4.1. OctoSPI

Active the OctoSPI in Non Secure as shown on the picture below.

  • Set the mode in Single SPI.
  • Select Port1 CLK for the CLK, Port1 NCS for the Chip Select and Port1 IO[1:0] for Data [3:0].
  • Choose the Device Type : RAM.

Ext Mem OctoSPI.png

4.2. FMC Bank

Active the FMC in Non Secure as shown on the picture below.

  • Choose the NE1 for the Chip Select
  • Configure the Memory type to NOR Flash.
  • Select 3bits for the Address, 16 bits for Data and Burst Read regarding the clock.
  • Tick the Address valid.

Ext Mem FMCBank.png

4.3. MMT

Once the configuration above is done,

  • Go to the MMT under Tools > Memory Management
  • Observe the activation of the External RAM (OctoSPI1) and the External Flash (FMC)

Ext Mem MMT.png

No categories assignedEdit