Coming soon |
1. Prerequisites
1.1. Host PC system requirements
1.1.1. Supported operating systems and architectures
- Windows® 7: 32 bits (x86), 64 bits (x64)
- Windows® 8.x: 32bits (x86), 64 bits (x64)
- Windows® 10: 32 bits (x86), 64 bits (x64)
- Linux® (tested on Red Hat®, Fedora® and Ubuntu® , 32 and 64 bits)
- macOS® (minimum version OS X® Yosemite)
1.1.2. ST-LINK driver
ST-LINK driver is required.
Install it from st.com.
1.1.3. ST-LINK server
ST-LINK server is required to use shared mode.
Install it from st.com
2. Hardware requirements
- One free USB2 or USB3 host port available on your device (Windows, Linux, or macOS).
- USB Type-A to Micro-B cable or Mini-B cable depending on target board
- STM32 target board
3. STM32CubeMonitor Installation
3.1. Windows operating system
- Double click setupSTM32CubeMonitor.exe to launch the installation wizard.
- Read the license agreement and accept it (if you reject it, the installation is aborted).
- Select "Create a desktop shortcut" if needed.
- Click next to launch the installation.
- The following dialog box is displayed when the installation is complete:
The application starts immediately after the installation has completed if the Launch STM32CubeMonitor box is checked.
3.2. Linux operating system
If you are using a USB port to connect to the STM32 microcontroller device, install the libusb1.0 package by typing the following command: sudo apt-get install libusb-1.0.0-dev
To use ST-LINK probe or USB DFU to connect to a target, copy the rule files located under the Driver/rules folder in /etc/udev/rules.d/ on Ubuntu ("sudo cp *.* /etc/udev/rules.d").
To install STM32CubeMonitor on under Linux, open a terminal window and enter the following command with root privileges:
sudo apt get install ./stm32cubemonitor_amd64.deb
A console opens to display the license information. Accept the license and start the installation. When it is complete, launch STM32CubeMonitor using the following command:
"run stm32cubemonitor.exe"
or click the application icon on the desktop.
3.3. macOS System
For macOS, launch setupSTM32CubeMonitor.dmg and into the installer window. A console will open to display license information. Accept license then drag and drop the STM32CubeMonitor icon on the Applications icon