This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Prerequisite
1.1. Host PC system requirements
1.1.1. Supported operations systems and architectures
- Windows® 7: 32-bit (x86), 64-bit (x64)
- Windows® 8.x: 32-bit (x86), 64-bit (x64)
- Windows® 10: 32-bit (x86), 64-bit (x64)
- Linux® (tested on Red Hat®, Fedora® and Ubuntu®, 32 and 64 bits)
- macOS® (minimum version OS X® Yosemite)
Note: macOS® is a trademark of Apple Inc. registered in the U.S. and other countries.
2. STM32CubeMonitor Installation
2.1. Windows system
2.2. Linux system
2.3. macOS System
3. Hardware support
One free USB2 or USB3 host port
USB Type-A to Micro-B cable or Mini-B cable depending on target board
STM32 target board