Revision as of 13:04, 12 February 2020 by Registered User (1 revision imported)

Template:ArticleMainWriter


STM32CubeMonitor allows to monitor several probes simultaneously, even if target are not similar.

In the example below, a Nucleo board L031K6 and a Discovery board F429ZI are used. Variables monitored are displayed in the same chart in the dashboard.


1. Design of the flow

Flows for each board are designed following method described in How to configure mandatory parameters before acquisition.

Then Start and Stop buttons are connected to variable node for each board, and finally processing node for each board are connected to the chart node.

multiprobe flow

2. Dashboard view

The corresponding dashboard shows that both variables are monitored on the same chart, with a legend corresponding to the board, float1(myVariableL031) and float1(myVariableF429)

dashboard view of a multiproble flow