This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
STM32CubeMonitor allows to write variables in target when running. Variables monitored as selected in How to configure mandatory parameters before acquisition can be overwritten in the target.
In the example below, a firmware of the Discovery board F429ZI is using a variable "t" that is slightly increased when target is running. This variable "t" is monitored and displayed in the chart.
1. Design of the flow
a "write" node is added to the flow as input of the acquisition out node.
2. Dashboard view
The end user can then fill value for the "t" variable and click on WRITE button to write the value in the memory target. Chart immediately reflects the change of this value.