How to perform additional calculations on measurements

Revision as of 10:47, 19 February 2020 by Registered User

A secondary feature of the processing node is the ability to perform calculations and statistics on the monitored variables.
These additional calculations and statistics are logged as variables (see article STM32CubeMonitor:How to record and replay data) and are added as outputs of the processing node to be rendered graphically, as for the other variables.

  • Operations on variables can be mathematical ( +, -, /, %, mod,...), trigonometry (sin(), cos(), tan()...) or logical (and, or , not ...)
  • Statistics on variables are minimum, maximum, average and standard deviation. The scope of these statistics can be the entire acquisition, or the last N points of the acquisition (N defined by the user).

After opening the processing node, post-processing functions can be accessed by opening the "Post-processing" section. Two sheets are available:

  • The Expression sheet allows expressions to be built, mixing the available variables, operations and statistics.
post processing Main.png
  • The Statistic sheet allows statistics to be built upon the available variables, for the entire acquisition or last N points.
postprocessing statistic.png

1. Example expression

Here are the steps to perform the sum of 2 variables:
1. Fill the field Expression name, in this example "SumOfVar1Var2".

postprocessing expression name.png


2. Write your formula directly in the field Formula, or by using the operations pick-list and double-clicking on the available variables.

postprocessing writeformula.png


3. Clicking on the button +add to check the expression coherence and add it to the outputs list.

postprocessing addexpression.png


4. Deploying the flow to save the new configuration. When starting an acquisition, the new expression is calculated and is visible, like the other variables.

postprocessing sumfo in graph.png

2. Example statistic

Here are the steps to perform the average of the 10 last read values of Variable1.
1. Fill the field Statistic name, in this example "AverageVar1".

postprocessing namestat.png


2. Select the Variable, in this example "Variable1".

postprocessing statistic selectvar.png


3. Select the Function, in this example "Average".

postprocessing statistic selectfunction.png


4. Select the Scope, in this example, the average of the 10 last values read.

postprocessing statistic selectscope.png


5. Click on the button +add statistic to add the statistic to outputs.

postprocessing statistic validation.png


6. Deploying the flow to save the new configuration. When an acquisition starts, the new statistic is calculated and is visible like the other variables.

postprocessing statistic graph.png