Revision as of 10:52, 12 March 2024 by Registered User

1. Overview

Before reading this article, it is highly recommended to read STM32CubeMonitor:Introduction and main principles of STM32CubeMonitor, to better understand the STM32CubeMonitor concepts.

J-Link is a probe distributed by SEGGER. STM32CubeMonitor is compatible with the J-Link probe. This article describes how to use the J-Link probe with STM32CubeMonitor.

2. J-Link connection

The J-Link probe must be connected to the STM32 board through the SWD connector. Jumper wires can be used for this purpose. The table below shows the mapping between the J-Link probe and the CN4 (SWD) connector of a Nucleo board. Note that, in this configuration, the Nucleo board is still powered by its ST-LINK interface through a USB cable.


For further information, visit the related SEGGER wiki page[1].


3. J-Link nodes

Two nodes are dedicated to J-Link:

acqjlinkout.png to define and/or select a J-Link probe configuration (probe name), open and close the connection, and send commands to the selected probe.

acqjlinkin.png to define and/or select a J-Link probe configuration (probe name), and receive data from the selected probe.


4. Import the basic J-Link flow

Import the following flow into the STM32CubeMonitor workspace:

[{"id":"2da90ba20341d53c","type":"tab","label":"Basic_Jlink_Flow","disabled":false,"info":"# Basic flow to start with STM32CubeMonitor."},{"id":"033af5d1d80fcdca","type":"ui_chartst","z":"2da90ba20341d53c","group":"f9c34dde.1e2f4","name":"myChart","order":4,"width":15,"height":9,"chartType":"line","curveType":"linear","duration":"10","ymin":"","ymax":"","x":580,"y":280,"wires":[]},{"id":"b0a4f04cddfd14ad","type":"ui_button","z":"2da90ba20341d53c","name":"","group":"f9c34dde.1e2f4","order":3,"width":5,"height":1,"passthru":false,"label":"Clear Graphs","tooltip":"","color":"","bgcolor":"","icon":"","payload":"","payloadType":"str","topic":"clear","x":430,"y":380,"wires":[["033af5d1d80fcdca"]]},{"id":"f97c9515f36990e4","type":"ui_button","z":"2da90ba20341d53c","name":"","group":"f9c34dde.1e2f4","order":1,"width":5,"height":1,"passthru":false,"label":"START Acquisition","tooltip":"","color":"","bgcolor":"","icon":"","payload":"","payloadType":"str","topic":"start","x":110,"y":80,"wires":[["802f93573b8b1085"]]},{"id":"6a883cd65e59cb83","type":"ui_button","z":"2da90ba20341d53c","name":"","group":"f9c34dde.1e2f4","order":2,"width":5,"height":1,"passthru":true,"label":"STOP Acquisition","tooltip":"","color":"","bgcolor":"","icon":"","payload":"","payloadType":"str","topic":"stop","x":110,"y":160,"wires":[["802f93573b8b1085"]]},{"id":"c2b3bd46e656df7d","type":"processing","z":"2da90ba20341d53c","groupname":"myVariables","groupid":"d59587ff.cd1748","expressions":[],"statistics":[],"logmode":"no","logformat":"stcm","x":390,"y":280,"wires":[["033af5d1d80fcdca"],[]]},{"id":"cb834759e76e66eb","type":"ui_toast","z":"2da90ba20341d53c","position":"top right","displayTime":"3","highlight":"","sendall":true,"outputs":0,"ok":"OK","cancel":"","raw":false,"topic":"","name":"","x":570,"y":220,"wires":[]},{"id":"802f93573b8b1085","type":"variables","z":"2da90ba20341d53c","groupname":"","accesspoint":0,"execonfig":"","variablelist":[],"triggerstartmode":"manual","triggername":"","triggerthreshold":"","frequencyType":"0","mode":"direct","lastImportedTime":-1,"openStatus":false,"x":320,"y":100,"wires":[["126044b96147c531"],[]]},{"id":"126044b96147c531","type":"acquisition jlink out","z":"2da90ba20341d53c","name":"","probeconfig":"","x":570,"y":80,"wires":[]},{"id":"64321dc13c3a5881","type":"acquisition jlink in","z":"2da90ba20341d53c","name":"","probeconfig":"","x":120,"y":300,"wires":[["c2b3bd46e656df7d"],[]]},{"id":"f9c34dde.1e2f4","type":"ui_group","name":"Chart","tab":"17d09b07.741a55","order":1,"disp":true,"width":15,"collapse":false},{"id":"17d09b07.741a55","type":"ui_tab","name":"Home","icon":"dashboard","disabled":false,"hidden":false}]


  • Navigate to Menu > Import > Clipboard
  • Copy the .json formatted flow and paste it in the area
  • Click on Import

The flow is now imported into the STM32CubeMonitor workspace.

5. Basic J-Link flow

Below is an example of a basic flow to perform an acquisition with a J-Link probe. Instead of using STlink acquisition nodes for an ST-LINK, Jlink acquisition nodes are used for the J-Link probe.

basic jlink flow.png

The J-Link probe must be configured by selecting it from the picklist and indicating its node name in the "Name" field.

basic jlink flow nodeconfig.png

The version of the DLL used by the J-Link probe is indicated.

basic jlink flow probe config.png

Unlike the ST-LINK, the J-link requires that the user specifies the type of board to monitor. The user makes this choice by selecting the product. Once these operations are completed, the user can click on deploy and perform an acquisition, just like with an ST-LINK.

selectproduct.png

6. Limitations

Jlink support is limited to Windows ® 10 and 11, 64 bits(x64).

Multiprobe is not supported with jlink probe

Snapshot mode is not supported by jlink probe for the acquisition

7. Troubleshoot

"File not found" appears in the MCU picklist when the "SupportedHW.txt" file is not present in the stm32cubemonitor-jlink-protocol directory. The file "SupportedHW.txt" is part of the installer Setupxxxxx.zip.

8. Reference