Revision as of 12:25, 31 January 2024 by Registered User
  1. Overview

JLink is a probe distributed by Segger. STM32CubeMonitor is compatible with JLink probe. We will describe here how to use JLink probe with STM32CubeMonitor.

JLink connection

J-Link probe have to be connected to STM32 board using the SWD connector. Jumper wires could be used. Hereafter, the mapping between JlinkProbe and CN4 (SWD) connector on Nucleo Board. Please note that in this configuration Nucleo board is still powered by ST-Link using USB cable.

For further informations, please visit: https://wiki.segger.com/Connecting_to_STM32_Nucleo_boards

NUCLEO CN4 J-Link
Pin 2 (TCK) Pin 9 (SWCLK / TCK)
Pin 3 (GND) Pin 4 (GND)
Pin 4 (TMS) Pin 7 (SWDIO / TMS)
Pin 5 (NRST) Pin 15 (nRST)
Pin 6 (SWO) Pin 13 (SWO / TDO)
Any Vdd Pin Pin 1 (VTref)

Two nodes are dedicated to JLink:

acqjlinkout.png

ack jlink out: Allow to define and/or select a probe configuration (probe name), open and close the connection and send commands to the selected probe.

acq jlink in: Allow to define and/or select a probe configuration (probe name), and receive data from the selected probe.

User must choose the type of MCU monitored by selecting it in the picklist.


Troubleshoot

File not found" appears in the MCU pick list when the SupportedHW.txt file is not present in the directory xxxxxxxxx. The file "SupporedHW.txt" is part of the installer Setupxxxxx.zip.