This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.- Overview
JLink is a probe distributed by Segger. STM32CubeMonitor is compatible with JLink probe. We will describe here how to use JLink probe with STM32CubeMonitor.
JLink connection
J-Link probe have to be connected to STM32 board using the SWD connector. Jumper wires could be used. Hereafter, the mapping between JlinkProbe and CN4 (SWD) connector on Nucleo Board. Please note that in this configuration Nucleo board is still powered by ST-Link using USB cable.
NUCLEO CN4 | J-Link |
---|---|
Pin 2 (TCK) | Pin 9 (SWCLK / TCK) |
Pin 3 (GND) | Pin 4 (GND) |
Pin 4 (TMS) | Pin 7 (SWDIO / TMS) |
Pin 5 (NRST) | Pin 15 (nRST) |
Pin 6 (SWO) | Pin 13 (SWO / TDO) |
Any Vdd Pin | Pin 1 (VTref) |
Troubleshoot
Filenotfound