This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article explains how to add nodes in the palette of STM32CubeMonitor.
The Node Red community offers more than 2500 modules on the nodered.org website. According to customer applications, it could be useful to import modules in the STM32CubeMonitor palette.
First of all, node.js has to be installed on the device system. We recommand to follow the node js installation guide.
When installation of node js done, the menu manage palette allow to add modules in the palette.
Open the menu and select manage palette.
Choose the module to install
then install the module
Finally the new module is added at the end of the palette
Is it possible to remove a module (or disable nodes) from the manage palette window.