This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.My proposed solution with standard nodes is :
I have added a slider to generate the value (but can be done by any node) then the “template” node formats the payload, and the change node set the topic.
The variable address and variable type must be filled here. For the type and address, the easiest way it to try first with a write panel and a debug node, and see the values. The Payload value from input will be inserted in the template. (the value to write)
The next node is a “change” to set the topic to write
The result :
When the slider is moved, the new value is written to g_constDouble