This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Fixed issues
ID | Summary |
---|---|
73456 | The SFRs view is not aware of the device tree configuration and consequently shows all peripherals regardless if they are managed by the Cortex®-M or not. |
85064 | Some macOS® versions report installation image corruption or that the image cannot be opened because the developer cannot be verified. The work-around is to execute the following command:
xattr -c /Applications/STM32CubeIDE.app |
124770 | The user must modify the memory split between the CM4 and CM0+ core. There are multiple CM0+ pre-compiled stacks with different memory size requirements. |
134020 | RAM linker script for STM32H7B0xB device has only 128K RAM. |
134147 | ST-LINK GDB server dead-lock in persistent mode after a few GDB-client connections. |
134674 | The Build Analyzer "Memory Regions"-tab has an error in the "End Address" column. |
130208 | Fixed issues with selecting text in Linker script editor and solved dark theme issues |
74149
138057 107232 73456 |
Fixed issue with SFR view – incorrect values during search and filters will show child nodes. |
135591 | OpenOCD – Shared ST-LINK option persistent when switching script generation method. |
136427 | Fixed the issue with SWV ITM Console going black. |
123405 | Fixed issue with SWV bandwidth performance with ST-LINK GDB server. |
131836 | ST-LINK GDB server can now abort debug launch when STM32CubeProgrammer fails to perform the flash download. |
2. Known issues
The known issues are split into general, OS-specific, and target-specific issues.
2.1. General issues
ID | Summary | ||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
59435 | Having a space or non-ASCII character in the project/workspace path or installation path is not fully supported. | ||||||||||||||||||||||||
63624 | Some STM32CubeMX pop-up dialogs are not opened in front of the STM32CubeIDE workbench on all OS's. | ||||||||||||||||||||||||
68184 | Hierarchical projects cannot be imported with the option Copy into workspace. | ||||||||||||||||||||||||
68440 | Hierarchical projects cannot be renamed. | ||||||||||||||||||||||||
89454 | Restart configuration only works for flash memory projects and not for RAM projects. Program Counter register is not set correctly. Manual work-around: In Restart configuration, manually set PC to the ResetHandler() in RAM: set $pc = 0x20000xxx. | ||||||||||||||||||||||||
109764 | FreeRTOS™ kernel-aware debugging: Full stack traces off all tasks do not work if configUSE_PORT_OPTIMISED_TASK_SELECTION 1 | ||||||||||||||||||||||||
115928 | Editing live expressions while target is running does not work with SEGGER J-Link. | ||||||||||||||||||||||||
124062 | GCC-10 is more strict with respect to declaration of global variables in header files. Read the GCC-10 porting guide. | ||||||||||||||||||||||||
133183 | STM32CubeIDE cannot debug using FreeRTOS aware with J-LINK.
Reset strategy == Connect under reset, requires Initialization commands: 2.2. OS-specific issues2.2.1. macOS®
2.3. Target-specific issues2.3.1. STM32H7
2.3.2. STM32MP1
2.3.3. STM32WB
1. Same limitation for Linux® and macOS® [[Category:STM32CubeIDE errata | 95]] |