Revision as of 11:37, 1 September 2021 by Registered User (Update Integration section)

1. Introduction

Azure RTOS NetX Duo is a dual IPv4 and IPv6 TCP/IP network stack designed specifically for deeply embedded, real-time, and IoT applications. It comes with different set of features. Alongside the TCP/IP IPv4/IPv6 network stack, it provides a crypto library implementing the standard crypto and hash methods, and a TLS/DTLS library to support secure network connections.

NetX Duo Overview


  • NetX Duo core offers a full TCP/IP IPv4IPV6 compliant stack with 3 types of API: TCP/IP, UDP/IP and RAW API.
  • Crypto core implements the common crypto cipher suites and hashing algorithms useful for securing connections and exchanging encrypted data: AES, 3DES, HMAC, RSA, SHA1, SHA224, SHA256, SHA384, SHA512, MD5, HMAC-SHA1, and so on (each algorithm has its own implementation file .c and header file .h, which facilitate the selection and the integration of the required algorithms by the applications).
  • TLS core implements the secure connection API. Based on both the Crypto core and NetX Duo core, it supports the TLS and DTLS protocols with their different variants. (TLS 1.0 TLS 1.2, TLS 1.3)

It also supports the X509 public signed certificates protocol.

  • Addon protocols are a pre-supported set of network applicative protocols that ease the integration of the networking feature in the end user application. The main supported protocols are the following:

DHCP, DNS, mDNS, HTTP, HTTPS, FTP, TELNET, MQTT, SMTP, POP3, SNTP, SNMP, and so on.

Further details are available in the NetX Duo official documentation

NetX Duo folders are organized as explained below:

NetX Duo Folders


2. STM32 Integration

NetX Duo can run on any networking hardware, such as Ethernet, WiFi modules, cellular modems, and so on. It requires a low-level driver to interact between the physical layer already chosen, and the NetX Duo core requests (initialize, transmit data, receive data).

NetX Duo Low Layer Interfacing

To achieve the interaction between the NetX Duo stack and the required PHY, software architecture should follow the arborescence below.

NetX Duo Low Layer Files



The following hardware configurations are currently supported:

  • Ethernet: Currently any STM32 board that provides an Ethernet IP, uses the Ethernet PHY microchip LAN874X (driver under Drivers/BSP/Components In the X-CUBE-AZRTOS-H7 package).
Info white.png Information
NetX requires the Zero-copy feature that is currently supported only in the STM32H7 HAL Ethernet driver.


  • nx_stm32_eth_config_template.h: a template config header file to tune the corresponding driver for aspecific STM32 MCU/board. This file should be copied into the application source tree and renamed to nx_stm32_eth_driver.h, then customized according to the driver needs.
  • nx_stm32_*_driver.h: the driver header file containing the driver defines and data structure.
  • nx_stm32_*_driver_config_template.h: an application level config file that allows users to tune some options related to the driver, a template file is provided in the driver source tree for reference.
  • nx_stm32_*_driver.c: this is referenced directly by the application and may be different between STM32 series depending on the supported features.
NetXDuo_LANConfiguration


This is not the final version, future versions are planned to add interrupt mode to the currently implemented polling mode.

  • nx_stm32_xxx_driver_template.c/.h: an empty interface that can be used to implement a new custom driver.


  • WiFi: this support is specifically focusing on WiFi modules supporting bypass mode and STM32 boards that provides MXCHIP module EMW3080.

To ensure this connection mode, user should configure it with some flags in mx_wifi_conf.h file:

  • "mx_wifi_conf_template.h": this application-level config file should be copied into the application source tree and renamed mx_wifi_conf.h then customized according to the application and driver needs.

Main configuration flags to take into consideration are the following:

       "MX_WIFI_USE_SPI use SPI" to communicate with MXCHIP instead of UART.
       "MX_WIFI_NETWORK_BYPASS_MODE" Use Bypass mode instead of AT commands.
       "MX_WIFI_TX_BUFFER_NO_COPY" No copy of TX buffer required.
       "WIFI_SSID" define here the username of the access point. 
       "WIFI_PASSWORD" define here the password of the access point.
  • "Nx_driver_framework.c": it is the default entry point processing for the NetX Driver used as interface between NetXDuo core and the EMW3080 Phy liaison.
  • "Nx_driver_framework.h": is the driver header file containing the driver defines and data structure.
  • "Nx_driver_emw3080.c": is a Phy interface to link commands between nx_driver_framework and the Mxchip module.
  • "Nx_driver_emw3080.h": is the driver header file containing the driver defines and data structure.
  • "Mx_wifi_azure_rtos.c": contains all tx and nx allocations required by mxchip.
NetXDuo_WiFiConfiguration

This architecture is being improved and aligned with other wireless and networking packages.

Info white.png Information
WiFi driver is not supported in X-CUBE-AZRTOS-H7 (first integration of Azure RTOS in STM32Cube Ecosystem) and is planned for a future releases. However, WiFi bypass mode is supported on STM32U5 package including Azure RTOS Middleware and applications


After low-level configuration, it is called in application code when an IP instance is created:

/* Create an IP instance by linking the nx network driver */

/* ETHERNET STM32H7 example:  */
  ret = nx_ip_create(&EthIP, "NetX IP Instance 0", NULL_IP_ADDRESS, NULL_IP_ADDRESS, 
&EthPool, nx_stm32_eth_driver, pointer, IP_MEMORY_SIZE, DEFAULT_PRIORITY);

/* WIFI STM32U5 example: */
ret = nx_ip_create(&IpInstance, "Main IP Instance", NULL_IP_ADDRESS, NULL_IP_ADDRESS, 
& AppPool, nx_driver_emw3080_entry, pointer, MEMORY_SIZE, DEFAULT_PRIORITY);

2.1. Known limitations

  • The support of the BSD API is not fully-compliant, this may impact the portability of legacy applications. More details are available in the official NetX Duo documentation official documentation

3. How to use

The main APIs needed to use the NetX Duo are described in table below: (further details and a full API description are available from NetX Duo official documentation)

Function Name Short Description
nx_tcp_socket_create( ) Create a TCP socket
nx_udp_socket_create( ) Create a UDP socket
nx_tcp_server_socket_listen( ) Set up TCP socket to listen
nx_udp_socket_bind( ) Bind UDP socket to the PORT
nx_tcp_server_socket_accept( ) Accept a TCP remote client socket connection
nx_tcp_socket_receive( ) Receive a packet from a TCP remote client
nx_udp_socket_receive( ) Receive a packet from a UDP remote client
nx_tcp_socket_disconnect( ) Disconnect the TCP server socket
nx_tcp_server_socket_unaccept( ) Reject the TCP server socket
nx_tcp_server_socket_relisten( ) Set up server socket for listening again

The main steps to use the NetX Duo are:

  • First, initialize nx_system from the tx_application_define function, then create a pool (named ETH_pool in the next example).


    NX_PARAMETER_NOT_USED(first_unused_memory);

    /* Initialize the NetX system.  */
    nx_system_initialize();

    /* Create a packet pool.  */
    status = nx_packet_pool_create(&pool_0, "NetX Main Packet Pool", SAMPLE_PACKET_SIZE,
                                   (UCHAR *)sample_pool_stack , sample_pool_stack_size);


  • Then, create and configure an IP instance which belongs to pool already created.
  • Enable the needed NetX Duo components depending on the target application:
Function Name Short Description
nx_arp_enable( ) Enable the Address Resolution Protocol (AutoIP Protocol need ARP)
nx_icmp_enable( ) Required for Ping
nx_udp_enable( ) Enable UDP traffic (DNS & DHCP need UDP)
nx_tcp_enable( ) Enable TCP traffic



4. Migration to NetX Duo

In order to migrate a development project from an existing network stack (like LwIP or others) to NetX Duo, there is no straightforward automatic procedure, but there are usually some API similarities helping to perform this task. Some comparative examples are provided below.

Action NetXDuo LwIP
DHCP Serice
/* create the DHCP client */
ret = nx_dhcp_create(&DHCPClient, &IpInstance, "DHCP Client");
  
/* Create an IP @ change callback */
ret = nx_ip_address_change_notify(&IpInstance, ip_address_change_notify_callback, NULL);

/* start DHCP client */
ret = nx_dhcp_start(&DhcpClient);
/* Start DHCP process to get IP@*/
dhcp_start(netif);

/* Get Client data */
dhcp = (struct dhcp *)netif_get_client_data(netif, LWIP_NETIF_CLIENT_DATA_INDEX_DHCP);

/* Wait until getting DHCP data */
if (dhcp_supplied_address(netif))
{
  DHCP_state = DHCP_ADDRESS_ASSIGNED;
}
HTTP Service
/* Create the HTTP Server.  */
status = nx_http_server_create(&HTTPServer, "WEB HTTP Server", &IPInstance, &ram_disk, 
                          pointer, SERVER8STQCK, &WebServerPool, NX_NULL, webserver_request_notify_callback);

/* Start the WEB HTTP Server.   */
status = nx_http_server_start(&HTTPServer);

/* Web Server callback when a new request from a web client is triggered */
static UINT webserver_request_notify_callback(NX_WEB_HTTP_SERVER *server_ptr, UINT request_type, CHAR* resource, NX_PACKET *packet_ptr);

/* Extract the client request type from the client request */
nx_web_http_server_type_get(server_ptr, server_ptr->nx_web_http_server_request_resource, temp_string, &string_length);
/* Create a new TCP connection handle */
conn = netconn_new(NETCONN_TCP);

/* Bind to port 80 (HTTP) with default IP address */
err = netconn_bind(conn, NULL, 80);

/* Put the connection into LISTEN state */
netconn_listen(conn);

/* Accept any incoming connection */
accept_err = netconn_accept(conn, &newconn);

/* Read the data from the port, blocking if nothing yet there. 
   We assume the request (the part we care about) is in one netbuf */
recv_err = netconn_recv(conn, &inbuf);

/* Get the data pointer and length in netbuf */
netbuf_data(inbuf, (void**)&buf, &buflen);





5. STM32 NetX Duo applications

The Following figure shows the project architecture and main application files.

NetX Duo Application Files

STM32 Packages provide the following set of applications (supported applications list may differ between products and boards):

Application Short Description
Nx_TCP_Echo_Server Demonstrates how to develop a NetX TCP server to communicate with a remote client using the NetX TCP socket API. [readme]
Nx_TCP_Echo_Client Demonstrates how to develop a NetX TCP client to communicate with a remote sever using the NetX TCP socket API. [readme]
Nx_UDP_Echo_Server Demonstrates how to develop a NetX UDP server to communicate with a remote client using the NetX UDP socket API. [readme]
Nx_UDP_Echo_Client Demonstrates how to develop a NetX UDP client to communicate with a remote sever using the NetX UDP socket API. [readme]
Nx_WebServer Demonstrates how to develop Web HTTP server based application. It is designed to load files and static web pages stored in an SD Card using a Web HTTP server, the code provides all required features to build a compliant Web HTTP Server. [readme]
Nx_MQTT_Client Demonstrates how to exchange data between client and server using MQTT protocol in an encrypted mode supporting TLS v1.2.. [readme]
Nx_SNTP_Client Demonstrates how to develop a NetX SNTP client and connect with an STNP server to get a time update. [readme]