Revision as of 11:13, 22 June 2021 by Registered User
This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or
pending task to finish installation of
Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Fixed issues
ID |
Summary
|
70505 |
Implemented a newlib-malloc solution that is safe by default.
|
95809 |
On Fedora®, the installation now depends on webkit2gtk3 which solves the issue of the Information Center not rendering properly.
|
99895 |
Implemented a project less debug solution with use of elf-file.
|
107086 |
Miscellaneous flags through the MCU GCC compiler are now processed correctly.
|
2. Known issues
The known issues are split into general, OS-specific issues and target-specific issues.
2.1. General issues
ID |
Summary
|
56223 |
The project importer for SW4STM32 cannot import all settings in projects from very old versions (older than 2.0).
|
59435 |
Having a space or non-ascii character in the project/workspace path or installation path is not fully supported.
|
63212 |
Editor hyperlinks sometimes jump to declaration instead of definition.
|
63624 |
Some STM32CubeMX pop-up dialogs are not opened in front of the STM32CubeIDE workbench on all OS's.
|
68184 |
Hierarchical projects cannot be imported with the option Copy into workspace.
|
68440 |
Hierarchical projects cannot be renamed.
|
74251 |
SWV Exception Trace log data tab displays a peripheral column, which is always empty.
|
89454 |
Restart configuration only works for Flash memory projects and not for RAM projects.
|
99894 |
The new GCC-9 toolchains produce more warnings than the previous GCC-7 toolchains.
|
100895 |
Editing live expressions while target is running does not work with SEGGER J-Link.
|
101005 |
New JRE™ bundling does not contain a valid certificate chain for the requested SSL connection. See knowledge article.
|
107869 |
Non-stop debug does not work with RTOS proxy.
|
2.2. OS-specific issues
2.2.1. macOS®
ID |
Summary
|
83159[1] |
After updating STM32CubeIDE, the post-update restart fails on Ubuntu® and macOS®. STM32CubeIDE must be restarted manually.
|
85064 |
Some macOS® versions report installation image corruption. This can be circumvented using the command: xattr -c /Applications/STM32CubeIDE.app
|
2.2.2. Linux
ID |
Summary
|
77518 |
MCUFinder is unusable on GNOME on Wayland.
|
83159[1] |
After updating STM32CubeIDE, the post-update restart fails on Ubuntu® and macOS®. STM32CubeIDE must be restarted manually.
|
2.3. Target-specific issues
2.3.1. STM32MP1
ID |
Summary
|
73456 |
An STM32MP1 project being debugged in Cortex®-M shows all peripheral registers in the SFR view, even those not managed by Cortex®-M.
|
73895 |
When using a proxy server, if the STM32MP1 is not accessible through the server, it is required to add the IP address to the proxy bypass list.
|
73896 |
The synchronization check between the IP-address entered in launch configuration and the IP-address of the target does not abort the launch in case of mismatch.
|
2.3.2. STM32H7
ID |
Summary
|
73552 |
Serial Wire Viewer configuration is not reset for STM32H7 devices on the next launch if it was terminated with record active when using ST-LINK GDB server.
|
79658 |
When debugging STM32H7 dual-core devices with one core going to sleep, ST-LINK GDB server reports 0x05F0001. This cannot be circumvented by using OpenOCD as it does not support debugging on STM32H7 dual-core devices using sleep modes.
|
2.3.3. U5
ID |
Summary
|
109124 |
When selecting the default auto frequency the ST-Link GDB Server does not detect the MCU. Use a frequency of <= 8000 KHz instead.
|
1. Same limitation for Ubuntu® and macOS®