This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Over time the probe list can be filled by unused probes, the the removal of unused probe is done with the "Delete" button of "Edit node probe" panel.
There are 3 ways to access to “Edit node panel”:
- The first way is opening the “acq in” or “acq out” probe. (Same as modifying the probe)
Select one probe and press the pencil button to access to “Edit node probe" panel.
In the “Edit node probe panel” select the probe to delete and press the “Delete” button.
- The second way is from “Configuration nodes” menu in “On all flows” part, double click on the probe to delete to open the “Edit probe node” panel and press the “Delete” button.
- The third way is available from the STM32CubeMonitor V1.2.0 which include Node-Red version 1.2. The access to probe is available from “Global Configuration Nodes” part in info tab.
From “Global Configuration Nodes/probe” in “info” tab, double click on the probe to delete and press the Delete button.