1. Design of a STM32Cube Expansion enhanced for ST Toolset
A STM32Cube Expansion enhanced for ST Toolset is an evolution of the initial concept of STM32Cube Expansion. The new packages contain now a part readable and configurable into STM32CubeMX (or STM32CubeIDE) on top of Ready-To-Use Project Samples.
It helps the integration of software components into STM32Cube ecosystem. The role is to limit the manual work to integrate a SW component (it will limit but it could remain some manual operations to be executed by the end user). The major advantage of integrating your software in STM32CubeMX is that you can allow the STM32CubeMX users to integrate your SW component on any board or MCU from the STM32 Galaxy.
2. Three Webinars to start up
Three webinar have been prepared by our teams to show you a part of the capacity of the CubeExpansion Do It Yourselves
- Sequencer Pack :
A utility for multi-tasking without an Operating System, which is HW independent code. In the example, a LED/GPIO is managed
Code to download: https://stmicroelectronics.sharepoint.com/teams/CubeExpansionProject/Shared%20Documents/Pack%20Examples/I-CUBE%20tutorial/Sequencer/I-CUBE-SEQUENCER.ZIP
- DSPDemo Pack :
This SW component uses the DSP integrated in the Core to generate an internal signal. This internal signal is then captured and displaid thanks to CubeMonitor. There is no hardware interaction
Code to download: https://stmicroelectronics.sharepoint.com/teams/CubeExpansionProject/Shared%20Documents/Pack%20Examples/I-CUBE%20tutorial/I-CUBE-DSPDEMO/I-CUBE-DSPDEMO.zip
- STDIO Pack
interest:
Code to download:
3. Auto-assessment
Any SW component is not adapted to the development of a STM32Cube Expansion enhanced for ST Toolset. Indeed, the possibility of configurations are huge and not covered completely by the tools. Some other method may be feasible but are not considered in the normal flow.
We refer to this list of questions to identify the right candidates. The questions should be taken in the generic understanding of the Industry.
- I’ve already used STM32CubeMX or STM32CubeIDE to generate a project? ==> If yes, move to the next question
The concept is based on the usage of STM32CubeMX. We recommend starting only when you have already acted as a standard user of STM32CubeMX. If not, start downloading and opening STM32CubeMX, pick up a STM32 MCU, configure peripherals, generate the project for your preferred IDE and look at the result.
- <My SW component> is well structured? ==> If yes, move to the next question
My software is structured in functional units/components self-content from an architecture point of view.
- <My SW component> has a standard build system? ==> If yes, move to the next question
We exclude cases such as complex cases with different linker scripts, generating more than one binary file, if your software needs to dynamically adapt the run-time configuration. STM32CubeMX generates simple project structure (cf basic or advanced structure)
- I’m ready to adapt my architecture to STM32Cube rules when interacting STM32Cube components ==> If yes, move to the next question
STMicroelectronics has defined some rules to interact between STM32Cube components to guarantee coherency between SW components. There is no impact on your own SW component architecture but on the structure of the project (location of your SW component into the project itself, location of the HAL drivers, usage of STM32Cube API…). Indeed, the project structure must be as expected by STM32CubeMX. Using STM32PackCreator and STM32CubeMX prevents most of the problems (link to STM32PackCreator Getting Started)
- I’m ready to add this delivery method on a long run ==> move to the next question
We value working with partners and customers on the long run. The work related to the STM32CubeExpansion package will be valuable if you intend to upgrade it regularly with new versions of your SW component. Therefore, the method could be done one time but needs to be thought on the long run.
- <My SW component> is HW agnostic ==> GO to training “DSPDEMO Sample”
Your software component has no relation with any HW components (no peripherals or IP of STM32). This video training and the associated I-Cube describe the creation of STM32CubeExpansion in a simple SW component.
- <My SW component> has some HW relation with UART, I2C, SPI, GPIO => GO to training “Sequencer I-Cube”
This video training and the associated I-Cube describe the creation of STM32CubeExpansion in a simple SW component with the usage of GPIO.
- <My SW component> has some HW relation with Timers => take care - refer to STM32PackCreator limitation
Basic usage of timers is supported. Complex and advanced features are too complex to be implemented in our tools.
- <My SW component> has some HW relation with other peripherals than the ones mentioned above => be cautious - GO to training "STDIO sample
This is part of our limitation regarding Tooling. It can be done with other methods but there are too complex to be explained here.
4. Three steps to design your STM32Cube Expansion enhanced for ST Toolset
The design of a STM32Cube Expansion enhanced for ST Toolset is usually done in three steps. In real work, you’ll have several iterative works between Step1 & Step2 up to have the right result.
4.1. Step1: Design a “pack enhanced for STM32CubeMX” using STM32PackCreator
First and foremost, start STM32PackCreator: Go to $YourLocation$\STMicroelectronics\STM32Cube\STM32CubeMX\utilities\STM32PackCreator
The methods to develop the step1 are explained through the video listed above or in the “Getting started Pack Creator”, accessible in the help menu of the STM32PackCreator.
Ensure that you’ve activated the “PACKAGES STM32Cube RULES COMPLIANT” in the STM32PackCreator.
Intermediate steps in this Step1 may be:
- Design a CMSIS Pack
- Design a simple configurable Pack
- Integrate a HW dependency
- Integrate an application
Video & Tutorial are available on GitHub and st.com.
You’ve obtained a pack enhanced for STM32CubeMX. This pack can be loaded, configured in STM32CubeMX and generate the associated code.
4.2. Step2: Develop two to three examples
You are going now to develop two to three examples on one or few STM32 boards. Those examples must of course be generated by STM32CubeMX tool, using your “pack enhanced for STM32CubeMX”.
The interests of this step are twice:
- You will validate your implementation of the pack on different HW and different configurations,
- You’ll prepare some project examples that you will integrate into the STM32CubeExpansion package itself. Your customers may indeed start directly from the example, without using STM32CubeMX tool.
To execute it, you will act as a user of your pack enhanced for STM32CubeMX and execute the following actions:
- You load your pack “enhanced for STM32CubeMX” inside STM32CubeMX (cf STM32CubeMX user manual for more detail).
We recommend the usage of STM32CubeMX. Indeed, even if STM32CubeIDE integrates the STM32CubeMX plugin, it will be not possible to generate the projects for the three IDEs (IAR™ EWARM, Keil® MDK-ARM, and STM32CubeIDE) from STM32CubeIDE. It will be limited to STM32CubeIDE only.
- You configure the peripherals, the SW components, the clock, the project settings to be adequate to your need.
- You copy paste the Drivers (HAL) that you need inside the Drivers directory inside your Package
- You generate a project (check the project settings below to take into account the Drivers from your Package).
- You add some user code in the user section to make it demonstrable.
- You save the STM32CubeMX configuration file (ioc) for each project. We recommend saving the name of the project like "Name_Of_Application#N”. It will be reflected also on the ioc file which will be called “Name_Of_Application#N.ioc”.
The project settings should be reflected like that
and
- You generate your projects for the 3 IDEs (IAR™ EWARM, Keil® MDK-ARM, and STM32CubeIDE) and test them.
4.3. Step3: Deliver a STM32Cube Expansion Package (I-CUBE)
This is the final step. It integrates the outputs of step1 and step2 together into a package called STM32Cube Expansion Package. These packages are published on www.st.com with X-CUBE part numbers if they are distributed, maintained and supported by STMicroelectronics. Some packages distributed, supported and maintained by ST Authorized Partners are also exposed on www.st.com with I-CUBE part numbers. The interests of this step are that you’ll deliver to your customer a single deliverable. - This .pack deliverable contains all necessary files to import software components and configure them in STM32CubeMX or STM32CubeIDE tool, and generate a project for any STM32-based hardware. - The .pack is in ZIP format and can also be unzipped and users can get started with ready-to-use project examples, pre-configured to compile in the 3 IDEs (IAR™ EWARM, Keil® MDK-ARM, and STM32CubeIDE) and run out-of-the-box on specific ST boards.
First, some cleanup actions are required:
- The line “ProjectManager.FirmwarePackage=XXXX” shall be removed from the file “.ioc” included in the examples folder. Indeed, STM32CubeMX versions will continue evolving and to avoid version issues, remove this line.
- The STM32Cube Expansion Package PDSC file shall be checked with the PackChk.exe provided by ARM.
- All non-user comments shall be removed from the IPconfig and IPmodes files, when available
Then, two documents have to be written
- A user getting started document (chm, rtf, pdf...) located under Documentation folder at the root of the Package is also expecting. the content would be:
- How to use your specific STM32Cube Expansion in STM32CubeMX
- The goals and usage of project examples
- Remaining manual operation on the charge of the end user if any.
- A release note document should be also included, describing the content release, the corrected issues....
A doc/ folder, containing the CHM file describing APIs and parameters of Middleware elements, should be located at the same level as the Middleware Release_Notes. Several examples of such documents can be found into Expansion Packages.
The documents should be referenced in the pdsc file using the following options (according to CMSIS-pack standard)
- For component or api documentation, use: <file category="doc" ...>
- For bundle documentation, use: <doc ...>
You could add some files and example projects in the additional files to the existing package thanks to the STM32PackCreator. You need to use “Additional Files” button.
You’re done! You can now deliver it as is to your customers, partners.
If you want to go further and make it exposed in STM32CubeMX tool, you can contact your ST local representative.
5. STM32Cube Expansion Structure
The STM32Cube Expansion Structure top level is the following:
- CubeMX: generated by STM32PackCreator (available in STM32CubeMX panel Tools). It contains the files required by STM32CubeMX in order to configure the SW Component.
- Middlewares: contains your SW component itself. Under ST subdirectories when coming from ST, under “Third_Party” when coming from your side or from a community.
- Projects (examples): contains the examples of projects (2 or 3). They have been generated by STM32CubeMX for several IDEs and for several boards. Here is an example of advanced structure.
Here is an example of basic structure.
- Drivers: contains the drivers which are required for the projects (examples). Copy paste them from the CubeFW Package of the series that you have taken as examples.
- Utilities: contains any PC software which could be useful for your pack
- Documentation: contains the getting started and or any other documentation related to the package except the release note.
Other documents at the root of the package:
- License.pdf: contains the license. It will be displaid during the installation process
- Release_Notes.html: contains information on the release such as goals, modified files, corrected bugs and limitation if any
- VendorName.CubeExpansionName.pdsc: the file pdsc contains the description of the file included into the packages
The STM32CubeExpansion structure follows the standard STM32CubePackage structure. This structure is fully described into the document UM2285 Development guidelines for STM32Cube Expansion Packages.
In conclusion, if you want to map the "step1", "step2" and "step3", it will be like that
6. Going further
- Creating software packs and STM32Cube Expansion Packages enhanced for STM32CubeMX (TLMS 15788 / UMxxxx)
- Development guidelines for STM32Cube Expansion Packages: define in details the structure of STM32Cube MCU Packages in general and STM32Cube Expansion Packages in particular (TLMS 13884 / UM2285 / V2 / guidelines)
- STM32Cube firmware component architecture (TLMS 6682 / UM2388 / firmware specification)
- STM32Cube BSP drivers development guidelines UM2298
- Development checklist for STM32Cube Expansion Packages
7. Frequently Asked Questions
- There are some existing plug in’s for Eclipse to manage CMSIS pack. Could I use them with STM32CubeIDE on top of STM32CubeMX plug-in?
- We don’t test external eclipse plug in.
- Could I use STM32CubeIDE to test and generate a STM32Cube Expansion Package?
- As a partner developing a STM32Cube Expansion package, we recommend using STM32CubeMX. Indeed, the STM32Cube Expansion package should include some examples for the 3 IDEs and this is feasible with STM32CubeMX
- I’ve analyzed several ST STM32Cube Expansion (X-CUBE-BLE1, X-CUBE-MEMS) but they can’t be re-opened with STM32PackCreator. Have they been designed with STM32PackCreator?
- The first X-CUBE have not been designed with STM32PackCreator. So, you may find some tricks which are not feasible with STM32PackCreator. STMicroelectronics supports only the STM32PackCreator feature set.
- There is a Example keyword into CMSIS pack standard. Could I use it to describe the 2 to 3 examples (step2) ?
- So far, this keyword is not used by STM32CubeMX so far.
- There is some beautiful User Interface into STM32CubeMX (for some peripherals). Could I reproduce the same with STM32PackCreator?
- STM32CubeMX allows some integration of java code to design complex User Interface. This feature is not expose to external plug in.
- Once the STM32Cube Expansion Package is selected into STM32CubeMX additional software management panel, I would like that some settings from dependent peripherals are automatically selected. Is it possible?
- This is not possible and not expected. Indeed, your SW component can be used with different series and so, this is not expected to pre-fill the parameters. Our recommendation is to provide some examples with a defined configuration to your users and also a “getting started” document.
- Could I modify the XML files generated by STM32PackCreator?
- STMicroelectronics doesn’t support this case.
- Could I use the Pack ARM CMSIS?
- The pack ARM CMSIS can be opened with STM32CubeMX but as some components are also coming from STM32Cube MCU Packages, you may face some incompatibilities. Take care about them.
- What is the difference between a STM32Cube Expansion Package and a CMSIS Pack?
- The STM32Cube Expansion Package enhanced for ST Toolset is in general configurable. The generated code by STM32CubeMX when using STM32Cube Expansion Package has always a similar structure. It is based on STMicroelectronics HAL and LL drivers. It embeds some ready to use examples with .ioc file.
- Where are my packages stored?
- Look at %HOME%\STM32Cube\Repository\Packs.
[[Category:]]